ユーザーガイド 6040

MAX11300/MAX11301 PIXI Configuration Software User Guide

筆者: Sean Long

要約: This user guide provides a step-by-step instruction to create a configuration bitstream for the MAX11300 and MAX11301 PIXI ICs. The MAX11300/MAX11301 Configuration Software provides easy configuration for all possible configuration modes. Each port can be configured through simple drag-and-drop functionality to select the mode required. The software tool generates the bitstream that users download to the target PIXI IC in order to configure its functionality within their end application. All configurations implemented through this software can be saved for later use.