ユーザーガイド 5981

PowerTool MAXPOWERTOOL002# Quick Start Guide


要約: The MAXPOWERTOOL002# is an interface adapter between a host PC (IBM-compatible) and Maxim’s PMBus-compatible power supply EV kits. The interface to the host PC is a standard type-A to mini-B USB cable. The interface to the EV kit is through a 16-pin ribbon cable that carries the PMBus commands.

The MAXPOWERTOOL002# is intended to be used with Maxim’s PowerTool GUI and works with the following devices: MAX20751, MAX15301, and MAX15303.