アプリケーションノート 7082

Non-Invasive Blood Pressure Monitoring System

筆者: Recep Ozgun

要約:

An optical sensor-based, cuffless blood pressure system is introduced in this application note. The most significant difference in the indications for the MaximBPT as compared to traditional noninvasive blood pressure (NIBP) devices is that MaximBPT requires calibration and is primarily designed to provide the user with trends in blood pressure, where successive estimations are relative to this calibration point. This application note provides a general description of blood pressure, along with the MaximBPT system, algorithms, and its operating principles. The protocols for calibration and measurement are specific to MaximBPT, yet the basic principles of clinical trials, reference measurements, and evaluation methodology are based on industry standards.


Introduction

Blood pressure (BP) is a vital sign that provides critical information about cardiac output, cardiac pressure, and hemodynamic stability.

BP correlates well with the risk of advanced cardiovascular disease (ACVD). (Chockalingam) Also, hypertension, a medical condition in which systolic BP is above 140mmHg and/or diastolic BP is above 90mmHg persistently, is a risk factor for coronary heart disease and the single most important risk factor for stroke. Systolic BP is the maximum pressure in the arteries when the heart contracts. Diastolic BP is the minimum pressure in the arteries between the heart's contractions.

Therefore, continuously monitoring BP is valuable. However, the conventional noninvasive method—a cuff sphygmomanometer—usually allows only one reading every few minutes. Moreover, the inflation process disturbs the user and makes BP measurement inconvenient during sleep or exercise.

Maxim Blood Pressure Trending System

Maxim Blood Pressure Trending (MaximBPT) is a BP measurement system using a photoplethysmography (PPG) signal obtained from the fingertip. The system requires user-specific calibrations, and successive measurements are relative to this calibration point. The goal of the system is to make BP measurements readily available to the user through widely available consumer devices like smartphones or wellness watches. The system is most useful and accurate when measurements are taken in a resting state, as in traditional cuff-based BP systems. This application note contains evaluation methods and design specifications for the MaximBPT system.

Operating Principles

In principle, changes in PPG shape are correlated to BP changes. The PPG pulse has two phases: the anacrotic phase is the rising edge of the pulse, and the catacrotic phase is the falling edge of the pulse (Figure 1). The first phase is associated with systole, and the second phase with diastole and wave reflections from the periphery. Some of the determinants of the PPG shape have been described in literature, such as systolic amplitude, pulse width, pulse area, peak-to-peak interval, pulse interval, and artery stiffness index. (Elgendi; Shin)

Waveform of the PPG and its characteristic parametersFigure 1. Waveform of the PPG and its characteristic parameters.

The MaximBPT system requires a PPG signal from the sensor and associated BP values from a traditional cuff-based BP device during calibration. Subsequent systolic and diastolic BP changes are calculated by PPG shape changes relative to the calibration instance.The MaximBPT system requires a PPG signal from the sensor and associated BP values from a traditional cuff-based BP device during calibration. Subsequent systolic and diastolic BP changes are calculated by PPG shape changes relative to the calibration instance.

System Components

Figure 2 depicts the main components of the MaximBPT system. It utilizes a Maxim wellness sensor, which can be adapted in mobile devices or wearables for wellness monitoring, and a MaximBPT software application (app) that uses the PPG signal of the wellness sensor.

Overview of the MaximBPT systemFigure 2. Overview of the MaximBPT system.

Operating Protocols

Calibration Protocol

Calibration is a critical step in which BP reference measurements are taken to calibrate the algorithm with the associated PPG signals. One of the following options is recommended to provide the BP reference values:

  • A trained medical professional uses a medical-grade BP device available at the doctor's office or hospitals
  • Self-measurement using an FDA-cleared, cuff-based BP measurement device, such as the following:
    • Omron® BP785N 10 Series Upper Arm Blood Pressure Monitor
    • Welch Allyn Home 1700 Series Blood Pressure Monitor
    • QardioArm® Wireless Blood Pressure Monitor

These calibration reference values are valid for 4 weeks, and thereafter recalibration is required to expect the accuracy figures to hold. The calibration protocol has three main sections:

  • Subject preparation
  • BP reference measurement
  • PPG collection from the fingertip

Subject Preparation

Before calibration, the subject should:

  • Use the bathroom, if needed
  • Refrain from exercising within the previous 30 minutes
  • Refrain from consuming alcohol, caffeine, or nicotine within the previous 30 minutes

During calibration, the subject should rest quietly for about five minutes in a seated position where subject's elbow rests on the table, slightly below the level of the heart. The palm should be turned upward, with the hand remaining open and relaxed. The arms, back, and feet should be supported and in a relaxed position. The legs should remain uncrossed.

BP Reference Measurement

The user will first create a unique user ID. MaximBPT calibration is required before the first use of the MaximBPT, and thereafter when the calibration expires. The app's graphical user interface (GUI) for calibration is depicted in Figure 3.

MaximBPT GUI and relevant instructions during the calibration procedureFigure 3. MaximBPT GUI and relevant instructions during the calibration procedure.

Once the user has created an ID or selected an existing ID, the user takes BP measurements with the reference device and records the systolic and diastolic BP measurements (in mmHg) within the MaximBPT application (Figure 3). It is important that the user follows the reference device instructions to ensure an accurate measurement.

PPG Data Collection by the MaximBPT Application

Once the user has collected the reference values, the user follows the MaximBPT application instructions for calibration.

After pressing the Measure BP button on the screen (Figure 3), the user places his or her finger onto the PPG sensor. The MaximBPT application collects the necessary BP values. Once the calibration PPG data collection is complete, the application returns the signal value success (Figure 4, left screenshot). The process takes approximately one minute.

If the calibration is not completed within a minute, the application will return a signal value of failure (Figure 4, right screenshot). Failure might occur if the PPG signal quality is low (due to low perfusion or motion artifacts).

Calibration progress state updates on the Android® applicationFigure 4. Calibration progress state updates on the Android® application.

Measurement Protocol

Subject Preparation
Subject preparation prior to measuring BP is identical to the preparation prior to calibration.

BP Measurement
Figure 5 depicts the GUI for capturing the BP measurement. Once the user is prepared, the user selects the appropriate user ID from the Create/Switch User screen. Then, the user presses the Measure BP button, which initiates system capture of the user's measurements. As the subject keeps his or her finger on the device, the BP values will be reported continuously.

MaximBPT GUI and relevant instructions during regular measurementFigure 5. MaximBPT GUI and relevant instructions during regular measurement.

During PPG data collection (capture of user measurements), the collection progress will be displayed on the GUI (Figure 6). After PPG data collection, BP trending values for systolic and diastolic BP will be reported in the table and in graphical format, and the signal status will either change to Success or Failure as described in the PPG Data Collection by the MaximBPT Application section.

The user can observe the BP measurements per every heartbeat in the GUI. The display screen also provides the statistical values of the current session only, such as minimum/maximum BP values.

After the measurement is complete, the results will be added in the history log. When the BP HISTORY button on the GUI Welcome screen (Figure 5) is pressed, it will take the user to the history log page that lists the calibration BP, measurements and trending values, and time stamps (Figure 7).

GUI reporting the BP trending valuesFigure 6. GUI reporting the BP trending values.

Example of a BP HISTORY screen in the MaximBPT applicationFigure 7. Example of a BP HISTORY screen in the MaximBPT application.

Evaluation Methodology

Accuracy Metrics

The Association for the Advancement of Medical Instrumentation (AAMI) accuracy requirements (ANSI/AAMI/ISO 81060-2) are referenced to evaluate the algorithm. Criterion 1 of this standard requires a BP measurement such that the mean of the estimation error (MERR) must be within or equal to ±5.0mmHg, and that the standard deviation of the error (STDERR) must be no greater than 8.0mmHg, both for systolic and diastolic BP measurements.

where n is the number of determinations, and PDUT and PREF are the BP determination by the device under test and the reference device, respectively.

These requirements will be the accuracy target for MaximBPT within the calibration hold period, which is defined as 4 weeks.

Evaluation Results

The evaluation dataset is based on a data collection that was performed in an independent medical device clinical trial laboratory, and it is compliant with the normative references mentioned in ANSI/AAMI/ISO 81060-2 standards document. The reference device is a sphygmomanometer with a dual auscultator, and measurements were taken by two medical professionals concurrently. PPG data and reference measurements were collected from 136 subjects. Twelve subjects were selected for evaluation, and their data was not used for algorithm development.

MaximBPT accuracy was evaluated by running the MaximBPT executable file offline with the PPG samples from these subjects. The evaluation dataset subjects were selected such that age, gender, and BP levels are similar to the datasets left for model development. Evaluation results are summarized in Table 1.

Table 1. Accuracy Table for the Evaluation Dataset

Systolic Blood Pressure Diastolic Blood Pressure
MERR STDERR MERR STDERR
Initial Calibration +2.7 4.2 -2.3 5.4
Post-Induction -3.1 5.9 -3.1 5.2
Rest-to-Rest +1.7 7.4 +0.1 7.6

This table depicts the mean (MERR) and standard deviation (STDERR) of the estimation error for post-calibration (a few minutes after calibration, 28 samples), post-induction (in a resting state, a few minutes after BP perturbations, 72 samples), and rest-to-rest (in a resting state, 3 to 4 weeks post-calibration, 216 samples) protocols. Each sample is a difference vector of two data packets, one from the calibration protocol and one from the test protocol.

Note that the Table 1 accuracy table is based on the most recent algorithm version and is subject to change.

Bland-Altman Plots

Bland-Altman is a graphical method to compare two quantitative measurements. Scatter plots of the differences between the test device and reference measurement vs. the actual blood pressure difference relative to calibration values provides a good visualization for blood pressure estimates and error bounds. It is commonly used for BP evaluation, as depicted in Figure 8.

Scatter plot of measurement error vs. true BP change for MaximBPT evaluation in rest-to-rest (week-3/4) protocol is givenFigure 8. Scatter plot of measurement error vs. true BP change for MaximBPT evaluation in rest-to-rest (week-3/4) protocol is given.

System Specifications

Table 2 summarizes the major system specifications such as BP or heart rate bands, device- and sensor-related parameter intervals where the algorithm reports valid estimations; and use-case details. These measurement and environmental factors, as well as hardware and software specifications, should be taken into account during system evaluation.

Table 2. System Requirements and Specifications

Category Features Specifications
BP Trending Measurement principle Optical PPG signal from fingertip
Measurement range Systolic BP 80mmHg to 180mmHg, trend ±30mmHg
Diastolic BP 50mmHg to 120mmHg, trend ±20mmHg
Measurement time 30s to 60s
Target accuracy AAMI/ISO 81060-2 (criterion 1 grading) within 4 weeks of calibration
User Patient population 22yrs to 65yrs old
Subject state Resting, at least 5min
Resting heart rate 50BPM to 95BPM
Measurement Arm and back are supported, PPG taken from fingertip, and finger is at heart level
Device Device type Smartphone or wearables
Display type Application GUI displayed on the smartphone screen
Operating conditions Average room temperature (+20°C to +25°C) and humidity (30% to 50%)
Android application Android 8.0 or higher; controls user interactions, stores measurement results
ControlsCalibration, measurement, and history buttons
Sensor PPG sampling rate 100Hz to 200Hz
Platforms MAX30101/02, MAX86150
Perfusion index (PI) 0.1% to 5%

Factors That Can Affect BP Readings

The following factors alter BP readings significantly for cuff-based traditional BP devices and/or Maxim's PPG-based BP measurement system.

Blood Pressure Cuff Is Too Small

It is important to make sure that the proper size BP cuff is used on the subject's upper arm. In fact, many measurement errors occur because of not taking the time to determine if the patient's arm circumference falls within the range of indicators on the cuff. Studies have shown that using a too small of a cuff can cause a patient's systolic BP measurement to increase up to 10mmHg. (Maxwell)

Blood Pressure Cuff Used over Clothing

During a measurement, the cuff should always be placed directly on the subject's arm. Studies have shown that measurement over clothing or with tight clothing pushed up can cause significant errors in the BP measurement. (Reeves; Handler)

Subject Is Not in a Resting State

To obtain an accurate measurement, it is important that the subject relaxes quietly in a comfortable chair for at least 5 minutes before a reading is taken. Activities such as exercising, talking, drinking, or eating can affect the systolic BP by 10mmHg to 20mmHg. (Zheng)

Subject's Positioning

During the measurement, the subject should always be seated in a comfortable chair, legs uncrossed, with their back and arm supported. If the subject's back is not supported, the diastolic measurement may be increased by 5mmHg to 10mmHg. Crossing the legs has shown to raise the systolic BP by 2mmHg to 8mmHg. The positioning of the upper arm below the heart level will also result in higher measurement results, whereas positioning the upper arm above the heart level will result in lower BP values. These differences can increase/decrease the systolic BP 2mmHg for every inch above/below the heart level. (Perloff; O'Brien; Handler)

Emotional State

Stress or anxiety can cause large elevations in BP. If the BP measurement is taken while the subject is thinking about something that causes tension or stress, the BP levels could significantly increase. (Perloff)

Smoking/Alcohol/Caffeine

Consumption of tobacco products (cigarettes, cigars, smokeless tobacco), alcohol, or caffeine (sodas, coffee, tea) causes BP levels to spike. Therefore, the subject should refrain from smoking/alcohol/caffeine intake at least 30 minutes before a measurement is taken. (James; Marmot; Groppelli)

Temperature

BP tends to increase when the temperature is low in the measurement environment. (Alperovitch; Barnett)

Full Bladder

BP is lower when the bladder is empty. As the bladder gradually fills, BP increases. Studies have shown that systolic BP measurements can increase 10mmHg to 15mmHg when the subject has a full bladder. (Scultéty)

References/Other Resources

Chockalingam, Arun; Campbell, Norman R.; and J. George Fodor. "Worldwide epidemic of hypertension." The Canadian Journal of Cardiology. vol. 22, no. 7, 2006, p. 553.

Elgendi, Mohamed. "On the Analysis of Fingertip Photoplethysmogram Signals." Current Cardiology Reviews. vol. 8, no. 1, 2012, pp. 14–25.

Shin, Hangsik and Se Dong Min. "Feasibility study for the non-invasive blood pressure estimation based on PPG morphology: normotensive subject study." Biomedical Engineering Online. vol. 16, no. 1, 2017, p. 10.

Maxwell, Morton H.; Schroth, Philip C.; Waks, Abraham U.; Karam, Maroun; and Leslie P. Dornfeld. "Error in blood-pressure measurement due to incorrect cuff size in obese patients." The Lancet. vol. 320, no. 8288, 1982, pp. 33–36.

Handler, Joel. "The importance of accurate blood pressure measurement." The Permanente Journal. vol. 13, no. 3, 2009, p. 51.

Reeves, Richard A. "Does this patient have hypertension? How to measure blood pressure." JAMA. 1995, vol. 273, no. 15, pp. 1211–8.

Zheng, Dingchang; Giovannini, Roberto; and Alan Murray. "Effect of respiration, talking and small body movements on blood pressure measurement." Journal of Human Hypertension. vol. 26, no. 7, 2012, p. 458.

Perloff, Dorothee; Grim, Carlene; Flack, John; Frohlich, Edward D; Hill, Martha; McDonald, Mary; and Bruce Z. Morgenstern. "Human Blood Pressure Determination by Sphygmomanometry." Circulation. vol. 88, no. 5, 1993, pp. 2460–2470.

O'Brien, Eoin, et al. "Practice guidelines of the European Society of Hypertension for clinic, ambulatory and self blood pressure measurement." Journal of Hypertension. vol. 23, no. 4, 2005, pp. 697–701.

James, Jack E. "Critical review of dietary caffeine and blood pressure: a relationship that should be taken more seriously." Psychosomatic Medicine. vol. 66, no. 1, 2004, pp. 63–71.

Marmot, Michael G., et al. "Alcohol and blood pressure: the INTERSALT study." BMJ Clinical Research. vol. 308, no. 6939, 1994, pp. 1263–1267.

Groppelli, Antonella; Giorgi, Dante M.; Omboni, Stefano; Parati, Gianfranco; and Giuseppe Mancia. "Persistent blood pressure increase induced by heavy smoking." Journal of Hypertension. vol. 10, no. 5, 1992, pp. 495–499.

Alpérovitch, Annick; Lacombe, Jean-Marc; Hanon, Olivier; Dartigues, Jean François; Ritchie, Karen; Ducimetière, Pierre; and Christophe Tzourio. "Relationship between blood pressure and outdoor temperature in a large sample of elderly individuals: The Three-City study." Archives of Internal Medicine. vol. 169, no. 1, 2009, pp. 75–80.

Barnett, Adrian; Sans, Susana; Salomaa, Veikko; Kuulasmaa, Kari; and Annette J. Dobson (WHO Monica Project). "The effect of temperature on systolic blood pressure." Blood Pressure Monitoring. vol. 12, no. 3, 2007, pp. 195–203.

Scultety, S.; Varga, B.; and D. Szabo. "Effect of bladder distension on blood pressure." International Urology and Nephrology. vol. 3, no. 1, 1971, pp. 11–19.

 

 Read this Next

  MAXREFDES220#: Finger Heart Rate and Pulse Oximeter Smart Sensor with Digital Signal Processing