アプリケーションノート 5751

Compiling Meter Code with New Computation Engine (CE) Code Images


要約: This application note describes how to modify demo code or meter application code so it can be compiled and linked with new computation engine (CE) code images for the 71M6531/71M6532 and 71M6533/71M6534 and 71M6541/71M6542/71M6543 family of electricity metering ICs.

Introduction

Background

The 71M6531/71M6532 and 71M6533/71M6534 and 71M6541/71M6542/71M6543 families of electricity metering ICs are designed to be used with computation engine (CE) codes that can be adapted to the application at hand. In some cases, special CE codes are required and supplied by Maxim to support different sensor types or features such as filtering or harmonic analysis.
Since CE codes occupy different spaces in flash memory and XRAM, depending on the application, several steps are needed to accommodate a specific CE code image. This is done by modifying both the meter code (demo code or meter application code) sources and the Keil® compiler settings (Keil µVision® 4).
This application note discusses the necessary steps to successfully integrate a new CE code image into meter code. A general knowledge of the tools, i.e. Keil µVision and Signum Systems™ WEMU51 is helpful when performing the tasks described in this application note. Reading the software user guide (SUG) for the 71M653x and/or 71M654x ICs is recommended.

General Interface Between Meter Code and CE Code

How CE Code and CE Data Files Are Delivered

Source code for the CE is not available to the customer. CE code is delivered as a code image that is linked into the meter code flash image and then interpreted as CE op codes and executed by the CE at run time. When executing, the CE code needs certain registers in XRAM (CE RAM) to be initialized. For example, calibration coefficients for an uncalibrated (default) meter are set to 0x4000, and typically a standard value for WRATE is also part of the CE data image. The files for CE code that are delivered to the customer are the following:
  • CE code image (for example CE34B07G_ce.c): This code is for the 71M6534 or 71M6533, and its version is B07G.
  • CE data image (for example CE34B07G_dat.c): This set of data is for the code version B07G for the 71M6534 or 71M6533.
CE files are named with the leading characters “CE”, followed by two digits specifying the meter system-on-chip (SoC) family, e.g. “34” for the 71M6533 and 71M6534, or “41” for the 71M6541 and 71M6542. The next letter generally specifies the silicon revision (A, B, C, …) that the code is compatible with. The two digits after the revision letter are the code type. When a new code is developed with significantly different functionality, a new number is selected for these two digits. No features or functionality can be directly derived from the two digits. Typically, an application note provided with a CE code describes the features and usage of a particular code type. The letter after the two digits is the revision code of the particular code type. For example, revision “D” contains fixes for issues that were in revision “C”. When several revisions of the same code type are available, the latest revision should be used.
A portion of a typical CE code image is shown below:
// File: ce34a02d_ce.c
//                                                                          
// CE Program Image File (8051 C format)
const short code NumCeCode=1280;	// The number of words in the 'CeCode' array.
const unsigned char code CeCode[]={
 0x20,0xe3, 0x74,0x45, 0xec,0xff, 0x8c,0x45, 0x20,0xe4, 0x74,0x46, 0xed,0xff, 0x8c,0x46,
 0x20,0xe3, 0x74,0x45, 0xec,0xff, 0x8c,0x45, 0x20,0xe4, 0x74,0x46, 0xed,0xff, 0x8c,0x46,
 0x20,0xe3, 0x74,0x45, 0xec,0xff, 0x8c,0x45, 0x20,0xe4, 0x74,0x46, 0xed,0xff, 0x8c,0x46,
 0x20,0xe3, 0x74,0x45, 0xec,0xff, 0x8c,0x45, 0x20,0xe4, 0x74,0x46, 0xed,0xff, 0x8c,0x46,
 ...
 0x8f,0x05, 0x21,0x03, 0x8f,0x03, 0x21,0x04, 0x8f,0x04, 0x21,0x05, 0x8f,0x05, 0x20,0x03,
 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff,
 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff,
 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff,
 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff, 0xff,0xff
};
Two bytes (16 bits) combined form one op code for the CE. 0xFFFF is the op code for the STOP instruction.
A portion of a typical CE data image is shown below:
// File: ce34a02d_dat.c
//                                                                          
// CE Data Image File (8051 C format)
const short code NumCeData=268;	// The number of words in the 'CeData' array.
const unsigned char code CeData[]={
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0xff,0xff,0xff,0xff,
 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00,
 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x50,0x00, 0x00,0x00,0x00,0xab, 0x00,0x00,0x19,0x2c, 0x00,0x00,0x09,0xd8,
 0x01,0x6d,0x24,0x90, 0xff,0xff,0xff,0xff, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0xff,0xff,0xff,0xff,
 0xff,0xff,0xff,0xff, 0x63,0x65,0x33,0x34, 0x61,0x30,0x32,0x64, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x0c, 0x00,0x00,0x59,0xba, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x18,0x00, 0x00,0x00,0x09,0xd8, 0x00,0x00,0x00,0x00, 0xff,0xff,0xff,0xff,
 0x00,0x00,0x40,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x20,0x00,0x00,0x00, 0x20,0x00,0x00,0x00, 0x60,0x00,0x00,0x00,
 0x60,0x00,0x00,0x00, 0x00,0x00,0x80,0x00, 0x40,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 …
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00
};
CE data is organized in 4-byte (32-bit) words. These are fixed-point data and can be any type of data processed by the CE, such as calibration coefficients, constants, intermediate results, or output data.
Note the 0x40/0x00 byte combinations (shown in yellow) starting in line 5 of the data field. These are the default settings for the calibration coefficients located at CE data registers 0x0010 and up. The values are actually to be interpreted as 0x00004000. At startup, the essential part of the CE data image needs to be copied to XRAM, starting at address 0x0000, for the CE code to have valid data to work with. This is done by the meter code. Data towards the end of the CE data image is 0x00, and the meter code may take a shortcut by not copying the zero data to CE RAM.
Note that some CE codes have non-zero data towards the end of the data image and that a shortcut cannot be used for those codes. An example for this type of code is shown below (note the non-zero bytes marked in yellow embedded in zero bytes):
const short code NumCeData=414;	// The number of words in the 'CeData' array.
const unsigned char code CeData[]={
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0xff,0xff,0xff,0xff,
 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00,
 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00, 0x00,0x00,0x40,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x50,0x00, 0x00,0x00,0x00,0xe3, 0x00,0x00,0x19,0x2c, 0x00,0x00,0x08,0x88,
 0x01,0x6d,0x24,0x90, 0xff,0xff,0xff,0xff, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0xff,0xff,0xff,0xff, 0x63,0x65,0x33,0x34, 0x61,0x32,0x30,0x62, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x0c, 0x00,0x00,0x58,0xc1, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x18,0x00, 0x00,0x00,0x09,0xd8, 0x00,0x00,0x00,0x00, 0xff,0xff,0xff,0xff,
 0x00,0x00,0x40,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x20,0x00,0x00,0x00, 0x20,0x00,0x00,0x00, 0x60,0x00,0x00,0x00,
 0x60,0x00,0x00,0x00, 0xff,0xff,0xff,0xff, 0x00,0x00,0x80,0x00, 0x40,0x00,0x00,0x00,
 0x00,0x00,0x00,0x50, 0x00,0x00,0x00,0x03, 0x03,0x35,0x92,0x44, 0x02,0xfe,0xcc,0xc8,
 0x02,0xfe,0xcc,0xc8, 0x02,0xfe,0xcc,0xc8, 0x02,0xfe,0xcc,0xc8, 0x05,0x90,0x0e,0x98,
 0x05,0x59,0x49,0x1c, 0x05,0x90,0x0e,0x98, 0x05,0x90,0x0e,0x98, 0x05,0x90,0x0e,0x98,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x0d, 0x12,0xe0, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x01, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0xff,0xff,0xff,0xff, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
 0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,
};

Flash Memory of the 71M653x and 71M654x ICs Reserved for CE Code

The flash memory spans from 0x0000 to 0xFFFF for a product with 64KB flash, to 0x1FFFF for a 128KB product, and to 0x3FFFF for a 256KB product. The CE code image is placed somewhere in this range on a 1KB boundary (0x0400) by the linker and then found by the CE at run time using the CE_LCTN pointer in I/O RAM. CE_LCTN multiplied by 1024 (0x0400) yields the flash location of the CE code. It is advantageous to locate the CE code at the top end of the flash memory where it can grow in size without affecting other code. For large size CE codes, CE_LCTN must move to an address 1KB or 2KB lower, because the end of that particular CE code may exceed the end address of the code bank.
Sometimes the default settings of the meter code do not work, because the CE code is too large. The meter code’s defaults already have 25% extra space, especially to permit some growth. However, very large CE codes may need more than 25% extra space.
The size of the code is specified in the NumCeCode constant, which is part of the CE code image. NumCeCode is the actual number of CE instructions in the code. It is inserted in the _ce.c code file when the file is generated. For example, NumCeCode is 1950 for many standard 71M653x CE codes. Since CE code is structured in 16-bit words, this makes the overall length of the code 2 × 1950 = 3900 bytes. Complex CE codes typically are larger, such as CE34A20, which has 2235 words, or 4470 bytes.

RAM of the 71M653x and 71M654x ICs

RAM for the CE codes is located in general XRAM, which is shared between the CE and the microprocessing unit (MPU) in all 71M653x and 71M654x ICs.
The XRAM for the 71M653x spans from 0x0000 to 0x0FFF (4KB). XRAM for 71M654x ranges between 3KB (0x0000 to 0x0BFF) and 5KB (0x0000 to 0x13FF), depending on the part type.
In all 71M653x and 71M654x parts, the lowest XRAM locations, starting at 0x0000 are reserved for the ADC outputs and calibration coefficients, to be followed by the CE registers and transfer variables (for exact CE register locations, see the data sheet). Above that, CE code uses XRAM space for internal variables. It is important that there is no overlap between XRAM usage by the MPU and by the CE. The MPU should occupy the XRAM towards the upper addresses.
CE codes state their XRAM usage in the NumCeData constant, which is measured in 32-bit words. For example, 320 32-bit words will result in 1280 bytes (0x500).
At run time, i.e. when the meter code starts, the MPU copies the constants in the CE data image to XRAM as part of the initialization. CeData is the source address specified for this copy operation. Note that CeData is declared as const unsigned char code, which means that the data image is treated as code and consequently placed in flash memory by the linker. The MPU code can find the CE data image at the location that the linker puts it at.
Basically, the CE data image can be located anywhere in flash. However, 1KB boundaries (0x0400) are re-commended because the MPU code may want to update the image in flash, e.g. when the user wants to store the calibration and other parameters not in EEPROM but in flash. Erasing a whole flash page is straightforward, which is what must happen before the CE parameters are written to non-zero flash. Having the CE data image not cross page boundaries is advantageous: when the CE data image is updated to the flash memory, the read/write operation is simpler when the image is within a flash page boundary (see the data sheet for the meter SoC for details).

General Memory Map

Figure 1 shows the general memory map: flash memory contains the code for the MPU plus the code and data images for the CE. For the CE data image, there is a non-zero portion and a zero portion. At run time, both the MPU and CE operate out of flash memory. When the MPU code starts, it copies the CE data image into XRAM, which is shared between the CE and MPU.
The MPU code may choose to copy only the non-zero portion of the CE data image or to copy the whole CE data image.
Figure 1. General memory map.
Figure 1. General memory map.
Keil Compiler Settings
Using new CE code requires the code and data files, for example CE34B07G_ce.c and CE34B07G_dat.c, to be copied into the CE folder of the code folder environment. Demo code sources are supplied by Maxim in a fixed folder structure. The meter application code used by customers may have a similar structure. An example for a 71M6533 Demo Code folder structure is shown below.
71M6533 Demo Code folder structure
When we open the CE folder, we see the collection of CE codes and CE data images that were supplied as part of the demo code. Note that only one CE code image and one data image are typically used for a code build. We have to let the Keil µVision environment know which CE code images to use. This is done by selecting the CE group in the left panel (Project Panel) of the Keil µVision 4 graphical user interface (GUI), right clicking, and then selecting ‘Manage Components’. When the ‘CE’ entry under ‘Groups’ is selected, as shown in Figure 2, the available CE files show up in the right panel under ‘Files’.
Project Components
Figure 2. Project Components tab.
Pressing the button ‘Add Files’ opens a dialog box that allows for browsing to the physical location of the CE code and data images for selection and inclusion into the code build. After this, the ‘Close’ button of the browse dialog box must be clicked. The unneeded CE files should be removed by selecting their file names and by pressing the delete button in the right panel under ‘Files’.
Note: This operation only removes the file from the Keil project. The removed files are still physically present on the hard drive.
Another tab in ‘Options for Target’ in the Keil PK51 environment must be adapted to accommodate the CE code to be merged: The ‘Target’ tab has an area where the RAM space needed for the CE code needs defining. This entry allows the Keil PK51 compiler/linker to define where in XRAM variables and stack for the 80515 MPU can be located. The Figure 3 below shows entries 0x06A4 in the ‘Start’ and 0x096C in the ‘Size’ window. The entry 0x06A4 reserves 0x06A4 or 1700 decimal bytes in XRAM space, i.e. the range from 0x0000 to 0x06A3, for CE RAM usage and leaves the area from 0x06A4 to 0x0FFF (for a 4KB RAM size) for the MPU. The entry 0x06A4 corresponds to NumCeData multiplied by 4, since each CE register/word is equivalent to four bytes. The entry under ‘Size’ is the difference between the maximum available XRAM size (4KB, or 0x1000 in this example) and the address given under ‘Start’.
Note that for all 71M653x ICs and for the 71M654xG ICs ‘Code Banking’ is checked and the number of banks is properly selected, i.e. 8 for 256KB flash memory and 4 for 128KB.
Target tab
Figure 3. Target tab.
One nice thing about the settings in the Keil compiler is that they are reflected in the Keil project file (*.uv2, *.uvproj), once the project is saved. This means that copying the Keil project file guarantees that the settings are properly applied and do not require manually reentering.

General Settings for MPU Code

CE codes are generated for a specific setting of the analog front-end (AFE), i.e. the combination of sampling frequency, finite impulse response (FIR) filter length, number and sequence of sampled channels, and other parameters. In some cases, the MPU clock has to be adapted, also. Operating the CE code with an AFE setting other than the specified results in malfunction.
CE codes typically come either with an application note of their own or with a brief description of the required settings for the AFE. The settings specified by the application note or description MUST be implemented exactly by corresponding changes in the MPU source code.
Note that LSB values must be adapted in source code if the LSBs for Wh, VARh, VnSQSUM_X, InSQSUM_X, or other metrology parameters have changed with the new CE code.

Flash Memory Operations and CE Code

By design, operations by the MPU code on the flash memory require the CE to be disabled. This is achieved by clearing the CE_E bit (bit 3 at I/O RAM address 0x2000). After clearing this bit, a delay of a complete CE code run (e.g. 396µs for codes sampling at 2520Hz, 458µs for codes sampling at 2184Hz) is required to allow the CE to encounter the STOP command before commencing any flash operation.

71M653x Family of Electricity Metering ICs

CE Code Location

For 71M653x demo code (as of revision 4p7b), an instruction in main.c loads CE_LCTN with decimal 31, resulting in 0x400 * 31 = 0x7C00. Later, the pointer is reloaded in ce_30.c with CE_LCTN_ADR, which is defined in options.h as 0x78. This makes the final CE location in flash 0x78 * 0x400 = 0x1E000. As mentioned before, it is advantageous to locate the CE code at the top end of the flash memory where it can grow in size without affecting other code. For large size CE codes (i.e. if NumCeCode > 512), CE_LCTN has to point to an address 1KB or 2KB lower, i.e. CE_LCTN must be decremented by 1 or 2.
CE_LCTN points to the address where the CE code starts, i.e. the first instruction. Note that NumCeCode occupies two bytes that are not part of the code itself. This means that when the CE code image is placed using the linker settings of Keil PK51, the image location is CE_LCTN - 2.

CE Clock Rate and Code Length

The 71M653x electricity metering ICs can operate the CE at the standard 4.915MHz rate or at the double clock rate of 9.3804MHz (when the CE_10MHZ bit is set). The values for sample frequency (frame rate), executable CE code cycles, and CE clock rate cannot be arbitrary due to the fact that the CE must complete one code run during the time slot allocated for the multiplexer frame.
A typical frame duration is 396.729µs (for a sampling frequency of 2520.62Hz), and at 4.9152MHz CE clock rate (203ns per instruction), 1950 CE instructions fit into one frame. All CE codes that exceed 1950 instructions (or more than 3.8KB code size) must be operated at a CE clock rate of 9.8304MHz (101.5ns per instruction), which allows for up to 3900 instructions (equivalent to 7.6KB CE code size) into one frame.
Typical polyphase CE codes that include the sampling of the neutral current operate at 2184.53Hz or 457.76µs. These codes allow for the execution of 2255 instructions at 4.9152MHz CE clock rate.
Single-phase codes can have faster frame rates, e.g. 3276.8Hz, with 305.176µs per frame. These codes fit only 1500 instructions at 4.9152MHz or 3000 instructions at 9.8304MHz.
Knowledge of the relation between sample frequency (frame rate), CE code cycles, and CE clock rate helps the user understand how the CE_10MHZ bit should be set, if this is not already mentioned in the application note for the given CE code.
If the CE_10MHZ bit is set, the M40MHZ bit must also be set. This means that the MPU clock rate must be adjusted, and, therefore, the baud rates and timer constants should also all be adjusted.

Keil Settings

The entry shown in Figure 4 in the ‘BL51 Misc’ tab (accessible with ‘Options for Target’ in the Keil PK51 environment) allocates the space above 0xDFFE for the CE code image (CE34A20A_CE.C in this case). Note that BANK3 is used, which places the code at flash location 0x1DFFE.
Figure 4. BL51 Misc tab.
Figure 4. BL51 Misc tab.
The CE data image is typically placed 1024 bytes above that, at 0xEFFE, resulting in 0x1EFFE using BANK3. In the figure above, the CE data image has been selected to start at 0x1F200 (0x1F1FE + 2).
See Figure 5 and refer to Table 38 in the data sheet for the physical location of BANK 3:
Figure 5. 71M653X bank switching table.
Figure 5. 71M653X bank switching table.

CE Data

The same space considerations applied to NumCeCode apply to NumCeData: If NumCeData × 4 is larger than 1024, the code image must move down in flash by 1KB. In that case, CE_LCTN must be decremented also to avoid overlap of CE code and CE data in flash memory.
At run time, the constants in the CE data image are copied to XRAM as part of the initialization. The following code in ce_30.c performs the copy operation:
FL_BANK = BANK_CE;
        memcpy_cer (
        (int32x_t *) CE_DATA_BASE, (int32r_t *) CeData, min(CE_DATA_SIZE, NumCeData)
           );
       FL_BANK = saved_bank;
       }
CE_DATA_BASE is defined in ce653x.h as 0x0000. In this file, CE_DATA_SIZE is defined as 0x0140 32-bit words (= 0x0500). Note that the copy routine uses the minimum of CE_DATA_SIZE and NumCeData. This is because only the lower part of the CE code image needs to be copied using CE_DATA_SIZE, which is the count used to copy the essential data from the CE data image in flash to the CE data area in XRAM. The rest of the data area (i.e. up to the full NumCeData size is not copied and should work alright when it is just cleared to zero. The purpose for this partial copy operation is to reduce the flash size consumed by the CE data tables. The CE programmers typically move all the special starting values (non-zero values) within CE_DATA_SIZE.
Note: Some CE codes have non-zero CE data at the end of their CE data image. These must be copied by the MPU. In this case, using the minimum of the CE_DATA_SIZE and NumCeData is not the recommended procedure, and the copy routine should use NumCeData × 4.
If a larger CE XRAM usage is required, CE_DATA_SIZE needs to change.
CE codes with larger allocation for XRAM need the following changes:
  • ‘Target’ tab accessible with ‘Options for Target’ in the Keil PK51 environment must specify the XRAM space needed for the CE code.
  • CE_DATA_SIZE needs to be updated (ce653x.h).

Hardware Initialization in MPU Code

Initialization of the I/O RAM is done using the structure uint8r_t_ri_defaults[ ] in defaults.c. This structure consists of several segments that treat a number of I/O addresses starting at a given offset from 0x2000 (the base address for the I/O RAM). It helps to have the I/O RAM map from the Firmware Interface section of the data sheet to decipher the entries. Most entries are hard-coded, for example 0x34 for address 0x2001, which initializes SUM_CYCLES with 0x34, or 52 decimal. In conjunction with PRE_SAMPS (two bits, set to zero, resulting in a numerical value of 42), the resulting number of samples per accumulation interval is 42 × 52 = 2184.
Some of the entries are derived from definitions, such as EQUATION | CE_10MHZ at address 0x2000, which is the logical OR of EQUATION, as defined in options.h and CE_10MHZ, as defined in IO653X.h, or MPU_FREQ at address 0x2004, which is defined in OPTIONS_GBL.H.
The later segments, e.g. for the general-purpose input output (GPIO) configuration starting at I/O RAM address 0x2030, are not as critical for CE function. An example for uint8r_t_ri_defaults[ ] in defaults.c is given below:
uint8r_t ri_defaults[] =
{ //   0     1     2     3     4     5     6     7
   0x00, 0x10,                            // address and length
   EQUATION | CE_10MHZ, 0x34,             // 2000-2001
   0x03,                                  // 2002 enable xfer_busy, RTC interrupt.
   0x00, MPU_FREQ, CONFIG1_VAL, 0x00,     // 2003..6
   0x24,                                  // 2007 enable PLL_OK 0x24
   0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, // 2008-F. DIO Resources, etc.
   0x11, 0x01,                     // address and length, index 18
   0x40,                           // Default value for the analog clock adjustment
   0x1C, 0x03,                     // address and length, index 21
   0x04, 0x00, 0x00,               // Default value for PREG and QREG
   0x20, 0x0A,                     // address and length, index 26
   0x00, 0x23,                     // 2020-1.  all states, all on
   0x00, 0xE0, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,  // 2022-9
   0x30, 0x2B,                         // address and length; LCD buffer/ DIO outputs
   // Clear segments visible on LCD or not DIOs; Leave DIOs as outputs
   0x00, 0x00,                         // 2030..1=seg42,43
   0x80, 0x80, 0x80, 0x80, 0x00, 0x00, // 2030..7=seg44..49=dio24..29 
   0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x80, // 2038..F=seg50-57=dio30..37
   0x80, 0x80, 0x80, 0x80, 0x80, 0x00, 0x00, 0x00, // 2040..7=58..65=dio38..45
   0x00, 0x80, 0x00, 0x80, 0x80, 0x80, 0x80, 0x80, // 2048..F=66..73=dio46..53
   0x80, 0x80, 0x90, 0x90, 0x00, 0x00, 0x00, 0x00, // 2050..7=74..81=dio54..61
   0x00, 0x00, 0x00,                               // 2058..A=dio40,41,blink19&18
   0x60, 0x08,                                     // address and length
   0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, // 2060-7. RTM.
   0x70, 0x01,                                     // address and length
   0x00,                                           // 2070
   0x80, 0x02,                                // address and length
   0x4B, 0x51,                                // 2080-1. 10ms Pulse_Width, Pulse_Interval.
   0x90, 0x0B,                          // address and length
   0x10, 0x32, 0x54, 0x76, 0x98, 0x00,  // 2090 normal sequence
   0x1A, 0x3B, 0x54, 0x76, 0x98,        // Alt sequence reads temp, vbat and aux
   0x9D, 0x01,               // address and length
   0x07,                     // 209D: 6 states
   0xA7, 0x09,               // address and length
   0x00,                     // 20A7: boot size
   0x31, 0x00, 0x00,                  // 20A8-A. CE5, WAKE, TMUX.
   0x00, 0x22, 0x22, 0x00, 0x00,      // 20AB..F; differential, diff. chop enabled
   0xFD, 0x03,                        // address and length
   0x00, 0x00, 0x00,                  // 20FD-F. TRIMSEL, TRIMX, TRIM.
   0, 0 // ending record
};

Adapting Meter Code and Keil Settings for Larger or Smaller CE Codes and Data

CE codes with sizes larger than the size used for the existing build (as stated in NumCeCode) need the following adjustments:
  • Adjust CE_LCTN_ADR downwards
  • ‘Target’ tab accessible with ‘Options for Target’ in the Keil PK51 environment must specify the flash space needed for the CE code. This entry must correspond to the new choice of CE_LCTN_ADR.
CE codes with larger or smaller allocation for XRAM need the following changes:
  • ‘Target’ tab accessible with ‘Options for Target’ in the Keil PK51 environment must specify the XRAM space needed for the CE code.
  • ‘BL51 Misc’ tab accessible with ‘Options for Target’ in the Keil PK51 environment must specify the location in flash memory.
  • CE_DATA_SIZE needs to be updated in source code (ce653x.h).
  • CE code should be checked for the existence of data beyond CE_DATA_SIZE.
  • Move the location of the totals structure in meter.c in XRAM if CE data extends beyond 0x04FF.

Downloading Code to the 71M653x Flash Memory

CE codes that operate the CE at 10MHz require that the CE10MHZ bit (bit 3) at I/O RAM address 0x2000 is set while downloading code using the ADM51 ICE. The normal procedure before downloading code is to just clear the entire byte at 0x2000, which clears the CE_E bit (bit 4) in the process. For CE codes that operate the CE at 10MHz, it is helpful to write the value 0x08 into I/O RAM address 0x2000 before downloading code, which maintains the CE10MHZ bit (bit 3).

71M654x Family of Electricity Metering ICs

General Comments

The considerations for the 71M654x codes are very similar to the 71M653x codes. A typical CE code for the 71M6543 is shown below. Note that the same variable, NumCeCode, is used to specify the length of the code.
// File: ce43a22_ce.c
//                                                                          
// CE Program Image File (8051 C format)
const short code NumCeCode=1512;	// The number of words in the 'CeCode' array.
const unsigned char code CeCode[]={
 0xec,0xff, 0x20,0x48, 0x74,0xd8, 0x8c,0x48, 0x74,0xd8, 0x8c,0x48, 0x74,0xd8, 0x8c,0x48,
 0x74,0xd8, 0x8c,0x48, 0x74,0xd8, 0x8c,0x48, 0x74,0xd8, 0x8c,0x48, 0xed,0xff, 0x20,0x4c,
 0x74,0xd9, 0x8c,0x4c, 0x74,0xd9, 0x8c,0x4c, 0x74,0xd9, 0x8c,0x4c, 0x74,0xd9, 0x8c,0x4c,
 0x74,0xd9, 0x8c,0x4c, 0x74,0xd9, 0x8c,0x4c, 0x20,0x5c, 0x8f,0x74, 0x20,0x5e, 0x8f,0x76,
 0x20,0x60, 0x8f,0x78, 0x20,0x5d, 0x8f,0x7a, 0x20,0x5f, 0x8f,0x7b, 0x20,0x61, 0x8f,0x7c,
 0x26,0x20, 0x8f,0x38, 0xf0,0x38, 0x20,0x5d, 0x68,0x5f, 0x69,0x61, 0x8f,0x38, 0x20,0xf9,
 0x05,0xfa, 0x15,0xf9, 0x8f,0xf9, 0x20,0xfa, 0x05,0x38, 0x11,0xf9, 0x8f,0xfa, 0x20,0xb0,
 0xd0,0x4f, 0xf0,0xf9, 0x2b,0x4f, 0x8f,0x38, 0x30,0x38, 0x81,0x38, 0x30,0x38, 0x86,0x38,
 0x20,0x38, 0x00,0xb2, 0x87,0xb3, 0x8f,0xb2, 0xb7,0xb2, 0x20,0xb3, 0x00,0xb4, 0x8f,0x38,
In this example, the specified length of 1512 words amounts to 3024 bytes (0x0BD0 bytes). In the 71M654x ICs, the location for the CE code in flash is coded into I/O RAM address 0x2109 (CE_LCTN).
Figure 6 shows the relationship between code space, CE_LCTN pointer, and the entry in the Keil BL51 linker tab.
Figure 6. Relationship between code space, CE_LCTN pointer, and Keil BL51 linker.
Figure 6. Relationship between code space, CE_LCTN pointer, and Keil BL51 linker.
The code window from the Signum emulator for flash area 0xCFD0 to 0xD05F is shown in Figure 7. The entry 0x05E8 (1512 decimal) at location 0xCFFE corresponds to NumCeCode. The CE code image itself starts at location 0xD000.
Figure 7. Code window in the Signum emulator.
Figure 7. Code window in the Signum emulator.

CE Data Image

In the 71M654x demo codes, the CE data image is copied into XRAM by a routine in Main.c():
    // Set CE RAM to default.
    memcpy((uint8x_t*)CE_DATA_BASE, CeData, (4 * NumCeData));
As opposed to the 71M653x demo code, the 71M654x demo code does not base the copy operation on the minimum of CE_DATA_SIZE and NumCeData. The 71M654x demo code copies the whole data image, as defined by NumCeData into XRAM.

Adapting I/O RAM Locations

To establish the environment for the CE code, the I/O RAM entries controlling multiplexer settings, FIR length, gain control, input pin configuration (single-ended/differential), clock selection, etc. must be examined and changed, if necessary.
In the 71M654x demo codes, the I/O RAM registers are controlled by a structure named io_ram_table[]. This structure can be found in main.c and does not contain named elements, which means that the bytes must be counted manually starting at I/O RAM address 0x2100, to determine their meaning.
The listing on the following page shows default entries for a typical code and their meaning. The structure contains four bytes at the beginning that determine the start address (0x2100) and the length of the entries (0x0013).
Note that CE_LCTN is set at 0x03, which places the CE code image at 0x0C00 in flash memory. This is typical for Maxim 71M654x demo codes. Allocating a location in the lower range of the flash memory makes the code compatible with both the 32KB and 64KB flash size variants of the ICs.
const uint8r_t io_ram_table[] = 
{ 
// Configuration without M6000 (Remote sensor) 
   // Wh = max(VA * IA); IA is shunt 
   0x21, 0x00, 0x00, 0x13,                          // address (0x2100) and length (0x13 = 19 bytes decimal)
   0x01, 0x11, 0x11, 0x11, 0x12, 0xA0, 0x00, 0x09,  // MUX_DIV=0, MUX10_SEL=1, MUX7_SEL=1, MUX6_SEL=1,
                                                    // MUX5_SEL=1, MUX4_SEL=1
                                                    // MUX3_SEL=1, MUX2_SEL=2, MUX1_SEL=A, MUX0SEL=0
                                                    // EQU=0, no chop, no RTM, CE_E=0, SUM_SAMPS[12:8]=9
   0xD8, 0x03, 0x42, 0x5D, 0x3A, 0x00, 0x00, 0x01,  // SUM_SAMPS[7:0]=0xD8 ? SUM_SAMPS = 2520 decimal
                                                    // CE_LCTN=3, PLS_MAXWDTH = 0x42, PLS_INTERVAL = 0x5D ? 93 decimal
                                                    // DIFFn_E = 1, FIR_LEN = 01, RTM
   0x02, 0x03, 0x04,                                // RTM, last byte not used. There is no I/O RAM address 0x2112
   #if POWER_CONTROL 
   0x22, 0x00, 0x00, 0x01,                          // address (0x2200) and length (0x01) 
   0x32,                                            // Clocks: MCK=19.6608MHz, MPU=0.6644MHz, ADC=0.66MHz 
   #endif 
   0x21, 0x00, 0x00, 0x01,                          // address (0x2100) and length (0x01) 
   0x30,                                            // set mux_div after ADC

Adapting Meter Code and Keil Settings for Larger CE Codes and Data

CE codes with sizes larger than the size used for the existing build (as stated in NumCeCode) need the following adjustments:
  • Adjust the source code in main.c, byte CE_LCTN at 0x2109.
  • ‘Target’ tab accessible with ‘Options for Target’ in the Keil PK51 environment must specify the flash space needed for the CE code. This entry must correspond to the new choice of CE_LCTN.
  • The structure totals as used in the 71M653x codes has been renamed to reg_data for the 71M654x codes, which is part of the nvm_s structure. reg_data, is set to 0x2800, which is the start of the NV-RAM data field in I/O RAM.
CE codes with larger allocation for XRAM need the following changes:
  • ‘Target’ tab accessible with ‘Options for Target’ in the Keil PK51 environment must specify the XRAM space needed for the CE code.
  • CE_DATA_SIZE needs to be updated in source code (ce654x.h).
  • CE code should be checked for the existence of data beyond CE_DATA_SIZE.
Note the window for allocating code space in flash memory looks different for the 71M654x family compared to the 71M653x family (see Figure 8):
Figure 8. BL51 Locate window in Keil uVision 4.
Figure 8. BL51 Locate window in Keil µVision® 4.
Note that other fixed flash addresses are used in 71M654x demo code:
// Flash addresses.
#define FLASH_CE_CAL   0xfc00 // Address of CE calibration.
#define FLASH_MPU_CAL  0xf800 // Address of MPU calibration.
The flash address 0xFC00 is reserved for saving key CE parameters such as calibration coefficients, WRATE, CECONFIG, etc. with the ]U command.
The flash address 0xF800 is reserved for saving key MPU parameters, i.e. the parameters that can be entered by the user with the ‘)’ key word, e.g. when the user enters “)3=+2080” to set the IMAX value to 208A.
Care must be taken not to overlap CE code or data images with these fixed flash locations.

Troubleshooting

The code image generated with the techniques detailed above may not always work initially. Some troubleshooting tips are listed below.
A good approach to troubleshooting meter or demo code involves the following steps:
  1. Connect the ADM51 emulator to the target and start the WEMU51 application.
  2. Erase the target flash memory.
  3. Clear the XRAM space using the SET command of the emulator. For example, the command SET /MDATA 0 3FF 0 fills the XRAM memory from 0 to 0x3FF with zeroes.
  4. Load the generated code image into the flash using the File – Load command in WEMU51.
  5. Check the location of CE code image in the Program Window (Did the image load into the expected location?, Is the image complete? Is there any overlap?)
  6. Check the location of CE data image in the Program Window (Did the image load into the expected location? Is the image complete? Is there any overlap?)
  7. Click RES and then GO in the WEMU51 user interface. Allow the code run for 1 to 2 seconds, then halt the code execution by clicking on the STOP button.
  8. Examine the XRAM near 0x0000 in the Data Window. The code should now have copied the CE data image to XRAM. Addresses near 0x0000 are overwritten with the ADC samples, but addresses from 0x0010 and up should reflect the CE data image. Check if the complete data image has been copied, i.e. the range from 0x0000 to NumCeData or at least up to CE_DATA_SIZE).
  9. Examine the I/O RAM, i.e. addresses starting at 0x2000 (71M653x) or 0x2000 and 0x2100 (71M654x). Check if the pointer for the CE code location has been initialized properly (CE_LCTN).
  10. Examine the I/O RAM registers that control the AFE, such as MUX_DIV, SUM_PRE, multiplexer slot assignments, FIR_LEN, PRE_E, and control registers for differential/single-ended operation of analog pins. All settings must correspond to the settings specified in the application note for the CE code.
次のステップ
EE-Mail EE-Mail配信の登録申し込みをして、興味のある分野の最新ドキュメントに関する自動通知を受け取る。
Download ダウンロード、PDFフォーマット
© , Maxim Integrated Products, Inc.
このウェブサイトのコンテンツは米国および各国の著作権法によって保護されています。コンテンツの複製を希望される場合は お問い合わせください。.
APP 5751:
アプリケーションノート 5751,AN5751, AN 5751, APP5751, Appnote5751, Appnote 5751