アプリケーションノート 5151

Special Considerations for Mode Changes During Active Operation of MAX14820/MAX14821 Sensor/Actuator Transceivers

筆者: Shasta Thomas

要約: The MAX14820/MAX14821 are Maxim's first sensor/actuator transceivers designed for IO-Link® device applications. Both transceivers have an on-board C/Q driver that can be adjusted via the SPI™ interface during active operation. However, there are some special considerations that must be taken into account to avoid falsely detecting a wake-up event. This application note discusses those considerations.

The IO-Link Wake-Up Protocol

In an IO-Link system, communication between a master and a device is point-to-point, with the master sending a request message and the device responding to it. During startup, the IO-Link master initiates a special wake-up current pulse that lasts from 30µs to 160µs to initiate communication with the device, while auto-adjusting the data transmission rate and checking the device identification.
The MAX14820/MAX14821 are Maxim's first sensor/actuator transceivers designed for IO-Link device applications. In these applications, the MAX14820/MAX14821 act as the physical layer interface to a microcontroller running the data-link layer protocol. The transceivers detect IO-Link wake-up requests from an IO-Link master on the C/Q line and, in turn, generate a wake-up signal to the microcontroller using the active-low wake-up output pin (/WU\) output.

Normal Wake-Up Detection

The MAX14820/MAX14821 can detect a wake-up request from an I/O Link master when the C/Q line is shorted for 80µs (typ) in any of the programmable output modes (push-pull, PNP, or NPN). The /WU\ output pulses low for 190µs (typ) when a valid wake-up pulse is detected on the C/Q line, signaling to the microcontroller that a wake-up request has been received. Wake-up detection is functional as long as the C/Q driver is enabled.
Figure 1 shows normal wake-up functionality with C/Q in push-pull mode. The master holds the C/Q line during a TX_ pulse, triggering a wake-up pulse on the MAX14820/MAX14821. As shown here, the devices generate a pulse on the /WU\ output when a wake-up event is detected.
Figure 1. Valid wake-up detection in push-pull mode (R1 = TXEN, CH3 = C/Q, CH4 = current out of C/Q, CH2 = TXC = TXQ, CH1 = /WU\).
Figure 1. Valid wake-up detection in push-pull mode (R1 = TXEN, CH3 = C/Q, CH4 = current out of C/Q, CH2 = TXC = TXQ, CH1 = /WU\).

Special Considerations

In some cases, the MAX14820/MAX14821 may generate an unexpected wake-up pulse on the /WU\ output if the C/Q line is held high or low, due to downstream circuitry or a large line capacitance. One example of this might occur during a C/Q mode change. Figure 2 shows a situation when an unexpected wake-up might occur. C/Q is changed from push-pull to NPN mode using the SPI interface. The TX_ logic goes high for the wake-up request duration, but the C/Q line voltage drops very slowly due to a large capacitance on the line. The C/Q voltage does not fall below the 8V (min) driver output voltage low threshold during the TX_ pulse and falsely indicates that a wake-up event has occurred.
Figure 2. Unexpected wake-up pulse on active-low WU when changing from push-pull to NPN mode (R1 = SCLK, R2 = /CS\, CH1 = SDI, R3 = TXEN, CH3 = C/Q, CH2 = TXC = TXQ, CH4 = /WU\).
Figure 2. Unexpected wake-up pulse on active-low WU when changing from push-pull to NPN mode (R1 = SCLK, R2 = /CS\, CH1 = SDI, R3 = TXEN, CH3 = C/Q, CH2 = TXC = TXQ, CH4 = /WU\).
The wake-up detection circuitry on the MAX14820/MAX14821 cannot be disabled while the C/Q driver is enabled. However, some simple hardware or software adjustments can negate the effect of the wake-up detect during mode transitions.
A purely software response is to program the controller to ignore pulses on the /WU\ output immediately following a mode change, giving the line time to discharge before acknowledging wake-up events as valid.
To actually disable an unexpected wake-up pulse during this period requires a solution that includes both hardware and software changes. The C/Q driver can be enabled through either the TXEN input pin or by setting the C/QDEn bit in the CQConfig register, so both of these controls must be disabled during a mode change. To do this, follow the steps below:
  1. Pull the TXEN input pin low.
  2. Set the C/QDEn bit to 0.
  3. Change the C/Q transceiver mode.
  4. Wait before turning the transceiver on again (either by pulling TXEN high or by setting C/QDEn to 1). Calculate the required wait time, tDISCHARGE, following a mode transition using the following equation:
    tDISCHARGE = CLINE × (VCC - 8V)/[IDISCHARGE]
    where CLINE is the maximum expected capacitance on the C/Q line, and IDISCHARGE is the discharge rate of the line capacitance. If the C/Q driver is in a high-impedance state immediately following the mode transition, then IDISCHARGE is the weak pulldown current on the C/Q pin (100µA (min), 400µA (max)). To decrease the discharge delay, it is also possible to enable the 9mA (max) C/Q load current, disabling the load when the driver is re-enabled.
Figure 3 shows an example of a mode transition on C/Q while a large capacitance downstream on the C/Q line discharges. The C/QDEn bit is set to 0 during the mode-change software command and TXEN pulses low until after all expected TX_ pulses are finished. The C/Q driver is enabled again by pulling TXEN high after the voltage on the C/Q line has fallen below the 8V (min) threshold. Clearly, the device does not generate a pulse on /WU\ under these conditions.
Figure 3. Unexpected wake-up pulse on active-low WU when changing from push-pull to NPN mode (R1 = SCLK, R2 = /CS\, CH1 = SDI, R3 = TXEN, CH3 = C/Q, CH2 = TXC = TXQ, CH4 = /WU\).
Figure 3. Unexpected wake-up pulse on active-low WU when changing from push-pull to NPN mode (R1 = SCLK, R2 = /CS\, CH1 = SDI, R3 = TXEN, CH3 = C/Q, CH2 = TXC = TXQ, CH4 = /WU\).
次のステップ
EE-Mail EE-Mail配信の登録申し込みをして、興味のある分野の最新ドキュメントに関する自動通知を受け取る。
Download ダウンロード、PDFフォーマット
© , Maxim Integrated Products, Inc.
このウェブサイトのコンテンツは米国および各国の著作権法によって保護されています。コンテンツの複製を希望される場合は お問い合わせください。.
APP 5151:
アプリケーションノート 5151,AN5151, AN 5151, APP5151, Appnote5151, Appnote 5151