アプリケーションノート 4668

Proper Filtering and Grounding of DeepCover Secure Microcontroller (Zatara ZA9L0/ZA9L1) Devices

筆者: Reza Ahmadi

要約: This application note discusses grounding techniques for DeepCover® Secure Microcontrollers (Zatara® ZA9L0 and Zatara ZA9L1). Special attention is given to FCC Class B criteria. The sources of radiation are explained and methods to suppress unwanted radiation are introduced. The radiation test is done with the recommended design in a single-layer board and the test results are shown at the end.


この文書は極めて特定的なアプリケーションに向けて書かれたものであり、独自技術に関する情報を含んでいるため、その開示は該当アプリケーションに直接関わっているお客様のみに限定させていただいております。この文書を請求される方は以下のフォームに必要事項を記入してください。適当と判断された場合は2営業日以内にご連絡いたします。

以下の情報はすべて英語で記入してください。


アプリケーションノート 4668,AN4668, AN 4668, APP4668, Appnote4668, Appnote 4668