アプリケーションノート 4614

Hardware and Software Considerations for Interfacing a Thermal Printer to a Zatara Evaluation (EV) Kit

筆者: Reza Ahmadi

要約: This application note explains how to use the bus interface on the Zatara® series devices to connect an APS thermal printer to the evaluation (EV) board of DeepCover® Secure Microcontrollers (Zatara ZA9L0 or Zatara ZA9L1). The note also discusses some of the precautions and optimizations that need to be considered during the design of the driver.


この文書は極めて特定的なアプリケーションに向けて書かれたものであり、独自技術に関する情報を含んでいるため、その開示は該当アプリケーションに直接関わっているお客様のみに限定させていただいております。この文書を請求される方は以下のフォームに必要事項を記入してください。適当と判断された場合は2営業日以内にご連絡いたします。

以下の情報はすべて英語で記入してください。


アプリケーションノート 4614,AN4614, AN 4614, APP4614, Appnote4614, Appnote 4614