アプリケーションノート 4417

Transceiver IC Generates ±30V

筆者: Nick Allen-Rowlandson

要約: This application note explains how an RS-232 transceiver and a few external components can be combined to generate supply rails up to ±30V. The MAX202 transceiver is featured in the design.

This design idea appeared in the July 20, 2006 issue of Electronic Design magazine.

When applications require only a few millamps of supply current, an RS-232 transceiver IC (here, the MAX202) and a few external components can generate bipolar supply rails up to ±30V. This capability is useful in ±15V op-amp circuits that provide, for example, meter drive, LCD bias, and gas-detector bias.

In the standard application for which it was designed, the internal charge pump of the MAX202 generates ±10V for driving an RS-232 line. In Figure 1 the IC's transmit section drives an external charge pump that generates up to ±30V. Modifications allow the circuit to generate other voltages, such as ±20V. With the addition of external linear regulators it can produce ±15V for bipolar op-amp circuits.

Figure 1. This RS-232 transceiver drives an external charge pump, which provides ±30V supply voltages at a few milliamps.
Figure 1. This RS-232 transceiver drives an external charge pump, which provides ±30V supply voltages at a few milliamps.

The maximum operating frequency for the external charge pump is approximately 120kHz, so a JK flip-flop (or other divide-by-2 circuit connected between +5V and ground) is inserted in the oscillator line to lower the frequency applied to the pump. Lower voltages can be obtained (±20V, for example) by connecting the anode of D1 and the cathode of D2 to ground instead of ±10V.
次のステップ
EE-Mail EE-Mail配信の登録申し込みをして、興味のある分野の最新ドキュメントに関する自動通知を受け取る。
Download ダウンロード、PDFフォーマット
© , Maxim Integrated Products, Inc.
このウェブサイトのコンテンツは米国および各国の著作権法によって保護されています。コンテンツの複製を希望される場合は お問い合わせください。.
APP 4417:
アプリケーションノート 4417,AN4417, AN 4417, APP4417, Appnote4417, Appnote 4417