アプリケーションノート 4400

Pseudo Random Number Generation Using Linear Feedback Shift Registers


要約: Linear feedback shift registers are introduced along with the polynomials that completely describe them. The application note describes how they can be implemented and techniques that can be used to improve the statistical properties of the numbers generated.

Introduction

LFSRs (linear feedback shift registers) provide a simple means for generating nonsequential lists of numbers quickly on microcontrollers. Generating the pseudo-random numbers only requires a right-shift operation and an XOR operation. Figure 1 shows a 5-bit LFSR. Figure 2 shows an LFSR implementation in C, and Figure 3 shows a 16-bit LFSR implementation in 8051 assembly.

LFSRs and Polynomials

A LFSR is specified entirely by its polynomial. For example, a 6th-degree polynomial with every term present is represented with the equation x6 + x5 + x4 + x3 + x2 + x + 1. There are 2(6 - 1) = 32 different possible polynomials of this size. Just as with numbers, some polynomials are prime or primitive. We are interested in primitive polynomials because they will give us maximum length periods when shifting. A maximum length polynomial of degree n will have 2n - 1 different states. A new state is transitioned to after each shift. Consequently, a 6th-degree polynomial will have 31 different states. Every number between 1 and 31 will occur in the shift register before it repeats. In the case of primitive 6th-degree polynomials, there are only six. Table 1 lists all the primitive 6th-degree polynomials and their respective polynomial masks. The polynomial mask is created by taking the binary representation of the polynomial and truncating the right-most bit. The mask is used in the code that implements the polynomial. It takes n bits to implement the polynomial mask for an nth-degree polynomial.

Every primitive polynomial will have an odd number of terms, which means that every mask for a primitive polynomial will have an even number of 1 bit. Every primitive polynomial also defines a second primitive polynomial, its dual. The dual can be found by subtracting the exponent from the degree of the polynomial for each term. For example, given the 6th-degree polynomial, x6 + x + 1, its dual is x6-6 + x6-1 + x6-0, which is equal to x6 + x5 + 1. In Table 1, polynomials 1 and 2, 3 and 4, 5 and 6 are the duals of each other.

Table 2 lists the period of each different size polynomial and the number of primitive polynomials that exist for each size. Table 3 lists one polynomial mask for each polynomial of a different size. It also shows the first four values that the LFSR will hold after consecutive shifts when the LFSR is initialized to one. This table should help to ensure that the implementation is correct.

The Structure of a LFSR

LFSRs can never have the value of zero, since every shift of a zeroed LFSR will leave it as zero. The LFSR must be initialized, i.e., seeded, to a nonzero value. When the LFSR holds 1 and is shifted once, its value will always be the value of the polynomial mask. When the register is all zeros except the most significant bit, then the next several shifts will show the high bit shift to the low bit with zero fill. For example, any 8-bit shift register with a primitive polynomial will eventually generate the sequence 0x80, 0x40, 0x20, 0x10, 8, 4, 2, 1 and then the polynomial mask.

Generating Pseudo-Random Numbers with LFSR

In general, a basic LFSR does not produce very good random numbers. A better sequence of numbers can be improved by picking a larger LFSR and using the lower bits for the random number. For example, if you have a 10-bit LFSR and want an 8-bit number, you can take the bottom 8 bits of the register for your number. With this method you will see each 8-bit number four times and zero, three times, before the LFSR finishes one period and repeats. This solves the problem of getting zeros, but still the numbers do not exhibit very good statistical properties. Instead you can use a subset of the LFSR for a random number to increase the permutations of the numbers and improve the random properties of the LFSR output.

Shifting the LFSR more than once before getting a random number also improves its statistical properties. Shifting the LFSR by a factor of its period will reduce the total period length by that factor. Table 2 has the factors of the periods.

The relatively short periods of the LFSRs can be solved by XORing the values of two or more different sized LFSRs together. The new period of these XORed LFSRs will be the LCM (least common multiple) of the periods. For example, the LCM of a primitive 4-bit and a primitive 6-bit LFSR is the LCM(15, 63), which is 315. When joining LFSRs in this way, be sure to use only the minimum number of bits of the LFSRs; it is a better practice to use less than that. With the 4- and 6-bit LFSRs, no more than the bottom 4 bits should be used. In Figure 2, the bottom 16 bits are used from 32- and 31-bit LFSRs. Note that XORing two LFSRs of the same size will not increase the period.

The unpredictability of the LFSRs can be increased by XORing a bit of "entropy" with the feedback term. Some care should be taken when doing this—there is a small chance that the LFSR will go to all zeros with the addition of the entropy bit. The zeroing of the LFSR will correct itself if entropy is added periodically. This method of XORing a bit with the feedback term is how CRCs (cyclic redundancy checks) are calculated.

Polynomials are not created equal. Some polynomials will definitely be better than others. Table 2 lists the number of primitive polynomials available for bit sizes up to 31 bits. Try different polynomials until you find one that meets your needs. The masks given in Table 3 were randomly selected.

All the basic statistical tests used for testing random number generators can be found in Donald Knuths, The Art of Computer Programming, Volume 2, Section 3.3. More extensive testing can be done using NIST's Statistical Test Suite. NIST also has several publications describing random number testing and references to other test software.

Figure 1. Simplified drawing of a LFSR.
Figure 1. Simplified drawing of a LFSR.

Figure 2. C code implementing a LFSR.
Figure 2. C code implementing a LFSR.

Figure 3. 8051 assembly code to implement a 16-bit LFSR with mask 0D295h.
Figure 3. 8051 assembly code to implement a 16-bit LFSR with mask 0D295h.

Table 1. All 6th-Degree Primitive Polynomials
  Irreducible Polynomial In Binary Form Binary Mask Mask
1
x6 + x + 1
1000011b
100001b
0x21
2
x6 + x5 + 1
1100001b
110000b
0x30
3
x6 + x5 + x2 + x + 1
1100111b
110011b
0x33
4
x6 + x5 + x4 + x + 1
1110011b
111001b
0x39
5
x6 + x5 + x3 + x2 + 1
1101101b
110110b
0x36
6
x6 + x4 + x3 + x + 1
1011011b
101101b
0x2D

Table 2. Polynomial Information
Degree Period Factors of Period No. of Primitive Polynomials of This Degree
3
7
7
2
4
15
3, 5
2
5
31
31
6
6
63
3, 3, 7
6
7
127
127
18
8
255
3, 5, 17
16
9
511
7, 73
48
10
1,023
3, 11, 31
60
11
2,047
23, 89
176
12
4,095
3, 3, 5, 7, 13
144
13
8,191
8191
630
14
16,383
3, 43, 127
756
15
32,767
7, 31, 151
1,800
16
65,535
3, 5, 17, 257
2,048
17
131,071
131071
7,710
18
262,143
3, 3, 3, 7, 19, 73
7,776
19
524,287
524287
27,594
20
1,048,575
3, 5, 5, 11, 31, 41
24,000
21
2,097,151
7, 7, 127, 337
84,672
22
4,194,303
3, 23, 89, 683
120,032
23
8,388,607
47, 178481
356,960
24
16,777,215
3, 3, 5, 7, 13, 17, 241
276,480
25
33,554,431
31, 601, 1801
1,296,000
26
67,108,863
3, 2731, 8191
1,719,900
27
134,217,727
7, 73, 262657
4,202,496
28
268,435,455
3, 5 29, 43, 113, 127
4,741,632
29
536,870,911
233, 1103, 2089
18,407,808
30
1,073,741,823
3, 3, 7, 11, 31, 151, 331
17,820,000
31
2,147,483,647
2147483647
69,273,666
32
4,294,967,295
3, 5, 17, 257, 65537
Not Available

Table 3. Sample Masks and First Four Values Output after Initializing LFSR with One
Degree Typical Mask First Four Values in LFSR After Consecutive Shifts
3
0x5
0x5
0x7
0x6
0x3
4
0x9
0x9
0xD
0xF
0xE
5
0x1D
0x1D
0x13
0x14
0xA
6
0x36
0x36
0x1B
0x3B
0x2B
7
0x69
0x69
0x5D
0x47
0x4A
8
0xA6
0xA6
0x53
0x8F
0xE1
9
0x17C
0x17C
0xBE
0x5F
0x153
10
0x32D
0x32D
0x2BB
0x270
0x138
11
0x4F2
0x4F2
0x279
0x5CE
0x2E7
12
0xD34
0xD34
0x69A
0x34D
0xC92
13
0x1349
0x1349
0x1AED
0x1E3F
0x1C56
14
0x2532
0x2532
0x1299
0x2C7E
0x163F
15
0x6699
0x6699
0x55D5
0x4C73
0x40A0
16
0xD295
0xD295
0xBBDF
0x8F7A
0x47BD
17
0x12933
0x12933
0x1BDAA
0xDED5
0x14659
18
0x2C93E
0x2C93E
0x1649F
0x27B71
0x3F486
19
0x593CA
0x593CA
0x2C9E5
0x4F738
0x27B9C
20
0xAFF95
0xAFF95
0xF805F
0xD3FBA
0x69FDD
21
0x12B6BC
0x12B6BC
0x95B5E
0x4ADAF
0x10E06B
22
0x2E652E
0x2E652E
0x173297
0x25FC65
0x3C9B1C
23
0x5373D6
0x5373D6
0x29B9EB
0x47AF23
0x70A447
24
0x9CCDAE
0x9CCDAE
0x4E66D7
0xBBFEC5
0xC132CC
25
0x12BA74D
0x12BA74D
0x1BE74EB
0x1F49D38
0xFA4E9C
26
0x36CD5A7
0x36CD5A7
0x2DABF74
0x16D5FBA
0xB6AFDD
27
0x4E5D793
0x4E5D793
0x6973C5A
0x34B9E2D
0x5401885
28
0xF5CDE95
0xF5CDE95
0x8F2B1DF
0xB25867A
0x592C33D
29
0x1A4E6FF2
0x1A4E6FF2
0xD2737F9
0x1CDDF40E
0xE6EFA07
30
0x29D1E9EB
0x29D1E9EB
0x3D391D1E
0x1E9C8E8F
0x269FAEAC
31
0x7A5BC2E3
0x7A5BC2E3
0x47762392
0x23BB11C9
0x6B864A07
32
0xB4BCD35C
0xB4BCD35C
0x5A5E69AE
0x2D2F34D7
0xA22B4937