Adding current-limiting circuitry to an emitter follower protects both the pass transistor and downstream circuitry from excessive current damage. The classic way to implement such current limiting is to add a ballast resistor between the pass transistor's emitter and the circuit output, and then monitor the resistor drop with a small-signal transistor. See R4 and Q2 in the power amplifier (or linear regulator) shown in
Figure 1.
Figure 1. A small-signal transistor (Q2) provides an output current limit for this power amplifier.
Unfortunately, the base-emitter voltage of the small-signal transistor sets the current-limit threshold for this circuit. That V
BE has a well-known temperature coefficient of -2mV/°C, which causes a substantial change in current limit across the operating temperature range.
An adjustable shunt regulator (U1 in
Figure 2) is preferable to the small-signal transistor for sensing current. This IC is chosen for its low-input threshold (0.6V), which is lower than that of common shunt regulators (1.25V to 2.5V). In addition, the IC's separate power-supply input allows it to maintain accuracy as the internal output transistor approaches saturation.
Figure 2. Substituting a shunt regulator (U1) for Q2 in the Figure 1 circuit improves the current-limit accuracy.
Figure 3 compares current-limit accuracies of the small-signal-transistor version of Figure 1 with the shunt-regulator version of Figure 2. The transistor version exhibits a 25% change in current-limit threshold over the operating temperature range, while the shunt-regulator provides better than 2% accuracy over that range (neglecting the temperature coefficients of the sense resistors).
Figure 3. Current-limit accuracy versus temperature for the circuits of Figure 1 (top trace) and Figure 2 (bottom trace).
A similar article appeared as a Design Idea in the February 2, 2006 edition of
EDN.
© , Maxim Integrated Products, Inc.
|
このウェブサイトのコンテンツは米国および各国の著作権法によって保護されています。コンテンツの複製を希望される場合は
お問い合わせください。.
APP 3867:
アプリケーションノート
3867,
AN3867,
AN 3867,
APP3867,
Appnote3867,
Appnote 3867
|
maxim_web:en/products/interface/signal-line-protection-ics,maxim_web:en/products/power,maxim_web:en/products/analog/amps
maxim_web:en/products/interface/signal-line-protection-ics,maxim_web:en/products/power,maxim_web:en/products/analog/amps