アプリケーションノート 3643

How to Use the DS1678 Real-Time Event Recorder


要約: This note demonstrates an application using the DS1678 real-time event recorder. The software example includes basic operating routines. A schematic of the application circuit is included.

DS1678 Pin Assignment
DS1678 Pin Assignment

Description

This application note demonstrates how to use the DS1678 real-time event recorder which logs events—level transitions on the INT input pin—into a 1024-word datalog memory array. The first event is recorded as a time stamp; subsequent events are recorded as elapsed time from the previous event. The time stamp and 1024-word datalog memory accommodate up to 1025 recorded events.

This example code includes functions for initiating a datalogging "mission." The user-selectable options are event resolution, trigger selection, and rollover (handling missions of more than 1025 events). The software also includes routines for ending a mission, for displaying the event datalog information, and for writing and reading the user RAM.

Operation

The program uses two general-purpose port pins (GPIOs) on a microcontroller to communicate with the DS1678 through the DS1678's I²C serial interface. An additional port pin is used to toggle the DS1678's INT input to drive events. In a typical application, the INT input would be connected to circuitry that conditions the signals from the event source, e.g., a thermostat in a HVAC system. This connection allows the DS1678 to record, for example, the start time and duration of each cooling or heating cycle.

This example uses an 8051-compatible microcontroller, the DS2250. User inputs and data outputs from the program are passed through an RS-232 interface from a terminal emulator program on a PC to a UART on the microcontroller. The Microcontroller Tool Kit software utility can be used to program the DS2250 microcontroller.

The software is shown in Figure 1. A schematic of the circuit is shown in Figure 2.

Figure 1. Program listing for interfacing a microcontroller to the DS1678.
Download

Figure 1. Program listing for interfacing a microcontroller to the DS1678.

Figure 2. Schematic for the DS1678 demonstration board.
For Larger Image

Figure 2. Schematic for the DS1678 demonstration board.

サンプル
DS1678 無料サンプル
次のステップ
EE-Mail EE-Mail配信の登録申し込みをして、興味のある分野の最新ドキュメントに関する自動通知を受け取る。
Download ダウンロード、PDFフォーマット
© , Maxim Integrated Products, Inc.
このウェブサイトのコンテンツは米国および各国の著作権法によって保護されています。コンテンツの複製を希望される場合は お問い合わせください。.
APP 3643:
アプリケーションノート 3643,AN3643, AN 3643, APP3643, Appnote3643, Appnote 3643