Systems such as laptop computers and other devices that have internal charge circuitry require a precise bi-directional current-sense amplifier to monitor accurately the battery's current regardless of polarity. The MAX4377 (a dual low-cost current-sense) can be used to produce a bi-directional current monitor.
Figure 1.
Output voltage OUT_ is proportional to the magnitude of the sense voltage (V
RS+ - V
RS-).
OUT_ is approximately zero when V
RS- > V
RS+.
When V
RS+ > V
RS-, V
OUT = (GAIN)(R
SENSE)(I
LOAD)
where GAIN = 20 for MAX4377T.
For example, R
SENSE = 100mΩ and I
LOAD = 1A produce, in the case of the MAX4377T, a full-scale output of 2V. However this circuit needs a two channel ADC in order to evaluate the charge and discharge currents. Simply adding a differential amplifier such as the MAX4198 produces a circuit with a single output able to provide the information of charge or discharge current.
Figure 2.
The output V
OUT will be (OUT2 - OUT1) + REF. Using a REF voltage of 2.5V we obtain an output swing from 0.5V to 4.5V (from 2.5V to 4.5V for discharge current and from 2.5V to 0.5V for charge current).
New bi-directional current-sense amplifiers such as the MAX4070, include the differential amplifier and reference on-chip.
A similar version of this article appeared in the September 2, 2002 issue of
Mundo Electronico magazine.
© , Maxim Integrated Products, Inc.
|
このウェブサイトのコンテンツは米国および各国の著作権法によって保護されています。コンテンツの複製を希望される場合は
お問い合わせください。.
APP 1949:
アプリケーションノート
1949,
AN1949,
AN 1949,
APP1949,
Appnote1949,
Appnote 1949
|
maxim_web:en/products/analog/amps,maxim_web:en/products/power/battery-management,maxim_web:en/products/power/battery-management/battery-fuel-gauges
maxim_web:en/products/analog/amps,maxim_web:en/products/power/battery-management,maxim_web:en/products/power/battery-management/battery-fuel-gauges