Get Technical Tips from Maxim Unfiltered Videos

March 07, 2018

Christine Young By: Christine Young
Blogger, Maxim Integrated 

 

You're on a tight project deadline and you've got some questions on how to set up the real-time clock (RTC) circuit. Or you need some pointers on configuring the microcontroller for a particular mode. Maybe you want to learn more about setting up a chip so that it can communicate with a PC.

Did you know that Maxim has a YouTube playlist devoted to quick technical tips and tricks? The “Maxim Unfiltered” playlist features short videos, all under five minutes, with our engineers sharing their expertise.

How to Set Up the DS1922 Thermochron

See how you can use OneWireViewer software to get the DS1922 iButton to communicate with a PC.


DS1922 ThermochronをOneWireViewerでセットアップする方法
4:50 November 10, 2017

How to Measure Temperature in Portable Projects II – Using the MAX17055 Fuel Gauge

Get some tips on adding temperature measurement to wearable electronic designs. The video also presents an evaluation of the MAX17055 fuel gauge IC, which features an internal temperature sensor and thermistor-driving interface.


携帯プロジェクトで温度を測定する方法II – 残量ゲージMAX17055を使用(日本語字幕)
3:12 November 13, 2017

How to Configure a Microcontroller for Deep Sleep Using the MAX32630

Learn more about designing with the MAX32630 ultra-low-power, high-performance Arm® Cortex®-M4F microcontroller for wearables. This IC, which features a floating-point unit, features four flexible power modes, a peripheral management unit, built-in dynamic clock gating, and firmware-controlled power gating.


MAX32630を使ってマイクロコントローラをディープスリープに設定する方法
4:31 March 05, 2018

Bookmark this playlist, as we’ll continue to upload new videos. And just let us know if there’s a video topic you’d like us to cover.