アプリケーションノート429

Programmable-Gain Amplifier, Using the MAX532 DAC


Abstract: This application note discusses how to use the MAX532 to build a programmable gain amplifier (PGA) that's suitable for AC gain control. No external components are necessary. Equations are provided to easily calculate the output values.

The MAX532 is a dual, 12-bit, voltage-output DAC. Access to the output amplifier's input terminals allows it to be easily configured as a programmable-gain amplifier (PGA) suitable for AC gain control.

The circuit configuration is that of an inverting amplifier, with R2 replaced by the effective resistance of the DAC ladder (Figure 1) and R1 replaced by internal feedback resistor RFB (Figure 2). In this circuit, an AC signal is applied to the feedback resistor input and the output signal is tied to the DAC reference input. The maximum signal at VOUT is limited by the amplifier's headroom from the supply rails (±12V to ±15V), which must be a minimum of 2.5V from either rail.

Figure 1. Fixed-gain inverting amplifier.
Figure 1. Fixed-gain inverting amplifier.

Figure 2. Programmable-gain amplifier.
Figure 2. Programmable-gain amplifier.

The DAC functions as a programmable resistor in the feedback of the amplifier such that :

VOUT/VIN = -R(DAC)/RFB,

where R(DAC) is the resistance of the DAC ladder and RFB is the value of the feedback resistor, which is R/2.

R(DAC) = R/2×[4096/(DAC CODE)], with the DAC CODE given as a decimal value. As the code decreases, the effective DAC resistance increases, and so the gain increases. The transfer function for the circuit is thus:



The code can be programmed between 1 and full scale (212-1). Zero code is not allowed, as it results in the DAC's appearing as an open circuit in the feedback loop.



関連製品
MAX532 デュアル、シリアル入力、電圧出力、乗算型12ビットDAC 無料
サンプル
 


次のステップ
EE-Mail EE-Mail配信の登録申し込みをして、興味のある分野の最新ドキュメントに関する自動通知を受け取る。
ダウンロード ダウンロード、PDFフォーマット (26kB)  

© Nov 01, 2000, Maxim Integrated Products, Inc.
このウェブサイトのコンテンツは米国および各国の著作権法によって保護されています。コンテンツの複製を希望される場合は、お問い合わせください

APP 429: Nov 01, 2000
アプリケーションノート429, AN429, AN 429, APP429, Appnote429, Appnote 429