アプリケーションノート3532

High-Power LED Driver Accepts Wide Input-Voltage Range


Abstract: Circuit based on a buck/boost converter controller regulates current to a white LED, despite an allowed variation of input voltage from 2.7V to 16.5V.

A similar version of this article appeared as a Design Brief in the January 20, 2005 issue of Electronic Design magazine.

The advent of high-power LEDs capable of replacing incandescent bulbs has produced a need for circuits that efficiently match the LEDs to available power sources (batteries, car electrical systems, etc.). The circuits should also be able to regulate and control the LED light output, despite variations in output voltage from the power source.

The circuit of Figure 1 starts and operates a 1A LED from a voltage that ranges from 2.7V minimum (the end of life for three alkaline primary cells) to 16.5V maximum (the maximum voltage for 12V automobile systems). Operation over that range is stable and smooth, even with more than 1Ω of internal resistance at the power source.

Figure 1. Wide input-voltage range, high-power LED driver.
Figure 1. Wide input-voltage range, high-power LED driver.

An inductive, buck-boost converter controller (IC1) with external MOSFET power switch is setup in a current-regulation loop using a 0.1Ω current-sense resistor in series with the power LED. (If the output circuit opens, the 6.2V Zener diode turns on, starting a voltage regulation loop.) Figure 2 shows the current regulation for 0.5A and 1A output currents, and Figure 3 shows the corresponding efficiencies, all plotted vs. the operating range of input voltage.

Figure 2. LED current vs. supply voltage for the Figure 1 circuit.
Figure 2. LED current vs. supply voltage for the Figure 1 circuit.

Figure 3. Efficiency vs. supply current for the Figure 1 circuit.
Figure 3. Efficiency vs. supply current for the Figure 1 circuit.

Replacing the 10kΩ feedback resistor (connected to the current-sense resistor) with a linear potentiometer of the same value enables efficient dimming of the LED. Starting from the maximum 1A regulation point set by the circuit values shown, the power-LED current (and hence its light output) can then be linearly swept through a range of more than 20:1.

関連製品
MAX774 -5V/-12V/-15Vまたは可変、高効率、低IQ、反転DC-DCコントローラ 無料
サンプル
 


次のステップ
EE-Mail EE-Mail配信の登録申し込みをして、興味のある分野の最新ドキュメントに関する自動通知を受け取る。
ダウンロード ダウンロード、PDFフォーマット (70kB)  

© Jun 15, 2005, Maxim Integrated Products, Inc.
このウェブサイトのコンテンツは米国および各国の著作権法によって保護されています。コンテンツの複製を希望される場合は、お問い合わせください

APP 3532: Jun 15, 2005
アプリケーションノート3532, AN3532, AN 3532, APP3532, Appnote3532, Appnote 3532