アプリケーションノート3209

Protecting Against Momentary Power Loss Due to Battery-Bounce


Abstract: Impact or vibration can cause momentary interruptions when batteries lose contact. To ensure continuity of power in battery-powered systems, add this three-IC circuit.

When you drop a battery-powered device, the impact can open internal contacts for as long as 10ms, producing a momentary loss of power that can cause a false low-battery indication. (There is sometimes a similar momentary effect on the device's owner, especially if the device is expensive, but that's beyond the scope of this application note).

You can insure continuity of power by adding a large capacitor across the battery. The capacitor must provide a certain amount of voltage headroom as margin against the discharge of load current. The capacitor voltage varies with discharge current as dV = Idt/C, so insufficient headroom calls for an even larger capacitor.

Another problem is that large capacitors tend to be leaky. Capacitor leakage is usually not a problem during normal operation, but during "sleep mode" it can be a substantial fraction of the total quiescent current and can cause a significant reduction in battery life.

The circuit of Figure 1 solves all these problems. Two AA batteries provide 3V power, which is boosted to 3.3V by a stepup dc-dc converter (U3). The large reserve capacitor of 2mF or 4mF is charged from the 3.3V output via a SPST CMOS analog switch (U1). The output of this 175Ω switch charges the reserve capacitor and drives the input of a low-dropout linear regulator (U2).

Figure 1. This circuit removes discontinuities in power by backing up the battery (two AA cells) with charge on a reserve capacitor.
Figure 1. This circuit removes discontinuities in power by backing up the battery (two AA cells) with charge on a reserve capacitor.

U2's output is set to provide 1.68V when the battery is removed. The output is also divided down by the 80k/120k divider to trip an internal comparator connected to the low-battery input (LBI). The comparator's open-drain output (LBO) feeds back to U1's digital input (DIN), which turns the switch on (high) and off (low).

Figures 2-5 show the circuit performance for different values of reserve capacitor and load current. Figures 5-6 remove switch-response time by wiring the switch in the ON position.

Figure 2. Figure 1 circuit with 4mF reserve capacitor and 100µA load: after removing the battery, power remains for 8.7s
Figure 2. Figure 1 circuit with 4mF reserve capacitor and 100µA load: after removing the battery, power remains for 8.7s.

Figure 3. Figure 1 circuit with 4mF reserve capacitor and 100mA load: after removing the battery, power remains for 10.8ms.
Figure 3. Figure 1 circuit with 4mF reserve capacitor and 100mA load: after removing the battery, power remains for 10.8ms.

Figure 4.   Figure 1 circuit with 2mF reserve capacitor and 100µA load: after removing the battery, power remains for 1.48s.
Figure 4. Figure 1 circuit with 2mF reserve capacitor and 100µA load: after removing the battery, power remains for 1.48s.

Figure 5. Figure 1 circuit with 2mF reserve capacitor and 100mA load: after removing the battery, power remains for 920µs.
Figure 5. Figure 1 circuit with 2mF reserve capacitor and 100mA load: after removing the battery, power remains for 920µs.

Figure 6. Figure 1 circuit with 2mF reserve capacitor, 100µA load, and switch wired closed: after removing the battery, power remains for 544ms.
Figure 6. Figure 1 circuit with 2mF reserve capacitor, 100µA load, and switch wired closed: after removing the battery, power remains for 544ms.

Figure 7. Figure 1 circuit with 2mF reserve capacitor, 100mA load, and switch wired closed: after removing the battery, power remains for 1.08ms.
Figure 7. Figure 1 circuit with 2mF reserve capacitor, 100mA load, and switch wired closed: after removing the battery, power remains for 1.08ms.



関連製品
MAX1674 高効率、低消費電流、小型、ステップアップDC-DCコンバータ 無料
サンプル
 
MAX4501 低電圧、SPST、CMOSアナログスイッチ 無料
サンプル
 
MAX882 スタンバイモード付き、5V/3.3Vまたは可変、低ドロップアウト、低IQ、200mAリニアレギュレータ 無料
サンプル
 


次のステップ
EE-Mail EE-Mail配信の登録申し込みをして、興味のある分野の最新ドキュメントに関する自動通知を受け取る。
ダウンロード ダウンロード、PDFフォーマット (132kB)  

© Jun 21, 2004, Maxim Integrated Products, Inc.
このウェブサイトのコンテンツは米国および各国の著作権法によって保護されています。コンテンツの複製を希望される場合は、お問い合わせください

APP 3209: Jun 21, 2004
アプリケーションノート3209, AN3209, AN 3209, APP3209, Appnote3209, Appnote 3209