アプリケーションノート298

Current-Limit Switch Is Digitally Programmable


Abstract: Current-limit switches are virtually ubiquitous in system controls. They provide a safe means for regulating the current delivered to a load circuit. The switches allow the load current to increase to a programmed limit but no higher. This application note illustrates the implementation of a digitally programmable current-limit switch using MAX890L a current-limited, high-side P-channel switch and MAX5160 digital potentiometer

Additional Information: Current-limit switches are virtually ubiquitous in system controls. They provide a safe means for regulating the current delivered to a load circuit. The switches allow the load current to increase to a programmed limit but no higher. Typically, the current limit is a function of the voltage across an external resistor, produced by the current from a fixed source internal to the switch IC. This voltage serves as the reference for an internal current-limiting amplifier. By replacing the resistor with a digital potentiometer, you can easily program the current limit (see the figure below). IC1 is a current-limit switch with a maximum programmable limit of 1A. The limit equals 1380/RSET, where RSET is the resistance between pins 5 and 6 of IC2. IC2 is a 50kΩ digital potentiometer whose resistance is programmable in 32 equal increments. With active-low CS held low, high-to-low transitions at active-low INC(pin 1) increments IC2's internal counter.

Figure 1. You can program a current limit to 1A in 32 equal increments by using a digital potentiometer.
Figure 1. You can program a current limit to 1A in 32 equal increments by using a digital potentiometer.

These transitions increase the resistance between W and L when U/active-low D is low and reduce it when U/active-low D is high. IC1 includes a thermal-shutdown capability that turns the load current completely off when the chip temperature exceeds 135°C. It restores the load current when the temperature cools by 10°C. If the short-circuit fault is still present, the switch cycles off and on, yielding a pulsed load current. An open-drain fault output (pin 8) switches low when the load demands current beyond the programmed limit, enabling an external system to monitor the condition of the current switch.

A similar version of this article appeared in the August 17, 2000 issue of EDN.



関連製品
MAX5160 低電力デジタルポテンショメータ 無料
サンプル
 
MAX890L 1.2A、電流制限、ハイサイドPチャネルスイッチ、サーマルシャットダウン付 無料
サンプル
 


次のステップ
EE-Mail EE-Mail配信の登録申し込みをして、興味のある分野の最新ドキュメントに関する自動通知を受け取る。
ダウンロード ダウンロード、PDFフォーマット (29kB)  

© Aug 17, 2000, Maxim Integrated Products, Inc.
このウェブサイトのコンテンツは米国および各国の著作権法によって保護されています。コンテンツの複製を希望される場合は、お問い合わせください

APP 298: Aug 17, 2000
アプリケーションノート298, AN298, AN 298, APP298, Appnote298, Appnote 298