NXP FTF Technology Forum

05/16/2016 - 05/19/2016
Austin, TX


Join us at this year's NXP FTF Technology Forum for the inspiration, training and ecosystem you need to compete in a relentless global marketplace. They will share the benefits of the expanded, secure and connected portfolio created by the 2015 merger of NXP and Freescale. More than 250 product and technology demos trigger your imagination and push your design boundaries. With more than 180 demos on board, the tour highlights everything from the smallest microcontrollers to the complex networking infrastructure that powers the new Smarter World.

Our Demo
Cameras are critical to today's automobile, improving safety and convenience. However, the task of managing up to eight cameras in a cost-effective manner is an engineering challenge.

That's why, at NXP FTF 2016, we're proud to introduce a new serial link solution for aggregating all those video streams. The MAX9286 quad GMSL deserializer was made to work hand-in-hand with NXP's S32V234 processor. Maxim's Gigabit Media Serial Link (GMSL) greatly simplifies system design by combining four camera streams into a single output. The solution also drives cables (up to 15M), distributes camera power, and manages camera function, all in an elegant design.


We will be at Pedestal 417 in the Smart Transport

Register ›