FAQS:  MAX21000 MAX21000, MAX21002 MAX21002, MAX21003 MAX21003

What are the differences among the MAX21000, MAX21002, and MAX21003?
Do the MAX21000, MAX21002, and MAX21003 have different identifier registers?
How can the internal temperature sensor be enabled?
How can the temperature registers TEMP_H and TEMP_L be converted to a temperature value?
Do the MAX21000, MAX21002, and MAX21003 perform automatic temperature compensation?
What is the self-test feature?
What is the expected format and variation of the self-test output?
How should the self-test output values be interpreted?
Do the MAX21000, MAX21002, and MAX21003 have bias compensation?
What is the default power mode of the MAX21000, MAX21002, and MAX21003?
Can the MAX21000 power mode be controlled in hardware?
Do the I2C interface pins feature internal pullups?
Which I2C communication speeds are supported?
Are the interrupt pins open-drain outputs or push-pull outputs?
Why is the interrupt pin generating an 8.8 MHz clock?
I'm using the MAX21000, MAX21002, or MAX21003 in normal mode and the X, Y, Z axes are enabled. Why is the data not changing?
How does the raw gyroscope data relate to degrees per second?
Does the MAX21000 accuracy change with the full-scale range?
Can the sample instant be synchronized to an external trigger?