Glossary Definition for daisy_chain

Glossary Term: daisy_chain 

Definition

A method of propagating signals along a bus in which the devices are connected in series and the signal passed from one device to the next. The daisy chain scheme permits assignment of device priorities based on the electrical position of the device on the bus.
Synonyms
  • Daisy-Chain

Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ

Comment on This Term (Corrections, Suggestions, etc.)

Suggest Another Term We Should Add