Glossary Definition for Transconductance Amplifier

Glossary Term: Transconductance Amplifier 

Definition

An amplifier that converts a voltage to a current. Also known by several other terms (see synonym list). One synonym is OTA, or operational transconductance amplifier, a term that marries the terms transconductance amplifier and operational amplifier.

The term derives from "transfer conductance" and is measured in siemens (S), where 1 siemens = 1 ampere per volt. It is represented with the symbol gm. The basic gain of vacuum tubes and FETs is expressed as transconductance.

See: Transimpedance Amplifier Buffers Current Transformer
Synonyms
  • OTA
  • VCIS
  • mutual conductance
  • operational transconductance amplifier
  • voltage controlled current source
Related Parts
  • MAX436 - 250MHz Wideband Transconductance Amplifier with Differential Output
  • MAX435 - 250MHz Wideband Transconductance Amplifier with Differential Output
See Also
Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ