Glossary Definition for Three-State

Glossary Term: Three-State 

Definition

A three-state, or Tri-State™, output has three electrical states: One, zero, and "Hi-Z," or "open." The hi-Z state is a high-impedance state in which the output is disconnected, leaving the signal open, to be driven by another device (or to be pulled up or down by a resistor provided to prevent an undefined state).

High-impedance schemes such as three-state are commonly used for a bus, in which several devices can be selected to drive the bus.

Tri-State™ is a trademark of National Semiconductor.

See Also
Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ