Glossary Definition for PA

Glossary Term: PA 

Definition

A power amplifier (PA) converts a low-power signal to a higher power one. Two common examples are audio amplifiers, used to drive loudspeakers and headphones, and RF power amplifiers, such as those used in the final stage of a transmitter.

What are the types of power amplifier?

Power amplifiers are divided into classes based on the amplifier’s characteristics. Classes A, AB, B, and C depend on their conduction angle, which is the number of degrees in a cycle during which the amplifying device conducts. Classes D and E are switching amplifiers. Classes D, DG, and H are also common audio amplifiers that are similar to Class AB but use different techniques to improve efficiency.

Classes A-C

A Class A amplifier has a 360o conduction angle (100% of the input signal is used). It is the most linear, meaning the output signal is the best representation of the input. It is, however, the least efficient. Subsequent classes are increasingly efficient and decreasingly linear:

Class Conduction angle Input Signal Used Efficiency Linearity
A 360o 100% Lowest Highest
AB 180o-360o 50-100% Medium low Medium high
B 180o 50% Medium high Medium low
C <180o <50% Highest Lowest

Power amplifier conduction angle diagram

Class C amplifiers conduct for up to half of a period and Class B for exactly half. Class AB amplifiers conduct for 50-100% of the cycle and Class A amplifiers for the whole cycle.

Class D

Class D amplifiers use pulse-width modulation (PWM) to produce rail-to-rail digital output signal with a variable duty cycle to approximate the analog input signal. They are highly efficient because the output transistors are always either fully turned on or fully turned off.

Classes G and H

Class G amplifiers are similar to Class AB amps, except that they use two or more supply voltages and are more efficient because they use the maximum supply voltage only when required. Class H power amps are similar to Class G, but the Class H topology does not require multiple power supplies.

Class DG

The Class DG amp is similar to the Class D amp but also uses a multilevel output stage to sense the magnitude of the output signal. It then switches the supply rails as needed to supply the required signal power more efficiently.

Learn More:

Synonyms
  • Power Amplifier

Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ