Glossary Definition for Ingress Protection

Glossary Term: Ingress Protection 

Definition

An Ingress Protection (IP) rating indicates how well an enclosure is protected from penetration by contaminants such as dust or fluids (such as water). IP ratings are defined in the IEC standard 60529.

See also:

Synonyms
  • IP
Keywords

ip, ingress protection, enclosure, iec 60529, thermochron, hygrochron, ibutton, ibutton capsule
Related Parts
  • DS9107 - iButton Capsule
  • DS1921H - High-Resolution Thermochron iButton Devices
  • DS1921G - Thermochron iButton Device
  • DS1923 - iButton Hygrochron Temperature/Humidity Logger with 8KB Data-Log Memory
  • DS1922T - iButton Temperature Loggers with 8KB Data-Log Memory
  • DS1922L - iButton Temperature Loggers with 8KB Data-Log Memory
  • DS1921Z - High-Resolution Thermochron iButton Devices
See Also
Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ