Glossary Definition for H-Bridge

Glossary Term: H-Bridge 

Definition

A circuit diagram which resembles the letter "H." The load is the horizontal line, connected between two pairs of intersecting lines. It is very common in DC motor-drive applications where switches are used in the "vertical" branches of the "H" to control the direction of current flow, and thus the rotational direction of the motor.

Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ