Glossary Definition for Burst Dimming

Glossary Term: Burst Dimming 

Definition

Burst Dimming is a method of controlling the brightness of cold cathode fluorescent lamps (CCFL) by turning the lamps on and off at a rate faster than the human eye can detect. The on/off rate is nominally 100Hz to 300Hz. The higher the ratio of on-time to off-time, the brighter the lamps will be. Because of CCFL response times, on-time to off-time ratios of less than 1% are not practical.
Keywords

cold cathode fluorescent, CCFL, brightness, dimming
Related Parts
  • DS3988 - 8-Channel Cold-Cathode Fluorescent Lamp Controller
  • DS3994 - 4-Channel Cold-Cathode Fluorescent Lamp Controller
See Also
Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ