Glossary Definition for Analog-Switch

Glossary Term: Analog-Switch 

Definition

An analog switch (sometimes just called a "switch") is a switching device capable of switching or routing analog signals (meaning signals that can have any level within a specified legal range), based on the level of a digital control signal. Commonly implemented using a "transmission gate," an analog switch performs a function similar to that of a relay.

For example, an analog switch can turn an audio signal on or off based on a MUTE signal; or analog switches could send one of two signals to a headphone amplifier.

Most commonly implemented using CMOS technology integrated circuits. Maxim makes hundreds of examples. See the Analog Switch and Multiplexer Product Line page.

Also see What is a Transmission Gate (Analog Switch)?.

Synonyms
  • Switch
  • Transmission Gate

Find a term alphabetically:
0-9ABCDEFGHIJKLMNOPQRSTUVWXYZ

Comment on This Term (Corrections, Suggestions, etc.)

Suggest Another Term We Should Add