Additional Information:
Introduction
CATV circuits operate in a 75Ω environment. Most RF laboratories equipped with standard test instruments employ 50Ω as the standard interface impedance.
In this application note, it will be shown that:
dBmV = 46.9897 + dBm50Ω
dBmV = 48.7506 + dBm75Ω
dBµV = 60 + dBmV
dBµV = 106.98 + dBm50Ω
dBµV = 108.75 + dBm75Ω
dBmV and dBµV
Most CATV measurements are referenced to voltage and measured in dBmV or dBµV. In the classic definition, dBmV is referenced to 1mVRMS and output voltage (VOUT) is measured in mVRMS (Equation 1). Since Equation 1 is a ratio of voltage, it can also be measured in mVP-P referenced to 1mVP-P or any voltage unit as long as the same units are used.
Inspection of Equation 1 shows dBmV to be independent of impedance.
In the classic definition, dBµV is referenced to 1µVRMS and output voltage (VOUT) is measured in µVRMS (Equation 2). Since Equation 1 is a ratio of voltage, it can also be measured in µVP-P referenced to 1µVP-P or any voltage unit as long as the same units are used.
Inspection of Equation 2 shows dBµV to be independent of impedance.
Conversion of dBm to dBmV
dBm is defined in Equation 3.
POUT is measured in mW. The dBm is referenced to 1mW. Equation 3 does depend on impedance of the load as shown in Equation 4. Most RF equipment has a 50Ω load or input impedance. Equation 3 is still valid for any load impedance including 75Ω.
Power depends on load impedance. Equation 4 equates power to voltage and load impedance.
Rearranging terms,
Solving Equation 3 for POUT,
Solving Equation 1 for VOUT,
Substituting Equation 3.1 and Equation 1.1 into Equation 4.1,
Solving for dBmV in terms of dBm,
Using R = 50Ω,
Equation 5.2 is valid for 50Ω measurement equipment.
Solving Equation 5.1 using R = 75Ω,
Equation 5.3 is valid for 75Ω measurement equipment.
Using the same technique it can be shown that the relationship for dBµV to dBmV is

Table 1 and Table 2 show conversions between dBmV, dBµV and dBm in a 50Ω and 75Ω environment.
Table 1. Conversions of Power 50Ω
dBmV |
dBµV |
dBm 50Ω |
mVRMS |
mW 50Ω |
8 |
68 |
-38.99 |
2.51 |
1.3E-04 |
9 |
69 |
-37.99 |
2.82 |
1.6E-04 |
10 |
70 |
-36.99 |
3.16 |
2.0E-04 |
11 |
71 |
-35.99 |
3.55 |
2.5E-04 |
12 |
72 |
-34.99 |
3.98 |
3.2E-04 |
13 |
73 |
-33.99 |
4.47 |
4.0E-04 |
14 |
74 |
-32.99 |
5.01 |
5.0E-04 |
15 |
75 |
-31.99 |
5.62 |
6.3E-04 |
16 |
76 |
-30.99 |
6.31 |
8.0E-04 |
17 |
77 |
-29.99 |
7.08 |
1.0E-03 |
18 |
78 |
-28.99 |
7.94 |
1.3E-03 |
19 |
79 |
-27.99 |
8.91 |
1.6E-03 |
20 |
80 |
-26.99 |
10.00 |
2.0E-03 |
21 |
81 |
-25.99 |
11.22 |
2.5E-03 |
22 |
82 |
-24.99 |
12.59 |
3.2E-03 |
23 |
83 |
-23.99 |
14.13 |
4.0E-03 |
24 |
84 |
-22.99 |
15.85 |
5.0E-03 |
25 |
85 |
-21.99 |
17.78 |
6.3E-03 |
26 |
86 |
-20.99 |
19.95 |
8.0E-03 |
27 |
87 |
-19.99 |
22.39 |
0.010 |
28 |
88 |
-18.99 |
25.12 |
0.013 |
29 |
89 |
-17.99 |
28.18 |
0.016 |
30 |
90 |
-16.99 |
31.62 |
0.020 |
31 |
91 |
-15.99 |
35.48 |
0.025 |
32 |
92 |
-14.99 |
39.81 |
0.032 |
33 |
93 |
-13.99 |
44.67 |
0.040 |
34 |
94 |
-12.99 |
50.12 |
0.050 |
35 |
95 |
-11.99 |
56.23 |
0.063 |
36 |
96 |
-10.99 |
63.10 |
0.080 |
37 |
97 |
-9.99 |
70.79 |
0.100 |
38 |
98 |
-8.99 |
79.43 |
0.126 |
39 |
99 |
-7.99 |
89.13 |
0.159 |
40 |
100 |
-6.99 |
100.00 |
0.200 |
41 |
101 |
-5.99 |
112.20 |
0.252 |
42 |
102 |
-4.99 |
125.89 |
0.317 |
43 |
103 |
-3.99 |
141.25 |
0.399 |
44 |
104 |
-2.99 |
158.49 |
0.502 |
45 |
105 |
-1.99 |
177.83 |
0.632 |
46 |
106 |
-0.99 |
199.53 |
0.796 |
47 |
107 |
0.01 |
223.87 |
1.002 |
48 |
108 |
1.01 |
251.19 |
1.262 |
49 |
109 |
2.01 |
281.84 |
1.589 |
50 |
110 |
3.01 |
316.23 |
2.000 |
51 |
111 |
4.01 |
354.81 |
2.518 |
52 |
112 |
5.01 |
398.11 |
3.170 |
53 |
113 |
6.01 |
446.68 |
3.991 |
54 |
114 |
7.01 |
501.19 |
5.024 |
55 |
115 |
8.01 |
562.34 |
6.325 |
56 |
116 |
9.01 |
630.96 |
7.962 |
57 |
117 |
10.01 |
707.95 |
10.024 |
58 |
118 |
11.01 |
794.33 |
12.619 |
59 |
119 |
12.01 |
891.25 |
15.887 |
60 |
120 |
13.01 |
1000.00 |
20.000 |
61 |
121 |
14.01 |
1122.02 |
25.179 |
62 |
122 |
15.01 |
1258.93 |
31.698 |
63 |
123 |
16.01 |
1412.54 |
39.905 |
64 |
124 |
17.01 |
1584.89 |
50.238 |
65 |
125 |
18.01 |
1778.28 |
63.246 |
66 |
126 |
19.01 |
1995.26 |
79.621 |
67 |
127 |
20.01 |
2238.72 |
100.237 |
68 |
128 |
21.01 |
2511.89 |
126.191 |
Table 2. Conversions of Power 75Ω
dBmV |
dBµV |
dBm 75Ω |
mVRMS |
mW 75Ω |
8 |
68 |
-40.75 |
2.51 |
8.4E-05 |
9 |
69 |
-39.75 |
2.82 |
1.1E-04 |
10 |
70 |
-38.75 |
3.16 |
1.3E-04 |
11 |
71 |
-37.75 |
3.55 |
1.7E-04 |
12 |
72 |
-36.75 |
3.98 |
2.1E-04 |
13 |
73 |
-35.75 |
4.47 |
2.7E-04 |
14 |
74 |
-34.75 |
5.01 |
3.3E-04 |
15 |
75 |
-33.75 |
5.62 |
4.2E-04 |
16 |
76 |
-32.75 |
6.31 |
5.3E-04 |
17 |
77 |
-31.75 |
7.08 |
6.7E-04 |
18 |
78 |
-30.75 |
7.94 |
8.4E-04 |
19 |
79 |
-29.75 |
8.91 |
1.1E-03 |
20 |
80 |
-28.75 |
10.00 |
1.3E-03 |
21 |
81 |
-27.75 |
11.22 |
1.7E-03 |
22 |
82 |
-26.75 |
12.59 |
2.1E-03 |
23 |
83 |
-25.75 |
14.13 |
2.7E-03 |
24 |
84 |
-24.75 |
15.85 |
3.3E-03 |
25 |
85 |
-23.75 |
17.78 |
4.2E-03 |
26 |
86 |
-22.75 |
19.95 |
5.3E-03 |
27 |
87 |
-21.75 |
22.39 |
6.7E-03 |
28 |
88 |
-20.75 |
25.12 |
8.4E-03 |
29 |
89 |
-19.75 |
28.18 |
0.011 |
30 |
90 |
-18.75 |
31.62 |
0.013 |
31 |
91 |
-17.75 |
35.48 |
0.017 |
32 |
92 |
-16.75 |
39.81 |
0.021 |
33 |
93 |
-15.75 |
44.67 |
0.027 |
34 |
94 |
-14.75 |
50.12 |
0.033 |
35 |
95 |
-13.75 |
56.23 |
0.042 |
36 |
96 |
-12.75 |
63.10 |
0.053 |
37 |
97 |
-11.75 |
70.79 |
0.067 |
38 |
98 |
-10.75 |
79.43 |
0.084 |
39 |
99 |
-9.75 |
89.13 |
0.106 |
40 |
100 |
-8.75 |
100.00 |
0.133 |
41 |
101 |
-7.75 |
112.20 |
0.168 |
42 |
102 |
-6.75 |
125.89 |
0.211 |
43 |
103 |
-5.75 |
141.25 |
0.266 |
44 |
104 |
-4.75 |
158.49 |
0.335 |
45 |
105 |
-3.75 |
177.83 |
0.422 |
46 |
106 |
-2.75 |
199.53 |
0.531 |
47 |
107 |
-1.75 |
223.87 |
0.668 |
48 |
108 |
-0.75 |
251.19 |
0.841 |
49 |
109 |
0.25 |
281.84 |
1.059 |
50 |
110 |
1.25 |
316.23 |
1.333 |
51 |
111 |
2.25 |
354.81 |
1.679 |
52 |
112 |
3.25 |
398.11 |
2.113 |
53 |
113 |
4.25 |
446.68 |
2.660 |
54 |
114 |
5.25 |
501.19 |
3.349 |
55 |
115 |
6.25 |
562.34 |
4.216 |
56 |
116 |
7.25 |
630.96 |
5.308 |
57 |
117 |
8.25 |
707.95 |
6.683 |
58 |
118 |
9.25 |
794.33 |
8.413 |
59 |
119 |
10.25 |
891.25 |
10.591 |
60 |
120 |
11.25 |
1000.00 |
13.333 |
61 |
121 |
12.25 |
1122.02 |
16.786 |
62 |
122 |
13.25 |
1258.93 |
21.132 |
63 |
123 |
14.25 |
1412.54 |
26.604 |
64 |
124 |
15.25 |
1584.89 |
33.492 |
65 |
125 |
16.25 |
1778.28 |
42.164 |
66 |
126 |
17.25 |
1995.26 |
53.081 |
67 |
127 |
18.25 |
2238.72 |
66.825 |
68 |
128 |
19.25 |
2511.89 |
84.128 |
|