TUTORIALS 5045

An Introduction to Preemphasis and Equalization in Maxim GMSL SerDes Devices

By: Caglar Yilmazer

Abstract: Transmit preemphasis and receive equalization can allow serializer/deserializer (SerDes) devices to operate over inexpensive cables or over extended distances. This application note describes how signals are degraded over cables and how to compensate for that degradation. Additionally, this document explains how to achieve a robust link with Maxim gigabit multimedia serial link (GMSL) products when using lossy cables. The article also provides an overview on line equalization.

A similar version of this article appeared on November 2, 2011 on John Day's Automotive Electronics News.

Introduction

Recent advances in video applications, along with the exponential expansion of data traffic volume, have raised the demand for higher data rates. As a result, low-cost twisted-pair (TP) cables have gained special interest. However, frequency-dependent attenuation over long runs of these TP cables is a major limiting factor to their optimal use. This frequency-dependent attenuation causes significant intersymbol interference (ISI) in the received signal, which, in turn, creates difficulty for clock and data recovery and causes a higher bit-error rate (BER). Figure 1 shows the representation of a transmitted signal being degraded by the cable before the signal arrives at the receiver. By significantly reducing ISI and recovering the severely degraded data, the transmitter and the receiver can employ some form of line equalization to enable reliable operation.
Figure 1. ISI at the receiver end.
Figure 1. ISI at the receiver end.
The high-speed 3.125Gbps transceivers in Maxim GMSL parts provide a robust link, by allowing the system designer to dynamically program the equalization level for a specific cable. The transmitter and receiver both have equalization adjustments that can be programmed either separately or together to extend the transmission distance. This flexible equalization adjustment allows the use of a wide range of low-cost lossy cables.
This application note explains how to design a robust link with Maxim GMSL products and lossy cables. It also provides an overview of line equalization.

GMSL Transmitter Preemphasis and Receiver Equalization

The GMSL link employs transmitter preemphasis and receiver equalization to compensate the losses of the transmission.

Transmitter Preemphasis

When no equalization is applied at the receiver end, a high-frequency "0" pulse may not be able to reach the midlevel of the signal swing after consecutive "1's", as shown in Figure 2. The figure illustrates how frequency-dependent attenuation can be overcome by emphasizing transitions and deemphasizing "no transitions."
Figure 2. Preemphasis filtering in time domain.
Figure 2. Preemphasis filtering in time domain.
The cable has a lowpass transfer function due to the conductor and dielectric losses, as shown in Figure 3. By utilizing equalization (a highpass transfer curve), a flat (uniform attenuation) system frequency response can be obtained within the bandwidth of the desired frequency range.
Figure 3. Preemphasis filtering in frequency domain.
Figure 3. Preemphasis filtering in frequency domain.
Effective use of this equalization technique will affect three main system design parameters:
  • Cable length
  • Cable type
  • Maximum system data rate
For instance, the totally closed eye at the end of a 10m cable can be reasonably opened by 6dB preemphasis (Figure 4).
Figure 4. 3.125Gbps data after 10m cable: (a) none vs. (b) 6dB preemphasis.
More detailed image
(PDF, 1.3MB)
Figure 4. 3.125Gbps data after 10m cable: (a) none vs. (b) 6dB preemphasis.
As described in the MAX9259 data sheet, the preemphasis level is set by register address 0x05, D[3:0]. The user can program the preemphasis level based on Table 1. The negative preemphasis levels correspond to where high-frequency terms are not emphasized, but only the low-frequency terms are deemphasized. It is also important to note that over-boosting will cause a slight increase in the timing jitter.
Table 1. Preemphasis and Deemphasis Levels
0x05 D[3:0] Preemphasis Level (dB)
1000 1.1
1001 2.2
1010 3.3
1011 4.4
1100 6.0
1101 8.0
1110 10.5
1111 14.0
  Deemphasis Level (dB)
0000 Not used
0001 -1.2
0010 -2.5
0011 -4.1
0100 -6.0
0111 Not used
In the following sections, how to utilize both the transmitter and receiver equalizers will be discussed, along with tabular test data.

Receiver Equalization

The basic idea behind the receiver equalization is described in Figure 5. The lossy link attenuates the forward channel data with an approximate first-order transfer function that has a much lower bandwidth than the data frequency (data frequency, fb, is equal to one-half of the bit rate). This causes deterministic jitter due to intersymbol interference. Moreover, the eye diagram at the end of this lossy cable can be totally closed for long cables. To compensate for this loss, the data is first processed through a transfer function, which is, ideally, the inverse of the cable transfer function. Hence, a sufficient bandwidth can be obtained when the link and the equalizer are cascaded. A 12-level programmable-gain approach was implemented in GMSL deserializers to prevent under- or over-boosting for different cable lengths. The gain can be set to 12 different levels of boost, ranging from 2dB to 13dB.
Figure 5. Data is equalized by applying the inverse of the channel transfer function within the receiver.
Figure 5. Data is equalized by applying the inverse of the channel transfer function within the receiver.
The receiver transfer function (AC characteristic) is shown in Figure 6 for different boost settings. The channel plus receiver transfer function are shown in Figure 7 for a 10m STP cable. Different boost levels are overlaid in this figure. The overall transfer function becomes maximally flat within the frequency range of interest when the boost word is 8 (9.4dB). The receiver input and output eye diagrams for a 10m STP cable are shown in Figure 8. Notice how the equalizer gain boost opens the totally closed eye.
What happens if the overall transfer function is not flat? In terms of ISI jitter, over-boosting is less harmful than under-boosting. As illustrated in Figure 9, when the boost level decreases below the optimal value, output jitter increases very quickly. Contrastingly, jitter increases slowly when the boost level increases above the optimal point.
Figure 6. Equalizer AC characteristics and boosting gain for different tuning words.
Figure 6. Equalizer AC characteristics and boosting gain for different tuning words.






Figure 7. AC response of cable and equalizer (cascaded) for different boost levels for a 10m STP cable.
Figure 7. AC response of cable and equalizer (cascaded) for different boost levels for a 10m STP cable.
Figure 8. Receiver input and output eye diagrams for a 10m cable when the boost is optimal.
Figure 8. Receiver input and output eye diagrams for a 10m cable when the boost is optimal.
Figure 9. Peak-to-peak ISI jitter vs. boosting gain for a 10m cable.
Figure 9. Peak-to-peak ISI jitter vs. boosting gain for a 10m cable.

Choosing the Optimal Preemphasis and Equalizer Setting

Perhaps you do not want to measure the cable loss with a spectrum analyzer. In that case, the easiest method for choosing an optimal preemphasis/equalizer setting is to look at the bit-error rate of the system at limit frequencies. Two real-world cases will be supplied here as examples.
In Table 2, we summarize the maximum pixel clock frequencies at which our SerDes pair, like the MAX9259/MAX9260 or the MAX9249/MAX9268, can operate with a 10m cable. Each column shows a different Rx equalizer boost gain, whereas each row corresponds to a different Tx preemphasis value. The SerDes pair under testing can operate up to 124MHz when the transmission medium is equalized properly. It reaches 124MHz with a minimum total boost of 14.1dB (1.1dB preemphasis and 13dB Rx equalization). After the total boost goes above 18.2dB (14dB preemphasis and 4.2dB Rx equalization), ISI again starts to increase, which limits the operation frequency. Thus, it is wise to choose a total boost value between 14.1dB and 18.2dB. We generally recommend choosing the big portion of boost from the Rx part, because the Rx equalizer has a constant low-frequency gain, whereas Tx attenuates the low-frequency to implement preemphasis. Attenuating the low-frequency means lower signal levels over the link, which makes the life more difficult for the receiver. So 3.3dB preemphasis and 13dB Rx boost would be a good selection. The same procedure can be applied for a 15m cable as well. Its maximum frequencies for different boost levels are summarized in Table 3. Minimum and maximum boost levels are 19.7dB (8dB preemphasis and 11.7dB Rx equalization) and 23.4dB (14dB preemphasis and 9.4dB Rx equalization), respectively, so 8dB preemphasis and 13dB Rx boost is the optimum choice.
Table 2. Example 10m Automotive STP Cable and Connectors
Rx 0000
2.1dB
0001
2.8dB
0010
3.4dB
0011
4.2dB
0100
5.2dB
0101
6.2dB
0110
7dB
0111
8.2dB
1000
9.4dB
1001
10.7dB
1010
11.7dB
1011
13dB
Tx
OFF 70 72 76 80 85 90 98 105 113 119 122 123
1.1dB 78 80 83 88 93 98 105 111 117 121 123 124
2.2dB 85 87 90 94 99 104 110 116 120 123 124 124
3.3dB 92 95 97 102 106 111 116 119 122 124 124 124
4.4dB 100 103 105 108 113 117 120 122 124 124 124 124
6.0dB 110 112 115 117 120 122 123 124 124 124 124 115
8.0dB 119 120 121 122 123 124 124 124 124 114 109 104
10.5dB 123 124 124 124 124 124 119 113 108 103 97 92
14.0dB 124 124 124 124 114 110 104 100 95 91 86 78
Table 3. Example 15m Automotive STP Cable and Connectors
Rx 0000
2.1dB
0001
2.8dB
0010
3.4dB
0011
4.2dB
0100
5.2dB
0101
6.2dB
0110
7dB
0111
8.2dB
1000
9.4dB
1001
10.7dB
1010
11.7dB
1011
13dB
Tx
OFF 47 48 50 52 54 57 61 67 76 84 94 104
1.1dB 53 54 55 57 60 63 68 75 82 90 101 110
2.2dB 58 59 61 63 66 70 76 81 89 97 106 114
3.3dB 64 65 67 69 73 77 83 88 95 104 112 118
4.4dB 71 73 74 77 81 84 90 96 104 110 117 120
6.0dB 81 82 84 87 91 95 101 107 112 118 121 123
8.0dB 93 94 96 99 103 108 112 116 120 122 124 124
10.5dB 108 110 112 113 117 119 121 122 124 124 124 124
14.0dB 118 118 119 121 122 123 124 124 124 110 101 94
Color Code
≥ 104MHz (3.125Gbps) 84MHz to 103MHz (2.5Gbps to 3.125Gbps)
66MHz to 83MHz (2.0Gbps to 2.5Gbps) < 66MHz (2.0Gbps)

Link Activity Detector

GMSL deserializers have a signal-detector circuit, which disables the receiver when there is no signal over the link. When the signal levels are very low due to long cables or high preemphasis levels, deserializers may not detect the activity over the link. Thus, it is highly recommended to disable the activity detector, while searching the optimum preemphasis and equalizer setting for long cables (> 10m). The detector can be disabled by writing "0x80" to the byte 11 of the deserializer. It can be enabled again by writing "0x20" to the same byte after the optimum values are chosen. According to our lab measurements, the activity detector works up to 8dB preemphasis for a 15m cable at the maximum PCLK frequency 104.16MHz. There is also a low threshold option for the activity detector. It can be programmed by writing "0x00" to the byte 11. According to lab measurements, the activity detector works up to 14dB preemphasis for a 15m cable when low threshold is selected. If the cable is longer than 15m and preemphasis is 14dB, it is recommended to disable the activity detector. Cables used in these measurements are standard automotive STP cables.