The Current DACs
The
DS1864 contains two 8-bit current-sink DACs with 1.5mA or 0.5mA selectable full-scale range. The DAC outputs must be at a voltage level between 0.7V and the DS1864's V
CC.
Current-to-Voltage Conversion
An operational amplifier in differential amplifier configuration is used to convert the 0.5mA full-scale current-mode output to 1V full-scale voltage-mode output (
Figure 1).
Figure 1. Circuit shows current-to-voltage conversion.
Compact Solution
Using a chip-scale packaged op amp and 0201 resistors will provide the most compact solution. The
MAX4233 is a two-channel op amp available in 1.5mm x 2mm 10-bump UCSP™.
Output Voltage Calculation
The output voltage is calculated in Equation 1.

Using the values shown in the Figure 1 drawing, the maximum output voltage is 1.005V when the DAC current is 0.5mA. To minimize offset and gain errors, 1% tolerance resistors should be used. Further, R1 should be selected so that the voltage at the DAC pin never falls below 0.7V.
© , Maxim Integrated Products, Inc.
|
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content,
contact us.
APP 4075:
TUTORIALS
4075,
AN4075,
AN 4075,
APP4075,
Appnote4075,
Appnote 4075
|
maxim_web:en/products/analog/data-converters/digital-potentiometers,maxim_web:en/products/comms/optical-comms,maxim_web:en/products/analog/data-converters/d-a-converters
maxim_web:en/products/analog/data-converters/digital-potentiometers,maxim_web:en/products/comms/optical-comms,maxim_web:en/products/analog/data-converters/d-a-converters