APPLICATION NOTE 825

Sawtooth Generator Exhibits ~1% Linearity And >80dB Dynamic Frequency Range


Abstract: Two integrated circuits (ICs) and some associated components form a voltage-controlled sawtooth generator that costs less than $3 and produces an auxiliary square wave at the same frequency. The generator is useful in a variety of applications. Its sawtooth waveform is commonly used, for example, to sweep the frequency of another generator.