Designing a Power Amplifier Optimized for Predistortion and Scintera’s RF PA Linearizer (RFPAL)
Errors
Keywords: predistortion, power, amplifier, optimized Related Parts
APPLICATION NOTE 5924
Designing a Power Amplifier Optimized for Predistortion and Scintera’s RF PA Linearizer (RFPAL)
Abstract:Designing a robust RF PA system dependent upon predistortion begins with the design of a RF power amplifier optimized for use with predistortion. There are a number of ways to design RF power amplifiers to achieve various performance goals, but in order for the amplifier system to achieve the best linearity and efficiency when operated with predistortion, the amplifier must be designed to follow the guidelines provided below. These guidelines assume the use of Scintera’s RF PA Linearizer (RFPAL) but are also useful in designing a system based on other types of predistortion. Using a RFPAL like the SC1894, an optimally tuned PA can achieve 20dBc or more improvement in linearity (see Table 1) thus allowing the amplifier to operate at Psat – PAR and at the peak possible efficiency. Conversely, a PA which has not been optimized for operation with RFPAL may achieve little to no improvement in linearity and it will likely fail to meet the spectral requirement.A typical closed loop system requires a feedback path that taps into the PA output, down-converts and then digitizes the signal which may then be used by the linearizer. Therefore a typical feedback path consists of blocks including a down mixer, variable gain amplifier and ADC. As a discrete implementation, these components add additional cost and power consumption to the system. The Scintera RFPAL integrates the linearizer and all necessary feedback components into a single IC. This vastly simplifies (and speeds up) the system implementation and minimizes the additional board space.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content,
contact us.
Thank You for interest in Maxim Integrated. Our free samples program limits the quantities that we can provide to each customer per calendar year.If you feel that you have received this message in error, please contact samples-admin@maximintegrated.com. Alternatively, you can click here to place an order.
Part Number
Description
Key Advantages
Request a Quote
Your quote has been successfully submitted. You will receive an email within 24 hours with pricing and availability. Visit My Quotes Thank you!