APPLICATION NOTE 4862

Reserved or \"Don't Care\" Bit Programming in the MAX5110/MAX5111 Multichannel DACs

By: David Fry

Abstract: The device register maps for the MAX5110/MAX5111 multichannel DACs contain some bits that are named \"reserved.\" This application note describes how these bits must be handled.


This document is written for a highly specific application and contains information about proprietary technology, and is only available to customers whose requirements closely match the application. To request the full document, please complete the form below.

Please enter information in English only.


APPLICATION NOTE 4862,AN4862, AN 4862, APP4862, Appnote4862, Appnote 4862