APPLICATION NOTE 4642

Getting Started with the MAXQ3180: Configuring the Registers

By: Ben Smith

Abstract: The MAXQ3180 polyphase, multifunction metering AFE contains a daunting number of configuration registers. Only a few of these registers must be configured to enable basic device operation. This application note describes how to configure these registers to ensure success. A table categorizes which registers must be loaded, which can be enabled, and which need not be modified.

Introduction

The MAXQ3180 is a sophisticated, three-phase electricity-meter IC that can be configured to operate in a wide variety of metering environments. To support that flexibility, it contains 68 configuration registers. Understanding how all of these registers work can be a daunting task. However, in most cases it is not necessary to load all 68 registers. In fact, to enable basic meter operation only 10 registers must typically be configured.

This application note describes which MAXQ3180 registers must be initialized and which can be initialized to enable certain features. The article also explains which registers can be safely left alone in almost all applications.

Essential Initialization

As soon as power is applied, the MAXQ3180 will begin operating, accumulating energy, and measuring voltage, current, and power. It is, nonetheless, critical to configure the device to match the transducers that connect the MAXQ3180 to the line so that it will deliver readings in meaningful units.

The MAXQ3180 performs measurements in a two-step process: first, it reads the physical phenomena (e.g., voltage, current, and power) and internally expresses them as arbitrary values called "meter units;" and second, it converts the values expressed as meter units to real-world units such as volts, amperes, and watts.

Reading the Physical Phenomena (Metrology)

The MAXQ3180's first step is to perform the required measurements and express these measurements accurately in "meter units," i.e., units that are suited to the measurement circuitry. Ensuring that a given measurement unit—volts, amperes, watts, or kilowatt-hours—is accurately reflected in meter units is accomplished in the calibration process. Once current, voltage, power, and energy are accurately expressed in meter units, the device must convert these meter unit measurements to some unit that is meaningful in the real world.

We will use voltage calibration as an example, but the general procedure applies to current, power, or energy as well. Assume a voltage-divider as an input circuit with a target conversion ratio of 600:1. This means that if 600V DC is applied to the input of the divider, the output voltage would be close to 1V. The logic for the MAXQ3180's current and voltage inputs has a range of 224 counts. Consequently in this example, one least-significant bit (LSB) change in the output code would correspond to a change in voltage of 600 × 2-24 volts, or 35.8µV. Put another way, if one applied a 120VRMS sine to the input, one would expect the raw RMS voltage register to read 120/(600 × 2-24), or 3,355,443 (0x33 3333).

Because of natural variability in the passive components used for scaling and filtering the input signal and in the input ADC itself, it is unlikely that the value read from the ADC will match the expected value. For this reason, a correction factor must be applied to the x.V_GAIN (where x is the phase identifier: A, B or C) register. For this example, assume that the value read from the raw RMS register was only 3,000,000 (0x2D C6C0). This means that a gain must be applied equal to 3,355,443/3,000,000 = 1.12.

The gain adjustment registers are configured so that a value of 0x4000 (16,384) is unity gain. To apply additional gain, program a value greater than this. In this case, we would program 16,384 × (3,355,443/3,000,000) = 18,325 (0x4795).

That completes the first step of the process: make the voltage channel accurately reflect the actual voltage applied in meter units. The second step now is to convert from a system in which one LSB is equal to 35.8µV to a system in which one LSB is equal to something simpler, for example, 1mV.

Calculate the Conversion Constants

The immediate problem is that only an integer-multiply operation is provided. To perform this conversion, one would normally divide by a noninteger, specifically, 1,000/35.8. The solution is, therefore, to arrange the scaling factor so that the desired unit is multiplied by a power of two. In this instance, the LSB will not be 1mV, but rather 1mV/216, or 15.3nV. When we take a measurement, we will simply discard the low-order 16 bits. What is left will be the voltage in millivolts.

To determine the scaling factor, just divide the raw LSB value (35.8µV) by the desired LSB value (15.3nV) and you will obtain 2,344 (0x0928). This is the value to load into the VOLT_CC register.

Now, anytime the V.A virtual register is read, the MAXQ3180 will multiply the A.VRMS register by 2,344 and report the product. This product will be the RMS voltage in units of 1mV/65,536. Host software will then discard the low-order 16 bits and report the remainder directly as the voltage in millivolts RMS.

Thus, for most applications one need only perform the calibration step (to establish the proper VRMS and IRMS levels) and calculate the conversion constants (for voltage, current, power, and energy).

Optional Initialization

Following the steps outlined above for voltage, current, energy, and power will provide accurate readings of these parameters. But there are many other functions provided in the MAXQ3180.

Interrupts

The MAXQ3180 has a sophisticated interrupt subsystem to alert the host processor of exceptional conditions. Conditions that can trigger an interrupt include:
  • Real or reactive energy flow changes direction, per phase
  • No zero-crossing events are detected on a phase for longer than some threshold time, per phase
  • Undervoltage, overvoltage, or overcurrent conditions are detected, per phase
  • An energy register has overflowed (a normal condition indicating that an accumulation should be made) , per phase
  • The configuration checksum has changed
  • The power to the MAXQ3180 is about to fail
For more information about the interrupt subsystem, consult the reference design for the MAXQ3180.

Pulse Configuration

Meter pulses are used to increment mechanical counters or to increment electronic energy-accumulation registers in many meters, and the MAXQ3180 fully supports meter pulses. Each of the two supported meter-pulse outputs has: a configuration register to select the parameter to be reflected in the meter pulse; a threshold register to establish the meter constant; and a pulse duration register to set the width of the meter pulse. For more information about the meter-pulse subsystem, consult the MAXQ3180 reference design.

Improved Accuracy

With ideal current and voltage transducers, the MAXQ3180 will provide excellent accuracy over a wide range of input currents. However, current transducers are never ideal. Often they have nonlinearities at the extreme ends of their operating range; frequently, the phase response of the sensor will change with changing current. The MAXQ3180 contains registers to compensate for this.

The MAXQ3180 has two fine-adjustment mechanisms to adjust for sensor inaccuracy. The first fine adjustment is a separate gain for low currents and offset adjustments for both low and high currents. This approach allows calibration using up to four points to adjust both gain and offset at low- and high-current levels.

The second fine adjustment is for trimming the voltage-to-current phase offset. In this adjustment scheme, you establish three current ranges by setting two thresholds. Current below both thresholds forms the first range. Current between the two thresholds forms the second range, and current above both thresholds forms the third range. A phase offset is then established for each of the three ranges for each of phase A, phase B, or phase C.

For more information about using the fine-adjustment registers to tune the accuracy of the MAXQ3180, see the MAXQ3180 reference design.

Summary

The MAXQ3180 is a flexible, electricity meter analog front-end (AFE) with several options to allow it to operate over a wide range of metering applications. By setting only a few registers (the calibration and scaling registers, in particular) you can get the electricity meter operating quickly and begin characterizing the accuracy of the new system.

LEGEND
            
                    
Registers that in common use must be loaded on initialization.
            
                    
Registers that are required to enable certain MAXQ3180 features, but may not be required in many applications.
            
                    
Registers that need not be modified in most applications.

Address Default Name Comment
0x002 0x00 OPMODE1 Set this register only if your connection mode is not standard delta or wye, if you wish to reverse pulse output polarity, or if you wish to enable communication CRC.
0x003 0x00 OPMODE2 This register contains bits for features that are infrequently used.
0x006 0x0000 IRQMASK Load only if interrupts are used.
0x010 0x0000 AUX_CFG Load only if the auxiliary channel is used (typically specialized applications).
0x014 0x0001 VOLT_CC Conversion constant for meter unit to real units conversion.
0x016 0x0001 AMP_CC Conversion constant for meter unit to real units conversion.
0x018 0x0001 PWR_CC Conversion constant for meter unit to real units conversion.
0x01A 0x0001 ENR_CC Conversion constant for meter unit to real units conversion.
0x01C 0x0010 CYCNT Load only if the DSP cycle time must be set to something other than 16 line cycles.
0x01E 0x00 PLSCFG1 Load if meter pulses are in use.
0x01F 0x00 PLSCFG2 Load if meter pulses are in use.
0x020 0x009C PLS1_WD Load if meter pulses are in use.
0x022 0x00100000 THR1 Load if meter pulses are in use.
0x026 0x009C PLS2_WD Load if meter pulses are in use.
0x028 0x00100000 THR2 Load if meter pulses are in use.
0x02C 0x00C8 REJ_NS Line-cycle filter; handle with care!
0x02E 0x4000 AVG_NS Line-cycle filter; handle with care!
0x030 0x4000 AVG_C Signal-path filter; handle with care!
0x032 0x00C8 HPF_C Signal-path filter; handle with care!
0x034 0x0091 B0FUND Fundamental-mode filter; handle with care!
0x036 0x000003B6 A1FUND Fundamental-mode filter; handle with care!
0x03A 0x0091 B0HARM Harmonic-mode filter; handle with care!
0x03C 0x000003B6 A1HARM Harmonic-mode filter; handle with care!
0x040 0x03E80000 Number of ADC frames per DSP cycle; automatically calculated and seldom needs manual intervention.
0x044 0xFFFF OCLVL Load only if overcurrent limits are used.
0x046 0xFFFF OVLVL Load only if overvoltage limits are used.
0x048 0x0000 UVLVL Load only if undervoltage limits are used.
0x04A 0x0003 NOLOAD Modify to match with your design specification.
0x054 0x2328 NZX_TIMO No zero-crossing timeout; generally no need to adjust this.
0x056 0x03E8 COM_TIMO Communications timeout; generally no need to adjust this.
0x058 0x0005 ACC_TIMO Energy accumulation startup delay; generally no need to reload this.
0x05A 0x0B00 ZC_LPF Zero-crossing filter; handle with care!
0x05C 0x0000 I1THR Set only if multirange phase compensation is desired.
0x05E 0x0000 I2THR Set only if multirange phase compensation is desired.
0x12E 0x0000 N_GAIN Neutral gain; adjust only if neutral current monitoring is used.
0x130 0x0000 A.I_GAIN Primary calibration register for phase A current.
0x132 0x0000 A.V_GAIN Primary calibration register for phase A voltage.
0x134 0x0000 A.E_GAIN Primary calibration register for phase A energy and power.
0x136 0x0000 A.EF_GAIN Adjust only if fundamental mode is used.
0x138 0x0000 A.OFFS_HI Secondary calibration for enhanced accuracy: phase A current offset, high range.
0x13A 0x0000 A.GAIN_LO Secondary calibration for enhanced accuracy: phase A current gain, low range.
0x13C 0x0000 A.OFFS_LO Secondary calibration for enhanced accuracy: phase A current offset, low range.
0x13E 0x0000 A.PA0 Secondary calibration for improved phase compensation.
0x140 0x0000 A.PA1 Secondary calibration for improved phase compensation.
0x142 0x0000 A.PA2 Secondary calibration for improved phase compensation.
0x145 0x00 A.MASK Set only if interrupts from this phase are desired.
0x21C 0x0000 B.I_GAIN Primary calibration register for phase B current.
0x21E 0x0000 B.V_GAIN Primary calibration register for phase B voltage.
0x220 0x0000 B.E_GAIN Primary calibration register for phase B energy and power.
0x222 0x0000 B.EF_GAIN Adjust only if fundamental mode is used.
0x224 0x0000 B.OFFS_HI Secondary calibration for enhanced accuracy: phase B current offset, high range.
0x226 0x0000 B.GAIN_LO Secondary calibration for enhanced accuracy: phase B current gain, low range.
0x228 0x0000 B.OFFS_LO Secondary calibration for enhanced accuracy: phase B current offset, low range.
0x22A 0x0000 B.PA0 Secondary calibration for improved phase compensation.
0x22C 0x0000 B.PA1 Secondary calibration for improved phase compensation.
0x22E 0x0000 B.PA2 Secondary calibration for improved phase compensation.
0x231 0x00 B.MASK Set only if interrupts from this phase are desired.
0x308 0x0000 C.I_GAIN Primary calibration register for phase C current.
0x30A 0x0000 C.V_GAIN Primary calibration register for phase C voltage.
0x30C 0x0000 C.E_GAIN Primary calibration register for phase C energy and power.
0x30E 0x0000 C.EF_GAIN Adjust only if fundamental mode is used.
0x310 0x0000 C.OFFS_HI Secondary calibration for enhanced accuracy: phase C current offset, high range.
0x312 0x0000 C.GAIN_LO Secondary calibration for enhanced accuracy: phase C current gain, low range.
0x314 0x0000 C.OFFS_LO Secondary calibration for enhanced accuracy: phase C current offset, low range.
0x316 0x0000 C.PA0 Secondary calibration for improved phase compensation.
0x318 0x0000 C.PA1 Secondary calibration for improved phase compensation.
0x31A 0x0000 C.PA2 Secondary calibration for improved phase compensation.
0x31D 0x00 C.MASK Set only if interrupts from this phase are desired.


Related Parts
MAXQ3180 Free Sample
Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format
© , Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.
APP 4642:
APPLICATION NOTE 4642,AN4642, AN 4642, APP4642, Appnote4642, Appnote 4642