/
/
/
/
Errors |
APPLICATION NOTE 4637
Determining LCM and OVD Thresholds for the DS3xxx CCFL Controllers
Abstract: The DS3881, DS3882, DS3988, DS3991, DS3992, and DS3994 are CCFL (cold-cathode fluorescent lamp)controllers that backlight LCDs (liquid crystal displays). Each controller channel has two input pins for lamp monitoring and current regulation, LCM and OVD. There are four thresholds associated with these two inputs. This application note describes how the thresholds are specified and how to determine correct threshold values based on the application.
LCM and OVD Thresholds and the Corresponding References
Each channel of the DS3881, DS3882, DS3988, DS3991, DS3992, and DS3994 CCFL (cold-cathode fluorescent lamp) controllers has two inputs, LCM for lamp current monitoring and OVD for overvoltage detection. There are four thresholds associated with LCM and OVD. Table 1 summarizes the description and symbol for each threshold.Table 1. Threshold Description and Symbols
Associated Pin | Symbol | Description |
LCM | VLOT | Lamp off threshold |
VLOC | Lamp overcurrent threshold | |
VLRT | Lamp regulation threshold | |
OVD | VOVDT | Lamp overvoltage threshold |
Both the LCM and OVD pins have an internal DC bias voltage, VDCB, which is 1.1V for the DS3881 and DS3882, and 1.35V for the DS3988, DS3991, DS3992, and DS3994. The thresholds can be referenced to either VDCB or signal ground (GND).
Depending on the voltage reference used, the thresholds specified in the various data sheets may appear to have different values although they are virtually the same. In the DS3881, DS3882, and DS3988 data sheets, the four thresholds are referenced to VDCB. In the DS3991, DS3992, and DS3994 data sheets, the four thresholds are referenced to ground and thus include VDCB. For example, the lamp regulation threshold (typical value) for the DS3988 is specified in the data sheet as 1.0V with respect to VDCB, and the VDCB is 1.35V. In the DS3994 data sheet the same parameter is specified as 2.35V and this value is with respect to signal ground. So the lamp regulation threshold of both the DS3988 and the DS3994 is virtually same. In fact, Note 3 in both data sheets explains this.
Determine Correct Thresholds Based on the Application
Since the threshold values can differ depending on the reference used, the user needs to correctly determine the reference (either VDCB or ground) and thus select the correct external component values. The general rule is to use VDCB as the reference if the LCM and OVD signals are AC coupled. This is typically the case for a single-lamp-per-channel application. However, the thresholds should be referenced to ground if no AC coupling is used. This guideline typically applies to applications using multiple lamps per channel applications. Two examples explain this principle.Application with a Single Lamp per Channel
In this application the internal DC bias voltage at the LCM and OVD pins allows for an AC-coupled input. This design can make the external circuitry very simple. A typical operating circuit for this application is shown in Figure 1.
Figure 1. Typical operating circuit with a single lamp per channel.
In this application, the thresholds are referenced to VDCB. The values are listed in Table 2 and may be different for other parts.
Table 2. DS3994 LCM and OVD Thresholds (for Figure 1)
Parameter | Symbol | Min | Typ | Max | Units |
Lamp off threshold | VLOT | 0.30 | 0.40 | 0.50 | V |
Lamp overcurrent threshold | VLOC | 1.80 | 2.00 | 2.20 | V |
Lamp regulation threshold | VLRT | 0.94 | 1.00 | 1.06 | V |
OVD threshold | VOVDT | 0.90 | 1.00 | 1.10 | V |
Application with Multiple Lamps per Channel
Figure 2 shows a typical operating circuit with multiple lamps per channel using the DS3994. In this application, the lamp currents and voltages must be wire-ORed and fed to the LCM and OVD inputs on the DS3994. Some external circuitry, including voltage-dividers and peak detectors, is used. Unlike the application with a single lamp per channel, the application with multiple lamps per channel does not use an AC-coupling capacitor at the LCM input. The DS3994 controls the lamp current based on the peak signal measured at the LCM input. With no AC-coupling capacitor, the peak control level will be the DC-bias voltage (1.35V) plus the lamp-regulation threshold (1.0V) or 2.35V nominal. Hence, the peak voltage level created by the lamp's current-feedback resistor must be attenuated to a target value of 2.35Vpeak at the LCM input so the device can control the lamp current to the proper level. Similarly, the OVD threshold in this application is 2.35Vpeak with respect to ground.
Figure 2. Typical operating circuit with multiple lamps per channel.
The thresholds used in Figure 2 are summarized in Table 3, voltages with respect to ground. These values may differ for other parts.
Table 3. DS3994 LCM and OVD Thresholds (for Figure 2)
Parameter | Symbol | Min | Typ | Max | Units |
Lamp off threshold | VLOT | 1.65 | 1.75 | 1.85 | V |
Lamp overcurrent threshold | VLOC | 3.15 | 3.35 | 3.55 | V |
Lamp regulation threshold | VLRT | 2.29 | 2.35 | 2.41 | V |
OVD threshold | VOVDT | 2.25 | 2.35 | 2.45 | V |
Summary
- Each channel of the DS3xxx CCFL controller has four thresholds for lamp monitoring and regulation.
- The thresholds may appear with different values in the respective data sheets depending on the reference used.
- The thresholds are typically referenced to the DC bias voltage (VDCB) when the LCM and OVD signals are AC coupled. This approach typically applies to the single-lamp-per-channel applications.
- The thresholds are referenced to ground when the LCM and OVD signals are connected to the corresponding pins without AC-coupling capacitors. This design typically applies to applications with multiple lamps per channel.
Next Steps | ||
EE-Mail | Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest. | |
Download | Download, PDF Format |
© , Maxim Integrated Products, Inc. |
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.
APP 4637:
APPLICATION NOTE 4637, AN4637, AN 4637, APP4637, Appnote4637, Appnote 4637 |
maxim_web:en/products/power,maxim_web:en/products/power/display-power-control
maxim_web:en/products/power,maxim_web:en/products/power/display-power-control