APPLICATION NOTE 4325

Transmit Pulse Control on the DS26518 T1/E1/J1 Transceiver


Abstract: As network-protection components are added to a system and/or signals must be routed through connectors and other PC-board requirements, sometimes it is necessary to manipulate the transmit waveform. This application note explains how the DS26518 T1/E1/J1 transceiver contains precise methods for making minor or major changes to the output pulse. The note also describes how to access factory test registers that allow a designer to modify the transmit waveform to meet a wide variety of application requirements.