APPLICATION NOTE 4118

DS33R11 Multichip-Module BSDL Testing


Abstract: This application note describes how to alter the printed wiring board (PWB) netlist of a design containing the DS33R11T1/E1/J1 transceiver so that the netlist complies with the Joint Test Action Group (JTAG) specifications. These alterations are necessary because the DS33R11 was designed as a multichip module with multiple die in a single package which cannot be defined by the Boundary-Scan Description Language (BSDL) for board-level JTAG testing. The application note contains external pin mapping tables, internal die-pad bond tables, and contact information so the designer can quickly achieve accurate JTAG boundary-scan board testing.

Introduction

When manufacturing hardware for a telecommunications system, one of the basic tasks is to test the system for any production flaws. While there are many ways to test the hardware, one of the most popular methods uses the Joint Test Action Group (JTAG) boundary-scan method. The boundary-scan test method involves some minor changes to the hardware before production so that hardware verification can be performed after production. During design, all of the Integrated Circuit (IC) devices which support JTAG are connected in a serial daisy-chain fashion through the JTAG test access port. Verification is done by a specialized JTAG test system which connects to the test access port. The JTAG test system then uses a combination of the printed wiring board (PWB) netlist, Boundary-Scan Description Language (BSDL) files, and PWB connectivity test vectors to verify the pin-to-pin connections.

BSDL testing is straightforward. Nonetheless, multichip module devices like the DS33R11 Inverse-Multiplexing Ethernet Mapper with Integrated T1/E1/J1 Transceiver cannot be properly described by a single BSDL file because there are multiple die in a single package. This shortcoming can be overcome with simple modification to the PWB netlist and by using two BSDL files to describe the device package instead of just one.

Modifying the Printed Wiring Board Netlist

Before JTAG boundary scan testing can be performed, the portion of the PWB netlist that describes the external connections to the DS33R11 package must be modified to split those connections between the internal DS33Z11 die and DS2155 die. Once completed, the netlist will define the DS33R11 package with two independent reference designators. These reference designators allow two different BSDL files to individually describe the DS33Z11 and DS2155 connections inside the DS33R11 package.

Tables 1, 2, and 3 and Figure 1 make the task of modifying the netlist easy. Table 1 lists all of the external DS33R11 package pins which only connect to the DS33Z11 die. Table 2 lists all of the external DS33R11 package pins which only connect to the DS2155 die. Table 3 lists all of the external DS33R11 package pins which connect to both the DS33Z11 die and the DS2155 die. Figure 1 shows the same information in a format created for easier viewing.

This PWB netlist modification and JTAG boundary scan test have been performed using a Concise Net List format netlist of the DS33R11 engineering evaluation board designed with Cadence Concept. Designers can perform the operation in approximately 30 to 60 minutes, depending on the netlist type and individual’s skill level. Most of the edits to the netlist file can be done with a simple text editor. Depending on the netlist type, however, it may be possible to edit the netlist in a program such as Microsoft® Excel which can sort rows based on column data. However the editing is done, it is important to pay careful attention to detail. Irregular data such as header and footer information must be maintained, and the netlist must always be saved in the original format.

The following is a list of steps needed to complete the process.
  1. Open the netlist file in a text editor and group all of the nets connected to the DS33R11 reference designator. As an example, the DS33R11 package on the DS33R11 engineering evaluation board has a reference designator of U01.
  2. Separate all of the nets isolated in step 1 among those connected to the DS33Z11 die, those connected to the DS2155 die, and those connected to both die. Use Tables 1, 2, and 3 and Figure 1 to complete this task.
  3. Change the reference designator for all of the DS33Z11 nets from U01 to U01_D1 (short for reference designator U01, device 1). This step assumes that the DS33R11 reference designator is U01. If the reference designator is not U01, change U01_D1 appropriately.
  4. Change the reference designator for all of the DS2155 nets from U01 to U01_D2 (short for reference designator U01, device 2). This assumes that the DS33R11 reference designator is U01. If it is not U01, change U01_D2 appropriately.
  5. Duplicate the 22 shared nets so that there are exactly two of each. Split them into two groups.
  6. Change the reference designator for first group of nets created in step 5 from U01 to U01_D1. This assumes that the DS33R11 reference designator is U01. If it is not U01, change U01_D1 appropriately.
  7. Change the reference designator for second group of nets created in step 5 from U01 to U01_D2. This assumes that the DS33R11 reference designator is U01. If it is not U01, change U01_D2 appropriately.
  8. Save the newly created netlist.
The newly created PCB netlist will actually contain two instances for the DS33R11 physical device. The first instance will describe the pin connections related to the DS33Z11 section; the second will describe pin connections related to the DS2155 section. The new netlist can be loaded into any JTAG test suite along with the two DS33R11 BSDL files and any associated test vectors.

Although the method documented here has been tested and verified to work properly, there can be some unforeseen complications with other netlist formats. If additional assistance is needed during JTAG boundary scan testing, please use the contact information below for further assistance.

Table 1. Device Pins for DS33Z11 Die Only
Pin Description   Pin Description   Pin Description
A7 JTCLK1   L17 VDD3   V13 SDA[5]
A8 RST   L18 RXD[0]   V14 SDA[10]
A11 CS   L19 RXD[1]   V15 SMASK[3]
A15 VSS   L20 RXD[2]   V16 SMASK[2]
A19 REF_CLK   M17 VDD3   V17 SDATA[29]
A20 REF_CLKO   M18 RXD[3]   V18 SDATA[18]
B7 JTD1   M19 RX_CRS/CRS_DV   V19 SDATA[20]
B10 VDD1.8   M20 RX_CLK   V20 VSS
B15 VDD1.8   N17 VDD3   W1 SDATA[15]
B20 MODEC[1]   N18 COL_DET   W2 SDATA[0]
C7 JTRST1   N19 VSS   W3 SDATA[14]
C8 JTMS1   N20 VSS   W4 SDATA[9]
C9 JTDI1   P2 RDEN/RBSYNC   W5 SDATA[5]
C10 VSS   P17 VDD3   W6 SDATA[7]
C12 VDD1.8   P18 VDD1.8   W7 SCAS
C15 A9   P19 VDD1.8   W8 VSS
C16 A8   P20 VSS   W9 SRAS
C19 MDC   R17 VDD3   W10 SWE
C20 MDIO   R18 VDD3   W11 SDA[11]
D5 TDEN/TBSYNC   R19 VDD1.8   W12 SDA[1]
D8 VSS   R20 VDD1.8   W13 SDA[6]
D9 VSS   T17 VDD3   W14 SDA[0]
D10 VSS   T18 VDD3   W15 SDA[3]
D18 VSS   T19 SDATA[25]   W16 SDATA[31]
D19 VSS   T20 SDATA[26]   W17 SDATA[30]
D20 VDD3   U4 VSS   W18 VSS
E2 TSERO   U5 VSS   W19 SDATA[28]
E18 VSS   U6 VSS   W20 SDATA[23]
E19 TXD[3]   U7 VSS   Y1 VSS
E20 TXD[2]   U8 VSS   Y2 SDATA[2]
F1 TCLKE   U9 VSS   Y3 SDATA[4]
F2 RCLKI   U10 VSS   Y4 SDATA[1]
F3 VDD1.8   U11 VSS   Y5 SDATA[3]
F17 VDD3   U12 VSS   Y6 SMASK[0]
F18 TXD[1]   U13 VSS   Y7 VSS
F19 TXD[0]   U14 VSS   Y8 SDCLKO
F20 TX_EN   U15 VSS   Y9 VDD1.8
G17 VDD3   U16 VSS   Y10 SDA[9]
G18 VDD3   U17 VDD3   Y11 SBA[0]
G19 RMIIMIIS   U18 VSS   Y12 SDA[7]
G20 DCEDTES   U19 SDATA[22]   Y13 VDD1.8
H1 RSERI   U20 SDATA[24]   Y14 SDA[4]
H17 VDD3   V1 SDATA[13]   Y15 SDA[2]
H18 QOVF   V2 SDATA[11]   Y16 SDATA[16]
H19 TX_CLK   V3 SDATA[12]   Y17 SDATA[17]
H20 VSS   V4 SDATA[10]   Y18 SDATA[27]
J17 VDD3   V5 SDATA[6]   Y19 SDATA[19]
J18 VDD1.8   V6 SDATA[8]   Y20 SDATA[21]
J19 VSS   V7 SMASK[1]      
J20 VDD1.8   V8 SYSCLKI      
K17 VDD3   V9 VDD1.8      
K18 RX_ERR   V10 SDCS      
K19 RX_DV   V11 SBA[1]      
K20 VSS   V12 SDA[8]      

Table 2. Device Pins for DS2155 Die Only
Pin Description   Pin Description   Pin Description
A1 RCHBLK   D13 DVDD   L2 RVSS
A2 TCHBLK   D14 DVDD   L3 RSIG
A3 RFSYNC   D15 DVDD   L4 RNEGI
A4 TDATA   D16 DVDD   M1 RRING
A5 TSSYNC   D17 DVDD   M2 RVSS
A6 JTCLK2   E1 TPOSO   M3 RDCLKO
B1 BPCLK   E3 TSERI   M4 RDCLKI
B2 LIUC   E4 TSYSCLK   N1 RLOS/LTC
B3 TPOSI   E17 DVDD   N2 RNEGO
B4 TSIG   F4 RSYSCLK   N3 RPOSO
B5 RCL   G1 TCHCLK   N4 DVSS
B6 JTDI2   G2 RCHCLK   P1 TVSS
B8 JTRST2   G3 RCLKO   P3 RSIGF
B9 JTMS2   G4 RSYNC   P4 DVSS
C1 TSYNC   H2 RSERO   R1 TTIP
C2 TDCLKO   H3 RDATA   R2 TTIP
C3 TNEGI   H4 MCLK   R3 TVSS
C4 TSTRST   J1 RVSS   R4 DVSS
C5 JTDO2   J2 RVSS   T1 TRING
D1 TDCLKI   J3 RPOSI   T2 TRING
D2 TCLKT   J4 XTALD   T3 TVSS
D3 TNEGO   K1 RTIP   T4 DVSS
D4 TESO   K2 RVSS   U1 TVDD
D7 CST   K3 RVDD   U2 TVSS
D11 DVDD   K4 8XCLK   U3 RMSYNC
D12 DVDD   L1 RVDD      

Table 3. Shared Device Pins for DS33Z11 and DS2155 Die
Pin Description
A10 INT
A12 D6
A13 D3
A14 D0
A16 A6
A17 A3
A18 A0
B11 RD/DS
B12 D7
B13 D4
B14 D1
B16 A7
B17 A4
B18 A1
B19 MODEC[0]
C11 WR/RW
C13 D5
C14 D2
C17 A5
C18 A2

Figure 1. DS33R11 256-ball BGA, color-coded pinout and die map.
More detailed image
(PDF)
Figure 1. DS33R11 256-ball BGA, color-coded pinout and die map.

References
If you have additional questions on the JTAG testing of the DS33R11, please contact the Telecommunication Applications support team by email, , or telephone at 01-972-371-6555.

For more information about the DS33R11 Inverse-Multiplexing Ethernet Mapper with Integrated T1/E1/J1 Transceiver, please consult the appropriate data sheet at: T/E Carrier and Packetized Communications.