APPLICATION NOTE 4029

The DS8007 and Smart Card Interface Fundamentals


Abstract: The DS8007 is a multiprotocol, low-cost, dual, smart card interface that supports all ISO 7816, EMV™, and GSM11-11 requirements. This one mixed-signal peripheral manages all the details of the interface between a microcontroller and two, independent smart cards. This application note describes some of the fundamentals of smart cards and how to communicate with them. Software is provided that uses the DS8007 to interface a smart card with a DS5002 Secure Microprocessor.