Using a DS1307 with a PIC Microcontroller
Discussion
This application note demonstrates how to use the DS1307 real-time clock (RTC) with a Microchip PIC16F628 microcontroller.The example code, written in assembly code, includes a routine for reading the time and date from the RTC and a routine to write time and date data to the RTC from user entries.
Operation
The program uses two general-purpose port pins on the microcontroller to communicate with the DS1307 using the I²C serial interface. The microcontroller's internal UART drives two port pins, which are connected to a DS232 line driver/receiver. User inputs and data outputs from the program are passed through the RS-232 interface from a terminal emulator program on a PC to the microcontroller. The RS-232 DTR input line controls the microcontroller's reset input.The microcontroller in this example is a PIC16F628. For information on the microcontroller used in this application note, including available programming tools, visit the Microchip web site.
The software is shown in Figure 1. A schematic of the circuit is shown in Figure 2.

Download (TXT, 10kB)
Figure 1. Program Listing

More detailed image (PDF, 126kB)
Figure 2. Schematic drawing of the DS1307 circuit used with a PIC microcontroller.