APPLICATION NOTE 3806

Performance Test for a Serializer and Deserializer Pair: MAX9247 and MAX9218


Abstract: High-speed serialized data connection has been widely used in video displays, digital camera sensing, and backplane data transmission in networks, servers, and 3G base stations. Maxim developed products for serial link transmitters and receivers. This application note demonstrates the performance of a typical serializer and deserializer (SerDes) pair (the MAX9247 and MAX9218) under various cable type, cable length, and data rate conditions. The resulting information is a good guide for applications that require high-speed, serialized data connection.

Introduction

Maxim's high-speed serializer and deserializer (SerDes) products have been used in automotive, networking, server, and 3G base stations for video, image, and data transmissions. The MAX9247 serializer and the MAX9218 deserializer form a typical pair of a single LVDS link with embedded clock. The highest serial-link data rate, which the pair can reach, is up to 800Mbps.

This application note demonstrates the performance of this data transceiver link based on different cable types, cable lengths, and data rates. The article also shows the performance improvements that result from Maxim's proprietary pre-emphasis function and line equalizer. To meet the harsh environment in an automotive application, this SerDes pair is also tested in the -40°C to +105°C temperature range.

Test Setup

The test setup consists of an Agilent ParBERT 81250 tester, TDS784C 1GHz digital scope, TEK P6247 Differential probe, and the MAX9217/MAX9218 EV kit board. The Agilent 81250 is a parallel bit error rate tester (BERT). The components are connected as shown in the following illustration (Figure 1).

Figure 1. Performance test setup of the MAX9247 and MAX9218.
Figure 1. Performance test setup of the MAX9247 and MAX9218.

The MAX9247 has 27 bits of parallel data inputs in which 18 bits are for RGB video data inputs and 9 bits are for controlling data inputs. The data rate at the LVDS serialized link is 20 times the parallel data rate, including 2 overhead bits. The first 9 output channels of the Agilent 81250 are connected to the first 9 RGB inputs (RGB_IN0 to RGB_IN8). The inversed outputs of the first 9 channels are connected to the remaining 9 RGB inputs (RGB_IN9 to RGB_IN17). The BERT is only implemented on the RGB data. The data sequence on each of the ParBERT's output channels is an independently generated pseudo-random bit stream with a nonrepeating length of 21492. The RGB data sequence is 1370 bits long. After the 1370 bits, a 20-bit interval is added for the control period. All the control bits (CNTL_IN0 to CNTL_8) are always set to be zeros. Figure 2 shows the data structure. The 1390-bit parallel data pattern is repeated during the test. The signal DE_IN alternates the RGB data period and the control period.

Figure 2. Sequence structure for the test data.
Figure 2. Sequence structure for the test data.

Test Conditions and Measurement Results

We tested three twist-pair cables, as listed in the following table.

Table 1. Cable Types Under Test
Manufacturer Part Number Length(M) Comments
NISSEI SIODIC F-2WME, AWG26 10, 20, 30 Shielded
SIODIC F-2WME, AWG28 10, 20, 30
General Cable CAT5E, AWG24 10, 20, 30 Unshielded
JAE MX38 20 Shielded

To test the performance of the SerDes pair vs. cable length and data rate, we observe the bit error rate (BER) for each cable length and record the highest parallel data rate under which there is no bit error in ten minutes. The data rate increment is 1Mbps. We use this method to measure the performance because of two observations about the LVDS SerDes transceiver: first, if there is no error within ten minutes, there probably will be no error for a few hours; second, when error bits are observed within the ten minutes even at a very low rate, a slight increase of the data rate (<0.5Mbps) will cause the loss-lock of the DE_OUT signal at the deserializer. Consequently, our approach is a reasonable trade-off between the test time and the measurement reliability. Our hypothesis is, therefore, that the link BER is less than 10-10 or 10-11 when no bit error occurs within ten minutes at a certain data rate. Statistically, we can calculate the confidence level of this hypothesis using Equation 1:



where N is the number of bits transmitted through the serial link in the observation period (e.g., ten minutes) and p is the hypothesized BER. Table 2 provides the CL for different data rates.





Table 2. Confidence Level vs. Data Rates in a Ten-Minute Observation
Parallel Data Rate(Mbps) Number, N, of Bits
Transmitted by the
Serial Link in Ten Minutes
Confidence Level of p
BER < 10-10 BER < 10-11
10 12 x 1010 > 99.999% 69.88%
20 24 x 1010 > 99.999% 90.92%
30 36 x 1010 > 99.999% 97.27%
40 48 x 1010 > 99.999% 99.18%

Test Results

Table 3 shows the performance results which are obtained over various cable types, cable lengths, and data rates, and with the pre-emphasis function and the LVDS equalizer on or off. The pre-emphasis function is integrated in the MAX9247 and can be enabled by setting the jumper JP15 to 'High' on the EV board. The proprietary LVDS equalizer is mounted on the MAX9247's LVDS output, as shown in Figure 1. For details on implementing the equalizer, please contact Maxim Application Support. All the data in Table 3 were generated at room temperature. Test results with the 30m NISSEI AWG26 cable over the extended temperature range are shown in Table 4.

Table 3. Reliable Data Rates for a SerDes Transceiver Tested Under Various Conditions
Cable Type Pre-Emphasis LVDS Link Equalizer Maximum Reliable Serial Data Rate (SDR)
Cable Length
10m 20m 30m
PCLK (MHz) SDR (Mbps) PCLK (MHz) SDR (Mbps) PCLK (MHz) SDR (Mbps)
NISSEI AWG26 Off Off 34 612 25 450 15 270
On Off 40 720 27 486 17 306
Off On 38 684 34 612 30 540
On On 43 774 39 702 35 630
NISSEI AWG28 Off Off 33 594 16 288 8 144
On Off 36 648 23 414 10 180
Off On 35 630 33 594 23 414
On On 41 738 37 666 28 504
General Cable CAT5e Off Off 38 684 26 468 16 288
On Off 42 756 28 504 18 324
Off On 38 684 35 630 32 576
On On 44 792 42 756 36 648
JAE MX38 Off Off     16 288    
On Off     24 432    
Off On     35 630    
On On     40 720    

Table 4. Reliable Data Rates for a SerDes Transceiver Operating Over the Extended Temperature Range(*)
Cable Type Maximum Reliable Serial Data Rate (SDR)
Temperature
-40°C 25°C 105°C
PCLK (MHz) SDR (Mbps) PCLK (MHz) SDR (Mbps) PCLK (MHz) SDR (Mbps)
NISSEI AGW26, 30m 36 648 35 630 31 558

*Note that in this test, the pre-emphasis and LVDS equalizer are both on.

The following eye diagrams were recorded at the deserializer's LVDS input port. These plots show the deserializer's data recovery capability under the distorted bit symbols. We can also see the significant improvement by the LVDS link equalizer on the eye diagrams.

Figure 3. NISSEI AWG26, 20m at 702Mbps with pre-emphasis and equalizer.
Figure 3. NISSEI AWG26, 20m at 702Mbps with pre-emphasis and equalizer.

Figure 4. NISSEI AWG26, 30m at 630Mbps with pre-emphasis and equalizer.
Figure 4. NISSEI AWG26, 30m at 630Mbps with pre-emphasis and equalizer.

Figure 5. NISSEI AWG26, 30m at 306Mbps with pre-emphasis.
Figure 5. NISSEI AWG26, 30m at 306Mbps with pre-emphasis.

Figure 6. NISSEI AWG26, 30m at 306Mbps with pre-emphasis and equalizer.
Figure 6. NISSEI AWG26, 30m at 306Mbps with pre-emphasis and equalizer.

Summary

From the results shown in Tables 3 and 4, we can make the following observations.
  • Although CAT5E unshielded cable has the better performance than the other two types of cable, it could have EMI issues in applications.
  • Pre-emphasis and LVDS equalization help the link performance. Pre-emphasis gives bigger boost for a short cable and the later provides more efficient improvement for a longer cable. For the 30m cables, the equalizer could double the data rates.
  • The performance variation in the extended temperature range is relatively small.
  • The cable wire gauge could limit the performance. A wire gauge larger than AWG28 is recommended.

Reference

  1. Maxim High-Speed Interconnect Design Guide
  2. MAX9247 data sheet
  3. MAX9218 data sheet
Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format
© , Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.
APP 3806:
APPLICATION NOTE 3806,AN3806, AN 3806, APP3806, Appnote3806, Appnote 3806