APPLICATION NOTE 3742

MAX3735A: Special Considerations When Interfacing the MAX3735A to the DS1859


Abstract: The MAX3735A and the DS1859 are commonly used in 155Mbps to 2.7Gbps SFP module applications. These devices work well together by providing the high speed operation, safety circuitry and monitoring that is often used in such modules. However in some applications special care should be taken regarding the interface of the two devices.