APPLICATION NOTE 3614

Staggering the Burst Dimmer on CCFL Displays


Abstract: To reduce the instantaneous current demand on the DC inverter power supply, the DS3984/DS3988 cold-cathode fluorescent lamp controllers stagger the start of the burst dimming cycle for each of the channels of a backlit LCD display.

Figure 1 shows the delay of channels 1 through 4 staggered by the DS3984/DS3988 cold-cathode fluorescent lamp controllers. The other channels are staggered in a similar fashion by using the DS3988 for up to 8 channels, or by cascading multiple DS3984/DS3988 controllers for applications requiring additional channels.

Figure 1. DS3984/DS3988 staggered burst dimming delay on channels 1 to 4.
Figure 1. DS3984/DS3988 staggered burst dimming delay on channels 1 to 4.

Figure 2 shows the effect the staggered delay has on the current demand of the DC-inverter power supply. In this example, the burst dimming is set to approximately 50%. The power supply slowly ramps up to just over 3A, and then slowly returns to 0A.

Figure 2. DC inverter supply current ramp at 50% burst dimming.
Figure 2. DC inverter supply current ramp at 50% burst dimming.
Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
© , Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.
APP 3614:
APPLICATION NOTE 3614,AN3614, AN 3614, APP3614, Appnote3614, Appnote 3614