APPLICATION NOTE 3193

MAX3983: Designing for 10Gbase-CX4 Transmitter Template Compliance with the MAX3983


Abstract: The MAX3983 cable driver/receiver was optimized to achieve maximum cable span without the use of automatic/adaptive equalization techniques. After its release new copper cable interface standards were completed, the most stringent of which are found in the IEEE802.3's 10Gbase-CX4 transmitter output template. This discussion will aid in achieving CX4 compliance using the MAX3983. With the addition of a few passive components, the high performance MAX3983 can easily be adjusted to meet this tight template.


Related Parts
MAX3983 Free Sample
Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format
© , Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.
APP 3193:
APPLICATION NOTE 3193,AN3193, AN 3193, APP3193, Appnote3193, Appnote 3193