Coherent Sampling Calculator (CSC)
The purpose of coherent sampling is to force an integer number of input cycles within the sampling window. Figure 1 shows several examples of coherent sampling in the time domain.

Figure 1a.

Figure 1b.

Figure 1c.

Figure 1d.
Figure 1a-d. Coherently sampled data contains an integer number of cycles within the sampling window. These figures show four sets of coherently sampled data. Each data set has 13 cycles within the sampling window and contains 64 data points. NWINDOW=13, NRECORD=64
Mathematically, coherent sampling is expressed as:
where:![]()
- fIN is the input frequency of the ADC under test.
- fSAMPLE is the sampling frequency of the ADC under test.
- NWINDOW is the integer number of cycles within the sampling window. This value must be an odd or prime number.
- NRECORD is the number of data points used to create your FFT. This value must be a power of 2.
The "Coherent Sampling Calculator" requires four input variables:
- fDSAMPLE is the desired sampling frequency of the ADC under test.
- fDIN is the desired input frequency of the ADC under test.
- NRECORD is the number of data points used to create your FFTs. This value must be a power of 2.
- SIGFIG is the desired number of significant figures after MHz in the coherent sampling results.
The Coherent Sampling Calculator includes a macro that allows the user to view the detailed intermediate steps of the calculation process. By default, the spreadsheet is set to hide these detailed calculations, however by clicking the "Show_Detailed_Calculations" button the user can get additional information such as the size of the coherent sampling window (tCWINDOW) and the number of input cycles in the coherent sampling window (NCWINDOW).
Figures 2-3 show examples of coherently sampled FFTs taken using the coherent sampling calculator and the MAX1211EVKIT.

Figure 2. Coherently sampled FFT from the MAX1211EVKIT.
fCIN=20.0031266MHz
fCSAMPLE=65.0002432MHz
NCWINDOW=2521
NRECORD=8192

Figure 3. Coherently sampled FFT from the MAX1211EVKIT.
fCIN=32.1271954MHz
fCSAMPLE=65.0002432MHz
NCWINDOW=4049
NRECORD=8192