APPLICATION NOTE 2243

MAX2371 Makes a Terrific IF AGC Amplifier at 220MHz

By: Roger Bremer

Abstract: The MAX2371 is an ideal low-noise amplifier (LNA) at low IF frequencies when a large dynamic range of gain is needed. This part works at frequencies not specified in the data sheet. Specific to this note is the 220MHz frequency.

General Description

The MAX2371 is a low-noise amplifier (LNA) IC designed for very low intermediate frequency receiver applications. The LNA features both a switched attenuator and an automatic gain control (AGC) intended as a low-noise gain stage. Between these two features, the device provides over 65dB of gain-control range. The LNA has a selectable current mode. When high current mode is selected, the IC will perform with maximum gain, IP3 and low noise figure. When peak performance is not required, low-current mode slightly degrades the aforementioned parameters while reducing current consumption.

Although the MAX2371 is specified in its data sheet as operating between 136 and 174 MHz, the part also functions well at other frequencies. The data in this note documents performance at 220MHz. The only change required to use the MAX2371 at this alternative frequency is to update the component values for the input and output matching networks. The values used are represented in the MAX2371 EVKit Schematic and BOM included at the end of this note.

Test Setup

Test Conditions:
1) Vcc = 2.85 V
2) Frequency = 220 MHz
3) Input Power = -30 dBm
4) Two Tone Spacing = 625 kHz
5) RF_ATTN = LOW
6) LNA_I = HIGH

Test Setup Diagram:

Figure 1. Diagram of the LNA test setup used to evaluate the MAX2371.
Figure 1. Diagram of the LNA test setup used to evaluate the MAX2371.

Measurement Results

Parameter Measured Data Comment
Max. Gain(dB) 12.5 Vgc = 1/2 Vcc
Noise Figure(dB) 2.2 Vgc = 1/2 Vcc
IIP3(dBm) 1.5 Vgc = 1/2 Vcc
Dynamic Range(dB) 55.0 From VGC
Gain Step (dB) 17.5 From RF_ATTN
Icc over Gain(mA) 3.7

Gain, IIP3, P1dB

IIP3, P1dB and Gain were measured for the MAX2371 over control voltage and temperature to show all operating conditions. Three temperatures were tested (-10°C, +25°C, +70°C) along with 8 AGC voltages. The results are plotted below.

Figure 2. The downward sloped curve set shows that  Gain varies less than 0.3dB over temperature.
Figure 2. The downward sloped curve set shows that Gain varies less than 0.3dB over temperature.

Figure 3. IIP3 has a variance of approximately 3.5dB over temperature.
Figure 3. IIP3 has a variance of approximately 3.5dB over temperature.

Figure 4. Input P1dB varies by less than 2dB over temperature.
Figure 4. Input P1dB varies by less than 2dB over temperature.

MAX2371 IF Amplifier Circuit S11 and Circuit S22

S11 and S22 were measured against control voltage. The results are plotted below. The input and output were each matched to 50 ohms using single section L-C matches.

Figure 5. Variance of S11 and S22 over VGC range.
Figure 5. Variance of S11 and S22 over VGC range.

Conclusion

This study of the MAX2371 illustrates its effectiveness and viability as an LNA at 220MHz. The IC provides good noise figure and low current consumption while offering a wide gain range.

MAX2371 EVKit Schematic

Figure 6.
Figure 6.

MAX2371 EVKit BOM

Item Reference Description Value
1 C1 0402 Capacitor Open
2 C10 0402 Capacitor 0.015uF
3 C19 Capacitor 100nF
4 C2 0402 Capacitor 8.2pF
5 C3 0402 Capacitor Open
6 C4 0402 Capacitor 1500pF
7 C5 0402 Capacitor 1500pF
8 C6 0402 Capacitor 4.7pF
9 C7 0402 Capacitor Open
10 C8 0805 Capacitor 1.0uF
11 C9 Capacitor 10nF
12 J1-3 Three PIN INLINE HEADER
13 J4 SIX PIN INLINE HEADER
14 J5-6 Two PIN INLINE HEADER
15 L1 0603 Inductor Open
16 L2 39nH
17 L4 0603 Inductor 33nH
18 L5 Inductor 82nH
19 P1-2 SMA Connector
20 R1 1.1K
21 R2 220
22 R3 0
23 U1 MAX2371EGC LNA/AGC Attenuator