Additional Information:
This application note describes a method to achieve local oscillator (LO) phase noise performance of nearly
-90dBc/Hz (at 10kHz offset) using the MAX2309 I/Q demodulator. A complete 100MHz intermediate frequency (IF) design solution is offered including voltage controlled oscillator (VCO), loop filter components, and performance plots.
Objective
Optimize the MAX2309 evaluation kit for LO phase noise as measured at the LO buffer output.
Procedure
A standard MAX2309 evaluation kit was obtained and the VCO tank components were re-configured, allowing for oscillation at 200MHz (twice the IF Frequency) with K
VCO = 6.6MHz/V. Please see the MAX2309 evaluation kit schematic for reference designator locations. The component values are shown in
Table 1.
Table 1. VCO Component Changes
Reference Designator |
New Value (200MHz) |
Part Number |
Manufacturer |
L5 |
82nH |
0805CS-820XKBC |
Coilcraft |
C61 |
3.9pF |
COG capacitor |
Murata |
C4, C6 |
27pF |
COG capacitor |
Murata |
D3, D5 |
Varactor |
SMV1763-079 |
Alpha-Industries |
Loop Filter Design 1
The loop filter component values are shown in
Table 2. This loop is designed for a unity gain frequency of 11.6kHz with 50° phase margin, and a 425µA charge pump current.
Table 2. Loop Filter #1
Reference Designator |
Filter Value |
C30 |
560pF |
R23 |
5.1kΩ |
C29 |
5.6nF |
R10 |
0Ω |
C31 |
Open |
Figure 1. 100MHz LO signal at LO buffer output ICP = 425µA, HP8561E.
Figure 2. Phase noise of 100MHz LO signal, HP8561E.
Important Note: Originally phase noise was measured at approximately -80dBc/Hz, however it was determined that the 13MHz reference source possessed less than acceptable noise output itself. The source was changed to a KSS VC-TCXO-208C-13.0 and phase noise improved by approximately 6dB.
Table 3. Key Test Parameters
Parameter |
Value |
Units |
VCC |
3.0 |
V |
FIF |
100 |
MHz |
FREF |
13 |
MHz |
FOSC |
200 |
MHz |
FCOMP |
1 |
MHz |
KVCO |
6.6 |
MHz/V |
Target Phase Noise at 10kHz |
-90 |
dBc/Hz |
TA |
+25 |
°C |
Loop Filter Design 2
After measuring phase noise with the modified VCO and loop filter, a second loop filter was evaluated. This filter was designed for a narrower loop bandwidth with a 9kHz unity gain frequency, 53° phase margin, and 425µA charge pump current. The values are shown in
Table 4.
Table 4. Loop Filter #2
Reference Designator |
Filter Value |
C30 |
1nF |
R23 |
3.9kΩ |
C29 |
10nF |
R10 |
0Ω |
C31 |
Open |
The phase noise was measured and the results are shown in
Figure 3 and
Figure 4.
Figure 3. 100MHz LO signal at LO buffer output ICP = 425µA, HP8561E.
Figure 4. Phase noise of 100MHz LO signal, HP8561E.
Finally, a 210µA charge pump current was selected to further reduce the loop bandwidth. This resulted in much improved phase noise at 10kHz offset at the expense of tuning speed. This loop has a unity gain frequency of 5kHz and still has very good phase margin of 44°. The final results are shown in
Figure 5 and
Figure 6.
Figure 5. 100MHz LO signal at LO buffer output ICP = 210µA, HP8561E.
Figure 6. Phase noise of 100MHz LO signal, HP8561E.
Figure 7. The MAX2309 Evaluation Board, 100MHz LO, Phase-noise optimized.
Figure 8. The MAX2309 Evaluation board.
Figure 9. The MAX2309 Evaluation board (cont.).
Conclusion
The MAX2309 is capable of achieving approximately -90dBc/Hz phase noise at 10kHz offset. While quite dependent on the reference oscillator spectral purity, loop filter design, and charge pump current, the end result is ultimately achievable once optimized.
© , Maxim Integrated Products, Inc.
|
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content,
contact us.
APP 1744:
APPLICATION NOTE
1744,
AN1744,
AN 1744,
APP1744,
Appnote1744,
Appnote 1744
|
maxim_web:en/products/power/display-power-control/display-drivers,maxim_web:en/products/comms/wireless-rf
maxim_web:en/products/power/display-power-control/display-drivers,maxim_web:en/products/comms/wireless-rf