APPLICATION NOTE 1016

Autotransformer Regulator Inverts 12V to -12V


Abstract: The autotransformer provides an alternative means of extending the output voltage range of an inverting DC-DC regulator besides using an external MOSFET or a flyback transformer. With an autotransformer, the input-output voltage can be extended beyond the specification limit of the integrated circuit (IC).

In Figure 1, a dc-dc regulator with internal switching MOSFET inverts 12V to produce an output of 200mA at -12V. The IC is a high-efficiency device whose low quiescent current (120µA maximum) is achieved with a CMOS process that limits the absolute maximum voltage to 21V (input to output). Thus, to avoid 24V across its terminals, the IC must isolate itself from the inductor-flyback voltage by driving either an external switch in a non-bootstrapped configuration, or an internal switch in a flyback-transformer configuration.

Figure 1. Autotransformer T1 limits the voltage across IC1, allowing use of a high-efficiency chip (with 21V absolute-maximum voltage) in this inverting dc-dc regulator.
Figure 1. Autotransformer T1 limits the voltage across IC1, allowing use of a high-efficiency chip (with 21V absolute-maximum voltage) in this inverting dc-dc regulator.

Autotransformer T1 (a center-tapped inductor with 1:1 turns ratio) offers a design alternative. In the circuit shown, LX flies back to 1/2VOUT plus a diode drop, or approximately -6V. V+ remains at 12V, producing an 18V maximum between V+ and LX that is well within the 21V limit.

Because IC1 drives the gate of its internal MOSFET between the V+ and OUT voltages, you normally connect OUT to VOUT to ensure sufficient gate drive (in a typical application, the chip inverts 5V to -5V). In this circuit the 12V input provides adequate gate drive, so OUT is connected to ground.


Related Parts
MAX764 Free Sample
Next Steps
EE-Mail Subscribe to EE-Mail and receive automatic notice of new documents in your areas of interest.
Download Download, PDF Format
© , Maxim Integrated Products, Inc.
The content on this webpage is protected by copyright laws of the United States and of foreign countries. For requests to copy this content, contact us.
APP 1016:
APPLICATION NOTE 1016,AN1016, AN 1016, APP1016, Appnote1016, Appnote 1016