The MAX7034 receiver reference design (RD) is a self-contained evaluation platform for exercising the product as a tube motor receiver module. This receiver (Rx) board includes a simple power supply, data interface, and an antenna connection, all in a small modular form factor that allows the receiver to be placed inside of a tubular enclosure. The Rx board was manufactured to be usable as-is. Gerber files are available for simple cut-and-paste of the radio system design.
The MAX7034 315MHz/434MHz amplitude-shift-keyed (ASK) superheterodyne receiver is configured in a near-standard form similar to the typical application circuit illustrated in the MAX7034 data sheet. The system is targeted for 433.92MHz operation and a 1kbps (NRZ) data rate. Four resistor connections are included in the design to allow flexible use of certain pins. Two connections have resistor footprints but are wired as shorts: R5 connects IR_SEL to VDD and R6 connects EN_REG to VDD. Two other connections are left open (unpopulated): R4 can connect DSP to DATAOUT for hysteresis and R7 can connect DSN to 3V3 for squelch. The module is designed to have a small footprint with minimal connections, to include a pair of pins for antenna/ground connections and a triplet of pins for ground/RX data/power connections. The board uses a 5V power supply.
Populated Rev-A2 board
The MAX7034 receiver reference design (RD) is a self-contained evaluation platform for exercising the product as a tube motor receiver module. This receiver (Rx) board includes a simple power supply, data interface, and an antenna connection, all in a small modular form factor that allows the receiver to be placed inside of a tubular enclosure. The Rx board was manufactured to be usable as-is. Gerber files are available for simple cut-and-paste of the radio system design.
The MAX7034 315MHz/434MHz amplitude-shift-keyed (ASK) superheterodyne receiver is configured in a near-standard form similar to the typical application circuit illustrated in the MAX7034 data sheet. The system is targeted for 433.92MHz operation and a 1kbps (NRZ) data rate. Four resistor connections are included in the design to allow flexible use of certain pins. Two connections have resistor footprints but are wired as shorts: R5 connects IR_SEL to VDD and R6 connects EN_REG to VDD. Two other connections are left open (unpopulated): R4 can connect DSP to DATAOUT for hysteresis and R7 can connect DSN to 3V3 for squelch. The module is designed to have a small footprint with minimal connections, to include a pair of pins for antenna/ground connections and a triplet of pins for ground/RX data/power connections. The board uses a 5V power supply.
Populated Rev-A2 board
The LFRD014 is designed as a demonstration platform for the MAX7034 receiver, using a very small form factor. It targets a low-cost, low bill-of-materials (BOM) count RF link—in this case, a tube motor application. The layout incorporates all of the required BOM on a 0.48-inch × 1.32-inch board. The IF filter and crystal both use footprints targeted for older, through-hole mounted components (at a lower cost). A pair of shunt capacitors is included on the crystal pins for minor frequency adjustment. The input network consists of a series cap (C4), series inductor (L1), shunt cap (C5), and a second series cap (C6). A placeholder is provided for the LNA source inductor (L2), but a short-to-ground is recommended. An inductor (L3) capacitor (C7) pair acts as the tank circuit, but it is recommended that the capacitor not be populated.
Power to the Rx board is commonly supplied by a regulated 5V source, such as one generated from line voltage using a wall transformer (Table 1).
Table 1. Rx I/O Headers | |
Header | Signal Description |
---|---|
ANT-1 | RX-ANT, antenna connection |
ANT-2 | GND, antenna ground connection |
POWER-1 | GND, supply ground connection |
POWER-2 | RXDATA, module output data connection |
POWER-3 | V5V, supply 5V power connection |
Supply current (IDD) at fRF = 433MHz, +5.0V | 7.2mA (typ) |
Shutdown supply current (I%-overbar_pre%SHDN%-overbar_post%) at fRF = 433MHz, +5.0V | 8µA (max) |
Sensitivity (PRFIN_MIN) (peak power level) | -113dBm (typ) |
For testing and debugging purposes, the LFRD014 board was configured with an incorrectly specified crystal and no adjustments were made for parasitic board influences. Initial sensitivity testing for this configuration measured -94.6dBm at a 0.2% bit-error rate (BER) level.
The receiver matching network is similar to the network suggested in the MAX7034 data sheet, which assumes a 50? antenna. A degeneration inductor from the low-noise amplifier (LNA) source pin of the MAX7034 (LNASRC) to ground can be populated in the LFRD014 to adjust the input impedance of the LNA. When the degeneration inductor is present, the LNA input impedance looks like a 50Ω resistor in series with a 2pF to 2.5pF capacitor (without the inductor, the input impedance looks like a 500Ω to 700Ω resistor in parallel with a 2pF to 2.5pF capacitor). These impedance models can be used to design matching networks for any antenna impedance. Note when the antenna impedance is 50?, the matching network is typically a series inductor (with a DC-blocking capacitor). During range testing of the LFRD014 module, a 17.2cm (1/4 wavelength) wire antenna was used.
One of the most common challenges associated with crystal-based receivers and transmitters is the proper tuning of the radio's oscillation circuit. The oscillator on the MAX7034 is intended to operate using a crystal specified with a 3pF load capacitance. This low value is not a very common specification for crystals; typically customers attempt to design a system using a crystal with a tested load capacitance of 6pF, 8pF, 10pF, or more, often due to cost or supply considerations. Using these crystals is not prohibited, but doing so presents a trade-off since the MAX7034 still only provides about 3.1pF of load to the crystal pins. This loading will cause a 10pF specified crystal to operate at a noticeably higher frequency than intended (see application note 1017, "How to Choose a Quartz Crystal Oscillator for the MAX1470 Superheterodyne Receiver" for further information). To compensate for this shift in frequency, a customer can present a larger load to the crystal by placing capacitors in the circuit. We recommend two shunt capacitors to ground rather than a parallel arrangement for enhanced flexibility and other loading benefits. The trade-off with this "adjusted" load is that too much capacitance connected to the circuit could cause a problem with the oscillation startup.
For demonstration purposes, the LFRD014 was populated with a 13.2256MHz crystal that had a specified CL of 8pF. A debug measurement was made to investigate the oscillating frequency of the crystal populated on the PCB. To perform this test, an R&S® ZVL3 spectrum analyzer and a "sniffer" antenna were used to probe the crystal frequency. This antenna was held in close proximity to the crystal (or touching one of the leads as needed) to obtain an estimate of the operating frequency. The peak was measured at 13.23049MHz, which is high by 370ppm. This translates to an operating frequency of 434.085MHz (32 × 13.23049 + 10.7), which placed the expected LO and carrier frequency at 165kHz—higher than intended. This off-frequency operation of the crystal oscillator resulted in an incoming ASK carrier and associated sidebands that were pushed to the edge or even past the knee of the IF filter. This caused an unnecessary attenuation of the signal power.
To further test the impact of this error, the passband of the IF was tested. By sweeping the carrier signal in frequency and monitoring the IF filter output with the spectrum analyzer (in max-hold mode) a plot of the filter bandwidth was collected. Marker M1 was placed at 10.7MHz (nominal center of the IF filter) and the delta marker D2 was placed at the frequency spike where the RF signal was tuned to 433.92MHz. The signal generator was set to 434.085MHz when the IF spike was at M1, confirming the shift in LO frequency. The plot illustrated in Figure 1 shows that the mistuning degrades the carrier by about 7dB. Sideband information needed for ASK demodulation is actually attenuated further, as well as being distorted due to the nonlinear location on the filter curve.
Figure 1. IF filter bandwidth, max-hold sweep.
The following entries were used for the estimates for a specified load capacitance of the crystal at 8pF: MAX7034; CPAR = 1.8pF; CSHUNT = 0pF; CSER = 10000pF; f0 = 13.2256MHz; C0 = 2.8pF; CL = 8.24pF; R1 = 60Ω; C1 = 11.1fF. With these values, the pulling calculation showed an actual RF frequency of 434.0853MHz. Then by adding experimental shunt capacitance values, a pair of 10pF capacitors will adjust the oscillation frequency back to the target value and, assuming the other crystal values are well estimated, the startup margin will be acceptable. The negative resistance calculation was -291.5Ω, compared to 4 × R1 of 240Ω. This left about -50Ω of additional margin.
As a first-order attempt to improve the sensitivity of the demonstration LFRD014 module, two 10pF shunt caps were added at C21 and C22. The resulting crystal oscillator frequency was confirmed to have moved and was now operating at the corrected frequency of 13.226MHz. After adjusting the RF generator to be centered back at 433.92MHz, sensitivity measured in at -107dBm. This 12.4dB improvement resulted from the proper tuning of the reference frequency for the local oscillator.
The next step to optimize the receiver is to make sure the tank circuit at the LNA output and mixer input is well tuned to the operating frequency. This off-chip inductor-capacitor pair provides a tuned, high-impedance circuit that converts the LNA current output into a voltage, which in turn is fed to the on-chip mixer.
In order to measure the tuning frequency of the tank circuit, a network analyzer is needed. Some of this data can be collected manually with an RF generator and a spectrum analyzer, but a two-port NA is the best tool for the job. The measurement stimulus comes from Port 1 of the NA, which is connected to the LNA input through the antenna feed. The measurement is taken by using a sniffer antenna connected to Port 2 of the network analyzer. This untuned antenna can be held in close proximity to the inductor of the tank circuit, where it will pick up radiated emissions at the circuit's resonant frequency and provide an S21 measurement. The use of a -20dBm or -30dBm source power setting is recommended to avoid putting the LNA input into overdrive.
The suggested component values for the tank circuit are a 27nH inductor in parallel with no capacitor, simply to allow the parasitics of the PCB to act as the resonant capacitive element. The resonant frequency of a tank circuit can be calculated from the following equation:
The predicted range in a flat unobstructed outdoor area is based on the following assumptions:
The following table provides a list of components used to populate the Rx board. Maxim recommends high-quality, wire-wound inductors for components used on the board.
Designation | Qty | Description |
---|---|---|
C2 | 1 | CAP, 0.01µF, 10% |
C1 C3 | 2 | CAP, 0.1µF, 10% |
C14 | 1 | CAP, 0.47µF, 10% |
C8-9 | 2 | CAP, 100pF, 5% |
C6 | 1 | CAP, 10pF, 5% |
C11 C13 | 2 | CAP, 1500pF, 5% |
C4 | 1 | CAP, 2.2pF, 5% |
C10 | 1 | CAP, 220pF, 5% |
C5 | 1 | CAP, 3.3pF, 5% |
C12 | 1 | CAP, 750pF, 5% |
C7 C21-22 | 3 | CAP, Open |
F1 | 1 | FLT\MURATA\SFTLA10M7FA00-B0, 10.7MHz |
L3 | 1 | IND-MOLDED, 27nH, 5% |
L1 | 1 | IND-MOLDED, 33nH, 5% |
U2 | 1 | MAX7034 |
R5-6 L2 | 3 | RES, 0Ω |
R2-3 | 2 | RES, 10kΩ |
R1 | 1 | RES, 20kΩ |
Y2 | 1 | XTAL-SMD, 13.2256Mhz |
Total Rx Cost (~1k quantities): | Rx BOM | $2.63 |
PCB | $0.50 | |
As configured | $3.13 |
(Revision A2: a detailed copy is available here.)
More detailed image. (PDF, 265KB)
(Revision A2: detailed scale plots are available here.)
Application note 1017, "How to Choose a Quartz Crystal Oscillator for the MAX1470 Superheterodyne Receiver"
Application note 2815, "Calculating the Sensitivity of an ASK Receiver"
Application note 3435, "Manchester Data Encoding for Radio Communications"
Application note 3671, "Data Slicing Techniques for UHF ASK Receivers"
Application note 4636, "Avoid PC-Layout Gotchas in ISM-RF Products"
Application note 5142, "Radio Link-Budget Calculations for ISM-RF Products"
The following plots show the packet transmissions from the key fob as decoded by the LFRD014 receiver. These plots were used to indicate range by qualitatively assessing the signal received by the reference design. Since a matching decoder was not available at the time of testing, a true operating range was not determined.
Rx data oscilloscope capture (zoomed in).
Rx data oscilloscope capture.
Rx data "out-of-range" noise.
R&S is a registered trademark and registered service mark of Rohde & Schwarz GmbH & Co. KG.