Top

Offline LED Driver Reference Design

Reference Design Disclaimer See the  Important Notice and Disclaimer  covering reference designs and other Maxim resources.

Description

Brief Circuit Description

This reference design is a flyback LED driver for offline environments (400VDC). The design can drive 27 WLEDs (white LEDs) at 400mA. With the jumper, J1, installed, the design drives 6 amber LEDs at 400mA. The design uses the MAX16801 HB LED controller and a three-winding transformer (coupled inductor). There is no electrical isolation as the current sense is fed directly into the IC control loop.

The transformer has an 18:6:1 turns ratio. Primary inductance is 800µH with a current rating of 750mA (peak) and a duty cycle always less than 50%.

The frequency of operation is 265kHz and is nonadjustable. Overvoltage protection (nonlatching) is at 120V. The UV detect level is 310V. The turn-on delay time is about 43msec, after which VIN will be about 22V and the IC will begin to drive the external MOSFET. This will, in turn, cause the VIN capacitor to decay until the bootstrap winding can provide support. Because of the high impedance of the LEDs at low voltage, the main secondary load will initially be only the output capacitor. The secondary-to-tertiary turns ratio is 6:1, which means that the bootstrap winding will supply 10V to the IC as soon as 60V develops across the output capacitor. For the 6-LED string option (i.e., with J1 installed), the output capacitor must, obviously, charge to 10.7V before 10V is available to the IC.

The calculated peak current in the primary winding of the inductor is 750mA. Leakage inductance is minimized by a split primary that sandwiches the secondary winding. The primary leakage inductance is measured at less than 5µH. Because of this low value, there is no special provision for dissipating the leakage inductance energy; all leakage energy is dissipated in the MOSFET itself. The transformer temperature rise is less than 30°C.

The switching MOSFET has an isolated tab, which allows the heatsink to be connected to ground. This minimizes the metallic surface area that experiences high-speed voltage transients, and, in turn, minimizes radiated EMI. The MOSFET sees less than a 40°C rise in temperature.

VIN: 400VDC ±10%
PWM: N/A
VLED config.: 27 LEDs (2.8VDC to 4VDC) in series (75.6VDC min to 108VDC max); 400mA
With jumper: 6 LEDs (2VDC to 3VDC) in series (12V min to 18V max); 400mA

Figure 1. The LED driver reference design is 1.9in x 3.9in, double sided.
More detailed image
 (PDF, 35.6kB)
Figure 1. The LED driver reference design is 1.9in x 3.9in, double sided.

Figure 2. Schematic of the LED driver reference design.
Figure 2. Schematic of the LED driver reference design.

Figure 3. Board layout of the LED driver.
More detailed image
 (PDF, 36.88kB)
Figure 3. Board layout of the LED driver.

Figure 4. Transformer specifications.
More detailed image
 (PDF, 88.75kB)
Figure 4. Transformer specifications.

Figure 5. BOM for the reference design.
More detailed image
 (PDF, 76.43kB)
Figure 5. BOM for the reference design.

Icon

Designed, Built, Tested

Board pictured here has been fully assembled and tested. Not available for sale.

 

Related Videos

View All Videos