Magnetic Resonance Imaging (MRI)

Description

Magnetic resonance imaging (MRI) systems provide highly detailed images of tissue in the body. The systems detect and process the signals generated when hydrogen atoms, which are abundant in tissue, are placed in a strong magnetic field and excited by a resonant magnetic excitation pulse. Hydrogen atoms have an inherent magnetic moment as a result of their nuclear spin. When placed in a strong magnetic field, the magnetic moments of these hydrogen nuclei tend to align. Simplistically, one can think of the hydrogen nuclei in a static magnetic field as a string under tension. The nuclei have a resonant, or "Larmor," frequency determined by their localized magnetic field strength, just as a string has a resonant frequency determined by the tension on it. For hydrogen nuclei in a typical 1.5T MRI field, the resonant frequency is approximately 64MHz.

More

Gradient Coils


To produce an image, the MRI system must first stimulate hydrogen nuclei in a specific 2D image plane in the body, and then determine the location of those nuclei within that plane as they precess back to their static state. These two tasks are accomplished using gradient coils which cause the magnetic field within a localized area to vary linearly as a function of spatial location. As a result, the resonant frequencies of the hydrogen nuclei are spatially dependent within the gradient. Varying the frequency of the excitation pulses controls the area in the body that is to be stimulated. The location of the stimulated nuclei as they precess back to their static state can also be determined by using the emitted resonant RF-frequency and phase information. An MRI system must have x, y, and z gradient coils to produce gradients in three dimensions and thereby create an image slice over any plane within the patient’s body. The application of each gradient field and the excitation pulses must be properly sequenced, or timed, to allow the collection of an image data set. By applying a gradient in the z direction, for example, one can change the resonant frequency required to excite a 2D slice in that plane. Therefore, the spatial location of the 2D plane to be imaged is controlled by changing the excitation frequency. After the excitation sequence is complete, another properly applied gradient in the x direction can be used to spatially change the resonant frequency of the nuclei as they return to their static position. The frequency information of this signal can then be used to locate the position of the nuclei in the x direction. Similarly, a gradient field properly applied in the y direction can be used to spatially change the phase of the resonant signals and, hence, be used to detect the location of the nuclei in the y direction. By properly applying gradient and RF-excitation signals in the proper sequence and at the proper frequency, the MRI system maps out a 3-D section of the body. To achieve adequate image quality and frame rates, the gradient coils in the MRI imaging system must rapidly change the strong static magnetic field by approximately 5% in the area of interest. High-voltage (operating at a few kilovolts) and high-current (100s of amps) power electronics are required to drive these gradient coils. Notwithstanding the large power requirements, low noise and stability are key performance metrics, since any ripple in the coil current causes noise in the subsequent RF pickup. That noise directly affects the integrity of the images. To differentiate tissue types, the MRI systems analyze the magnitude of the received signals. Excited nuclei continue to radiate a signal until the energy absorbed during the excitation phase has been released. The time constant of these exponentially decaying signals ranges from tens of milliseconds to over a second; the recovery time is a function of field strength and the type of tissue. It is the variations in this time constant that allow different tissue types to be identified.

Back to Top |

Transmit/Receive Coils


Transmit and receive coils are used both to stimulate the hydrogen nuclei and to receive the signals generated as the nuclei recover. These coils must be optimized for the particular body area to be imaged, so they are available in a wide variety of configurations. Depending on the area of the body to be imaged, either separate transmit and receive coils or combined transmit/receive coils are used. In addition, to improve image acquisition times, MRI systems use multiple transmit/receive coils to recover more information in parallel, thus utilizing the spatial information associated with the location of the coils.

Back to Top |

RF Receiver


An RF receiver is used to process the signals from the receiver coils. Most modern MRI systems have six or more receivers to process the signals range from approximately 1MHz to 300MHz, with the frequency range highly dependent on applied static magnetic field strength. The bandwidth of the received signal is small, typically less than 20kHz, and dependent on the magnitude of the gradient field. A traditional MRI receiver configuration has a low-noise amplifier (LNA) followed by a mixer. The mixer mixes the signal of interest to a low-frequency IF frequency for conversion by a high-resolution, low-speed, 12-bit to 16-bit analog-todigital converter (ADC). In this receive architecture, the ADCs used have relatively low sample rates below 1MHz. Because of the low-bandwidth requirements, ADCs with higher 1MHz to 5MHz sample rates can be used to convert multiple channels by time-multiplexing the receive channels through an analog multiplexer into a single ADC.

With the advent of higher performance ADCs, newer receiver architectures are now possible. High-input-bandwidth, high resolution, 12-bit to 16-bit ADCs with sample rates up to 100MHz can also be used to directly sample the signals, thereby eliminating the need for analog mixers in the receive chain.

Back to Top |

Transmitter


The MRI transmitter generates the RF pulses necessary to resonate the hydrogen nuclei. The range of frequencies in the transmit excitation pulse and the magnitude of the gradient field determine the width of the image slice. A typical transmit pulse will produce an output signal with a relatively narrow ±1kHz bandwidth. The time-domain waveform required to produce this narrow frequency band typically resembles a traditional sync function. This waveform is usually generated digitally at baseband and then up converted by a mixer to the appropriate center frequency. Traditional transmit implementations require relatively low-speed, digital-to-analog converters (DACs) to generate the baseband waveform, as the bandwidth of this signal is relatively small.

Again, with recent advances in DAC technology other potential transmit architectures are achievable. Very-high-speed, high-resolution DACs can be utilized for direct RF generation of transmit pulses up to 300MHz. Waveform generation and up conversion over a broad band of frequencies can, therefore, now be accomplished in the digital domain.

Back to Top |

Image Signal Processing


Both frequency and phase data are collected in what is commonly referred to as the k-space. A two dimensional Fourier transform of this k-space is computed by a display processor/computer to produce a gray-scale image.

Back to Top |


Soundmatters Dash7 Portable Speaker

Soundmatters’s Dash7 portable speaker is part of the company’s portfolio of high-quality, ultra-small audio systems.

Webinar: The Critical Role of Actionable Insights for the Wearable Healthcare Revolution

A revolution in wearable patient monitoring is allowing medical professionals to proactively manage preventative care needs and chronic conditions, In this webinar, wearable device developers will learn how to take advantages of multiple sensor measurements to improve the accuracy of actionable insights for remote patient monitoring.

Learn more: Maxim's Sensor Experience ›

Learn more: Healthcare ›

Ultra-Low Power PMIC with 3-Output Buck-Boost, 2-LDOs and Power-Path Charger

MAX77654

Provides highly-integrated battery charging and power-supply solutions for applications where power, size and efficiency are critical.

Learn more ›

Introduction to the MAX20459 Automotive High-Current Step-Down Converter with USB-C Protection/Host Charger

This video provides an introduction to Maxim's Automotive High-Current Step-Down Converter with USB-C Protection/Host Charger - the MAX20459.

Introduction to MAX77958 Standalone USB-C Power Delivery Controller

This video provides an introduction to Maxim's Standalone USB-C Power Delivery Controller - the MAX77958.

Introduction to the MAX16545B MAX16545C, and MAX16543 Integrated Protection IC on 12V Bus with an Integrated MOSFET, Lossless Current Sensing, and PMBus Interface

This video provides an introduction to Maxim’s protection solution for high-current +12V power: the MAX16545B/C and MAX16543.

Introduction to the MAX31825 1-Wire® Temperature Sensor With ±1°C Accuracy

This video provides an introduction to Maxim's 1-Wire® Temperature Sensor With ±1°C Accuracy - the MAX31825.

Introduction to the MAX40002 MAX40003 MAX40004 MAX40005 MAX40014 NanoPower 4-Bump Comparator in Ultra-Tiny 0.73 x 0.73mm WLP/SOT23 Packages

This video provides an introduction to Maxim's NanoPower 4-Bump Wafer-Level-Package Comparator, the MAX40002 to 15 family.

ISO 16750-2, Level III Cold Crank Detail

Cold crank detail per ISO 16750-2, Level III

4-Channel Backlight Driver with Boost Controller

4-channel backlight driver with boost

5V LDO bias during cold crank

2.5V, 100ms cold-crank spike that doesn’t affect the output voltage (VBOOST) and LED current.

5V LDO Bias During Cold Crank

5V LDO bias during cold crank

Multiple Automotive Displays

Multiple displays in the car

Webinar: When and Why System Reliability Matters

In this webinar, gain a deeper understanding of when and why system reliability matters. You’ll get an introduction to the MAX32670 low-power microcontroller, which helps increase system robustness via ECC (error correcting code) and provides a wide array of security features.

Learn more: Maxim's Sensor Experience ›

Learn more: MAX32670 ›

Inis Mor Island Cliffs

As the tall, sharp edge of the cliffs of Inis Mor Island in Ireland illustrates, achieving performance at the edge in a manufacturing environment requires a new way of thinking to reach these new heights. Photo courtesy of Brian DeAngelis.

Complete Optical Biosensing Module with Ultra-Low-Power Biometric Sensor Hub

MAXM86146

Highly-integrated, optical data acquisition system combines optical biosensing AFE with a powerful Arm® MCU and two photodiodes.

Learn more ›

COVID-19 Relief Effort from Maxim Integrated

Maxim employees prepare food donations to support COVID-19 relief efforts.

Ventilator

Maxim Integrated provides ICs for ventilators and other equipment used in the care of COVID-19 patients.

Data Center

Maxim’s analog PAM4 chipset delivers DSP-like performance for hyperscale data center applications, without DSP costs, power, or latency.

Maxim Integrated Website Homepage

Maxim Integrated Website Homepage

Equine SmartBits horse bridle bit

Biometric sensors integrated into a horse bridle bit from Equine SmartBits measure horse biometrics.

Automotive Surround-View Camera System

An ASIL-grade camera protector IC like the MAX20087 can support reliable operation of automotive surround-view camera systems

Service Robot at CES 2020

Service robots were all the rage at CES 2020

Electric Car Charging Stable, Circa Early 1900s

An electric car charging stable presented one method to “refuel” an electric vehicle in the early 1900s.

E-scooter

Location Tracking Chips Design Enabling e-Scooter Navigation

Self-Driving Car Sensors

Autonomous vehicles require many sets of “eyes,” courtesy of cameras, radar, and LiDAR sensors.

Hollysys Customer Testimonial

One of Asia’s leading automation and IT solutions providers, HollySys develops industrial automation products like PLCs.

LUXROBO IoT and Robotics Development Platform

After replacing many of the legacy ICs in its IoT and robotics development platform with Maxim analog devices, LUXROBO shortened its design cycle and reduced the solution footprint of its products.

MAX22191 digital Input IC block diagram

Diagram of How a XOR Function Works

Formula Student Germany Competitors

Formula Student Germany participants used the DS1922 iButton temperature logger to monitor their electric race car batteries.

Diagram of Self-Driving Car’s laser/receiver system

Diagram of Self-Driving Car’s laser/receiver system

ATE from NCATEST Technologies

NCATEST Technologies reduced the size and power consumption of one of its new ATE solutions using Maxim Integrated pin electronics and analog ICs.

Car Camera

Secure authentication protects this vehicle’s left-side mirror camera from being compromised. Photo courtesy of Bell Ka Pang/Shutterstock

Wearable sports technologies provide runners and other fitness buffs with valuable insights about performance and overall well-being

Wearable sports technologies provide runners and other fitness buffs with valuable insights about performance and overall well-being.

Healthcare Wearables

Healthcare wearables like smartwatches that continuously monitor vital signs are enabling users to proactively manage their health and wellbeing.

MAX11410

Diagram of MAX11410 multichannel 24-bit ADC delivers accurate sensing

MediaTek Autus 120 SoC

MediaTek’s Autus 120 SoC-based reference design, which supports automotive surround-view applications, uses Maxim GMSL SerDes technology.

True-Wireless Earbud

True-wireless earbuds design with a small, bidirectional DC powerline communication management IC and a buck-boost converter with dynamic voltage.

Philips RDT’s Tempus Pro

Philips RDT’s Tempus Pro - One of the market’s smallest, lightest, and most rugged pre-hospital vital signs monitors

Low-Power Microcontroller for Wearables

To infuse its fitness tracker with high levels of processing power at low power consumption, WHOOP turned to Maxim’s DARWIN low-power microcontrollers.

Circuit Board

EE-Sim speeds the design of switching power converters.

Digital Frontier wafer tester

Reduce power usage using NAND flash wafer tester with Maxim’s MAX9972 low-power ATE driver/comparator.

Insulin Pump

Insulin pump hacking can cause patient safety issues.

Circuit Board with Electronic Components

An Excel add-in converts ideal electronic component values into the nearest standard E series value, eliminating manual calculations.

Mikroe RTC 7 Click

Mikroe’s Real Time Clock 7 Click provides an affordable way to evaluate the MAX31341B nanoPower Real Time Clock

Diagram of Confidentiality Via Asymmetric Key Algorithm

How asymmetric key algorithm provides confidentiality

A standard AC induction motor

Industrial Automation

Future of IC Automation in Factory Setting

: Wearable Medical Device

Wearable Medical Device with optical biosensors that generate PPG data

Classical Cryptographic System

A one-time pad provides an encryption technique for a classical closed-loop cryptographic system.

Wireless Weather Station

Protect IoT applications, including remote sensors in wireless designs, using secure microcontrollers and physically unclonable function technology

Virtual Doctor Visit

Remote patient monitoring tools like virtual doctor visits are becoming more popular during the current COVID-19 pandemic.

Introduction to the MAX25612 MAX25612B Automotive Synchronous High-Voltage LED Controller

This video provides an introduction to Maxim's Automotive Synchronous High-Voltage LED Controller - the MAX25612 and MAX25612B.

Diagram of SHA3-256 Function for Secure Hash Generation

Very Low Input-Voltage Boost Converter Enables Direct Methanol Fuel Cell Hearing Aids

 

Very Low Input-Voltage Boost Converter Enables Direct Methanol Fuel Cell Hearing Aids
Learn how a very low input-voltage boost converter enables direct methanol fuel cells (DMFC) power hearing aids for a full day on a single, fast refill.

Featured parts: MAX17220, MAX17221, MAX17222, MAX17223, MAX17224, MAX17225
Read more ›

How Remote Patient Monitoring Can Help Us Battle COVID-19

Watch this video to learn how remote patient monitoring tools like biosensing wearables can help detect COVID-19 indicators. You’ll also get tips for designing accurate wearables and getting them to market quickly.

Learn more: Healthcare Solutions ›

Surpass Temperature Sensing Expectations with a Next-Generation Delta-Sigma Converter

 

Surpass Temperature Sensing Expectations with a Next-Generation Delta-Sigma Converter
Combine your high temperature thermocouple and precision RTD temperature sensors to accurately measure the hottest of your enviroments.

Featured part: MAX11410
Read more ›

How to Get Your Healthcare Wearable Off the Ground Faster

Discover MAXREFDES103, the wrist-worn health center platform that measures SP02, heart rate, and heart-rate variability. Designed with ultra-small and low-power optical sensors, along with proprietary algorithms, the MAXREFDES103 gives wearables a priceless competitive first-to-market advantage.

Learn more: MAXREFDES103 ›

How to Regulate Inrush Currents in DC-DC Converters Using Soft-Start

Teja discusses the benefit of having a soft-start feature in a DC-DC converter. He shows how it helps to reduce inrush currents, ensuring that they do not reach the converter’s peak current limits. He then uses the MAX17501 to demonstrate the effectiveness of the soft-start feature at startup.

Learn more: MAX17501 ›

Diagram of Symmetric Key Algorithms

How symmetric key algorithms provide confidentiality

MOSFET Dynamic Input Capacitance

Xilinx Zynq Ultrascale+ FPGA Power Solution

 

Complete Power Solutions for Zynq Ultrascale+ Reference Designs

Learn more ›

Xilinx Versal VC1902 AI Core

 

High Performance, Small Solution Size, and High Scalability for the Latest Generation of Xilinx FPGAs and SoCs.

Learn more ›

Accurately Diagnosing Sleep Apnea

 

"Maxim's optical sensors offer the best power-quality tradeoff.”
  - - Bart Van Pee, Ectosense Co-founder and COO


Featured products: MAX30102, MAXM86161,

Read Their Story ›

How to Quickly Measure SpO2, HR, and HRV Blood from Your Wrist Using the MAXREFDES103

Venkatesh describes what you can expect to find as you unbox the MAXREFDES103, our latest wrist-worn SpO2, heart-rate (HR), and heart-rate variability (HRV) reference design. He then explains the simple, step-by-step instructions to follow to start making measurements (datalogging) quickly.

Learn more: MAXREFDES103 ›

MAX14906 Industrial Quad Digital IO Enables Robust, Smaller Designs

Learn more about the MAX14906 quad industrial digital IO IC, with individual software-configurable channels that can function as either a digital input or digital output. The IC enables smaller designs with lower power dissipation, making it ideal for industrial automation equipment.

Learn more: MAX14960 ›

Quick Overview of the MAX14906 Quad Industrial Digital IO

Bring yourself quickly up to speed on the cool new features of the MAX14906 quad industrial digital IO—the IC that puts the "IO" into "digital IO." Discover how it enables smaller, more robust, and flexible industrial automation solutions.

Learn more: MAX14960 ›

Chapter 4: Physically Unclonable Function (PUF)

Chapter 5: Cryptographic Implementations - Hardware vs. Software

Chapter 6: Time to Think About the How and Where of Cryptography

Chapter 7: Easy Cryptography with Secure Authenticators and Coprocessors

Designing High-Quality Smart-Grid Equipment

 

"Maxim ICs are good for the power grid, and we hope Maxim can develop more products for this application area.”
  - Mr. Chen Qiurong, Sr. Manager of Hardware R&D, Beijing Sifang Automation


Featured products: MAX125, MAX16006, MAX6725, MAX13487E, MAX14841E, DS1338Z

Read Their Story ›

Introduction to the DS28C16 Low Voltage SHA-3 Authenticator

This video provides an introduction to the DS28C16 Low Voltage SHA-3 Authenticator

USB-C Fundamentals

Learn the fundamentals of the USB Type-C standard and how it is used for battery charging. In this video, Sagar describes the USB-C charging architecture before comparing USB-C charging capacity with legacy USB standards. Finally, he explains how the pin layout of the USB-C connector makes it reversible.

Learn more: Battery Management ›

How ChipDNA PUF Technology Delivers the Highest Level of IoT Security

Discover how ChipDNA PUF (Physically Unclonable Function) technology provides the highest level of data security for the IoT. With PUF, you can be confident that sensitive data handled by your IoT devices won't end up in the wrong hands.

Learn more: ChipDNA ›

Make Your Digital IO Interface Simpler but Stronger

If you're tired of large, complex, and power-hungry interfaces, upgrade to Maxim’s industrial digital I/O solutions. With up to 8 channels of fixed or configurable I/O, our robust ICs integrate multiple features to simplify your designs: isolation, translation, diagnostics, SafeDemag.

Learn more: Industrial Digital I/O ›

Evaluation System for the DS28C40

DS28C40EVKIT

Provides the hardware and software necessary to exercise the features of the DS28C40.

Learn more ›

Automotive DeepCover Secure Authenticators Stop Counterfeit Parts

Counterfeit after-market automotive parts can ruin the ADAS driving experience. Our DeepCover® secure authenticators, such as the DS28C40, make it impossible for third-party manufacturers to clone critical components for after-market auto repairs.

Learn more: DS28C40 ›

Infrared-Based Gesture Sensor

MAX25205

Data-acquisition system detects hand swipe and finger rotation gestures.

Learn more ›

Blood Pressure Monitoring from Wearable Device

Wearable medical devices can be used by patients at home to monitor blood pressure.

Xilinx Artix-7 FPGA Power Solution

 

Cost- and Efficiency-Optimized Power Solutions for Artix-7 Reference Designs

Learn more ›

Xilinx Spartan-7 FPGA Power Solution

 

Cost- and Efficiency-Optimized Power Solutions for Spartan-7 Reference Designs

Learn more ›

Introduction to the MAX15162 8V to 60V Smart Dual 1.5A Circuit Breaker with Accurate Current Monitoring  

This video provides an introduction to Maxim's 8V to 60V Smart Dual 1.5A Circuit Breaker with Accurate Current Monitoring - the MAX15162.

Introduction to the MAX18066 MAX18166 High-Efficiency, 4A, Step-Down DC-DC Regulators with Internal Power Switches

This video provides an introduction to Maxim's High-Efficiency, 4A, Step-Down DC-DC Regulators with Internal Power Switches - the MAX18066 MAX18166.

Maxim’s Automotive ICs Get You There First

With Maxim’s extensive automotive portfolio, you can build cars that deliver what today’s consumer demands: safety, security, power, and performance. See how our advanced automotive ICs, designed from the ground up, meet tough design challenges for ADAS, infotainment, power management, lighting, EV powertrain, and more.

Learn more › Automotive Solutions

Ultra-Low-Power Optical Data Acquisition System for Pulse Oximetry and HR Detection

MAX86170B

Features best-in-class SNR for measuring hydration, muscle, and tissue oxygen saturation at multiple body locations.

Learn more ›

Introduction to the MAX77511 MAX77711 10V Input Quad-Phase Configurable 3A/Phase High-Efficiency Buck Converter

This video provides an introduction to Maxim's 10V Input Quad-Phase Configurable 3A/Phase High-Efficiency Buck Converter - the MAX77511 MAX77711.

Evaluation Kit for MAX32665/MAX32666/ MAX32667/MAX32668

MAX32666EVKIT

Platforms to evaluate the MAX32665/MAX32666 high-efficiency Arm® microcontroller and audio DSP for wearable and hearable device applications.

Learn More ›

Evaluation Kit for MAX32650/MAX32651/MAX32652

MAX32650-EVKIT

Platform to evaluate the MAX32650 ultra-low-power memory-scalable microcontroller designed specifically for high-performance, battery-powered applications.

Learn More ›

Evaluation System for the MAX32660

MAX32660-EVSYS

Compact development platform that provides access to all the features of the MAX32660 in a tiny, easy-to-use board.

Learn More ›

Compact Development Board to Build Small, Power-Optimized IoT Applications

MAX32630-EVKIT

Power-optimized Arm Cortex-M4F. Optimal peripheral mix provides platform scalability. On-board Bluetooth 4.0 BLE transceiver with chip antenna.

Learn more ›

Chapter 1: Cryptography: Why Do We Need It?

Gain a basic understanding of how cryptography works and how cryptography can help you protect your designs from security threats.

See more ›

Chapter 2: Cryptographic Fundamentals

Learn about the fundamental concepts behind modern cryptography, including how symmetric and asymmetric keys work to achieve confidentiality, identification and authentication, integrity, and non-repudiation.

See more ›

DeepCover® Automotive I2C Authenticator

DS28C40

Provides a core set of cryptographic tools derived from symmetric and asymmetric security functions.

Learn more ›

Ultra Compact Development Board Fits in the Tightest Spaces, Reduces Power

MAX32625PICO

Power-optimized Arm® Cortex®-M4F. On-board PMIC provides all necessary voltages. Ultra-compact 0.6in x 1.0in dual-row header footprint.

Learn more ›

Unveiling the Smallest LoRaWAN Module for IoT

 

"Maxim offers a portfolio of chipsets and solutions that have the potential to disrupt current IoT solutions.”
  -Dr. Schekeb Fateh, Business Development, Miromico


Featured products: MAX32625, MAX32626

Read Their Story ›

ChipDNA Secure Microcontroller

MAX32520

Arm Cortex M4 Micro provides FIPS/NIST compliant TRNG with environmental and tamper detection circuitry.

Learn more ›

Chapter 3: Cryptographic Algorithms

Smile, You’re on My Security Camera!

 

Smile, You’re on My Security Camera!
Advances in wireless and IoT technologies are fueling the market growth of security camera systems. Outdoor security cameras must operate for a long time on small disposable batteries. This design solution shows how a high-performance power management system can power an outdoor security camera several months longer than an ordinary solution.

Featured parts: MAX38640, MAX38641, MAX38642, MAX38643>
Read more ›

Introduction to the MAX17673 MAX17673A Integrated 4.5V to 60V Synchronous 1.5A High Voltage Buck and Dual 2.7V to 5.5V, 1A Buck Regulators

This video provides an introduction to the MAX17673, an integrated 4.5V to 60V Synchronous 1.5A High Voltage Buck and Dual 2.7V to 5.5V, 1A Buck Regulators.

Getting Started Estimating the State-of-Charge for Li-Ion Batteries

Samantha explores some of the complex characteristics of Li-ion batteries that make it difficult to accurately determine battery state-of-charge (SoC). She examines how load, temperature, and age can affect a battery’s capacity and voltage, both of which are used to estimate battery SoC.

Learn more › Battery Fuel Gauges

How to Locate the Outline Drawings, Land Patterns, and CAD Symbols and Footprints on Maxim’s Website

Samantha shows how to locate outline drawings, land pattern drawings, and CAD symbols and footprints for all Maxim parts. She also demonstrates how to use Maxim’s CAD tools with Ultra Librarian®.

Learn more › CAD Tools

Himalaya uSLIC Modules: High-Efficiency Power in Tiny Packages

Learn how uSLIC DC- DC step-down power modules enable power supplies to be designed into very tight, space-constrained areas for reliable, robust power conversion.

Learn more › uSLIC Power Modules

Diagram of IoT System Architecture

An IoT system typically consists of devices, gateways, and the data system.

Introduction to the DS28E16 DeepCover® 1-Wire SHA-3 Secure Authenticator

This video provides an introduction to the DS28E16 DeepCover® 1-Wire SHA-3 Secure Authenticator

Shrink Your Power Supply with Efficient uSLIC Step-Down Power Module

Explore the many high-performance features of this 4.5V to 36V, 2A Himalaya uSLIC step-down power module including its wide input voltage, high efficiency, wide temp range, and ultra-small size.

Learn more: MAXM17635 ›

Providing Small, Efficient Industrial Automation Products

 

"Our purpose is to make our customers’ products more integrated. Maxim’s digital input, for example, is more integrated, which can make our customers’ products smaller and more efficient.”
  -Mr. Xia Xianqiu, R&D Manager, HollySys


Featured products: MAX14912, MAX22190, MAX14931, MAX17503, MAX3042, MAX3094E, MAX6071, MAX14783E, MAX14945

Read Their Story ›

Producing World-Class Portable Sound Systems

 

"As we experiment with speaker sound using the MAX98390, we can quickly know the possible sound effects of the final product.”
  -Henry, Acoustic Engineer, Soundmatters


Featured product: MAX98390

Read Their Story ›

Simplified Modern Cryptographic System

Get a high level of security from a symmetric key cryptographic system

Diagram of How Encryption Ensures Confidentiality

Diagram of how encryption ensures information is kept confidential.

Diagram of How Identification and Authentication Work

Example of how identification and authentication work in a cryptographic system

Diagram of Message Integrity Example

Diagram of how a message digest helps preserve message integrity

Introduction to the MAX22700E/D, MAX22701E/D and MAX22702E/D Ultra-High CMTI Isolated Gate Drivers

This video provides an introduction to Maxim's Ultra-High CMTI Isolated Gate Drivers - the MAX22700E/D, MAX22701E/D and MAX22702E/D.

Keeping Race Car Batteries Safe

 

"We chose the iButton because it is easily implemented, as it does not need any connector or external power supply. It is also very robust.”
  -Sarah Battige, Formula Student Germany Operative Team


Featured product: DS1922T

Read Their Story ›

Creating High-Quality Smart Metering Solution

 

"MAX22445 helped us pass meter type tests with more stringent requirements than IEC.”
 -Joe Leong Kok Keen, Staff Design Engineer, Hardware, EDMI


Featured product: MAX22445

Read Their Story ›

Introduction to the MAX17823B MAX17841B Automotive 12-Channel High-Voltage Data Acquisition System with SPI Communication Interface

This video provides an introduction to Maxim's Automotive 12-Channel High-Voltage Data Acquisition System with SPI Communication Interface - the MAX17823B and MAX17841B.

Introduction to the MAX40027 Dual 280ps High-Speed Comparator, Ultra-Low Dispersion with LVDS Outputs

This video provides an introduction to Maxim's Dual 280ps High-Speed Comparator, Ultra-Low Dispersion with LVDS Outputs - the MAX40027.

American Electric Vehicle Co.’s Road Buggy

American Electric Vehicle Co.’s Road Buggy could travel at speeds up to 17mph.

Physicist Raymond Gaston Planté, inventor of the rechargeable storage battery

Physicist Raymond Gaston Planté invented the rechargeable storage battery in 1859.

Siemens Self-Excited Dynamo

The self-excited generator is a dynamo that was set in motion by the residual magnetism of its powerful electromagnet.

William Morrison’s First Electric Vehicle

Chemist William Morrison built an electric carriage in 1887 and also developed a rechargeable battery for the vehicle.

Garage Electric Vehicle Charging Station

After 1905, a mercury arc rectifier system could be installed in a garage to provide electric vehicle charging.

Introduction to the MAX15093 MAX15093A 2.7V to 18V, 15A, Hot-Swap Solution with Current Report Output

This video provides an introduction to Maxim’s protection solution for 2.7V to 18V power, up to 15A amps: the MAX15093 and MAX15093A.

Introduction to the MAX32592 DeepCover Secure Microcontroller with ARM926EJ-S Processor Core

This video provides an introduction to Maxim’s DeepCover Secure Microcontroller with ARM926EJ-S Processor Core – the MAX32592 is the natural evolution of the popular MAX32590. It addresses applications where space is a real constraint while bringing a significant price cut.

Introduction to the MAX32561 DeepCover Secure Arm Cortex-M3 Flash Microcontroller

This video provides an introduction to Maxim's MAX32561, a single chip solution to integrate most of the interfaces required to build a modern financial pinpad or MPOS. The product can save many external components, saving on the PCB footprint. The product also comes with security, software stacks and evaluation reports to simplify EMV and PCI-PTS certifications while compressing the time to market when designing new pinpads and MPOS devices.

Introduction to the MAX86916 Integrated Optical Sensor Module for Mobile Health

This video provides an introduction to Maxim's Integrated Optical Sensor Module for Mobile Health - the MAX86916.

Introduction to the MAX25410 Automotive USB Power Delivery Port Protector

This video provides an introduction to Maxim's Automotive USB Power Delivery Port Protector - the MAX25410.

Introduction to the MAX16158 Nanopower, Tiny Supervisor with Manual Reset Input

This video provides an introduction to Maxim's Nanopower, Tiny Supervisor with Manual Reset Input - the MAX16158.

CIOE


Shenzhen, China
09/09/2020 - 09/11/2020

InfoComm 2020 is the largest professional audiovisual trade show in North America, with thousands of products for audio, unified communications and collaboration, display, video, control, digital signage, home automation, security, VR, and live events.

Register

Unlocking Human Performance with MAX32652

 

With 3MB flash, 1MB SRAM, and multiple memory-expansion interfaces, the MAX32652 provides the onboard memory and processing power at low power consumption WHOOP needed.

Featured products: MAX32652, MAX14745, MAX17223

Read Their Story ›

Acceleration Plethysmogram (APG)

An acceleration plethysmogram (APG) waveform is the result of a common way to process PPG data.

Power Spectral Density of PPG Data

Diagram of Power Spectral Density of PPG Data.

Introduction to the MAX20353 Wearable Charge Management Solution

This video provides an introduction to Maxim's Wearable Charge Management Solution - the MAX20353.

Introduction to the MAX25200 MAX25201 MAX25202 36V HV Synchronous Boost Controller for Infotainment Application

This video provides an introduction to Maxim's 36V HV Synchronous Boost Controller for Infotainment Application - the MAX25200 MAX25201 MAX25202.

Introduction to the MAX33012E +5V, 5Mbps CAN Transceiver with ±65V Fault Protection, Fault Detection and Reporting, ±25V CMR, and ±45kV ESD Protection

This video provides an introduction to Maxim's +5V, 5Mbps CAN Transceiver with ±65V Fault Protection, Fault Detection and Reporting, ±25V CMR, and ±45kV ESD Protection - the MAX33012E.

Introduction to the MAX25024 Automotive Low Input Voltage I2C 4-Channel 150mA Backlight Driver Supporting ASIL B

This video provides an introduction to Maxim's Automotive Low Input Voltage I2C 4-Channel 150mA Backlight Driver Supporting ASIL B - the MAX25024

Introduction to the MAXM17630 MAXM17631 MAXM17632 4.5V to 36V, 1A Himalaya uSLIC Step-Down Power Modules

This video provides an introduction to Maxim’s 4.5V to 36V, 1A High Efficiency, Synchronous DC-DC Step-Down uSLIC Power modules – the MAXM17630/1/2.

Introduction to the MAX25205 Gesture Sensor for Automotive Applications

This video provides an introduction to Maxim's Gesture Sensor for Automotive Applications - the MAX25205.

Diagram of MAX40660/MAX40661 transimpedance amplifiers for automotive LiDAR systems

Diagram of MAX40660/MAX40661 transimpedance amplifiers for automotive LiDAR systems

Diagram of MAX40025/MAX40026 transimpedance amplifiers for automotive LiDAR systems

Diagram of MAX40025/MAX40026 transimpedance amplifiers for automotive LiDAR systems

Autonomous Vehicles laser

Autonomous Vehicles laser/receiver system transmits light across the view to find objects with the reflection of the laser light.

MAX77654 block diagram

MAX77654 SIMO PMIC diagram of location-tracking chips IoT devices like e-bikes and e-scooters

Introduction to the MAX20499 Automotive Single 8A/12A Step-Down Converter Family

This video provides an introduction to Maxim's Automotive Single 8A/12A Step-Down Converter Family - the MAX20499.

Introduction to the MAX15095 MAX15095A MAX15095D 2.7V to 18V, 6.6A Integrated Hot-Swap/Electronic Circuit Breaker

This video provides an introduction to Maxim’s protection solution for 2.7V to 18V power, up to 6.6A amps: the MAX15095.

Introduction to the MAX14829 Low-Power IO-Link Device Transceiver with Dual Drivers

This video provides an introduction to Maxim's Low-Power IO-Link Device Transceiver with Dual Drivers - the MAX14829.

Introduction to the MAX20328 MAX20328A MAX20328B MUX Switches for USB Type-C Audio Adapter Accessories

This video provides an introduction to Maxim’s newest USB Type-C audio interface IC with integrated protection – the MAX20328, MAX20328A and MAX20328B.

Introduction to the MAX25601A MAX25601B MAX25601C MAX25601D Synchronous Boost and Synchronous Buck LED Controllers

This video provides an introduction to Maxim's Synchronous Boost and Synchronous Buck LED Controllers - the MAX25601A MAX25601B MAX25601C MAX25601D

Introduction to the MAX22025, MAX22028 Compact, Isolated, Half-Duplex RS-485/RS-422 Transceivers with Autodirection Control

This video provides an introduction to Maxim's Compact, Isolated, Half-Duplex RS-485/RS-422 Transceivers with Autodirection Control - the MAX22025 and MAX22028.

Secure Authentication in Automotive System

Using a secure authenticator in an automotive system prevents clones and counterfeits from operating within that system.

Improving Patient Outcomes with Remote Monitoring

 

"The DS1340 gave us a shorter design cycle as it has a built-in crystal.""
 -Neil Lundy, Technical Manager of Electronics, Philips RDT


Featured product: DS1340

Read Their Story ›

E Series function Excel options dialog box

Introduction to the MAX20075D MAX20076D MAX20076E MAX25276D 36V, 600mA/1.2A Mini Buck Converter with 3.5µA IQ

This video provides an introduction to Maxim's 36V, 600mA/1.2A Mini Buck Converter with 3.5µA IQ - the MAX20075D MAX25275 MAX20076D MAX25276D

Introduction to the MAX25613 Automotive Infrared LED Controller

This video provides an introduction to Maxim’s Automotive IR-LED Controller for Driver Monitoring Systems - the MAX25613.

Introduction to the DS28C39 DeepCover Secure ECDSA Bidirectional Authenticator with ChipDNA PUF Protection

This presentation provides an introduction to Maxim's DeepCover Secure ECDSA Bidirectional Authenticator with ChipDNA PUF Protection - the DS28C39.

Introduction to the MAX30131 MAX30132 MAX30134 4-Channel Ultra-low Power Electrochemical Sensor AFE

This video provides an introduction to Maxim's 4-Channel Ultra-low Power Electrochemical Sensor AFE - the MAX30131 MAX30132 MAX30134.

Arnold Schwarzenegger Robot at CES 2020

A robotic bust of Arnold Schwarzenegger at CES 2020 moves its face in a life-like manner.

Robot System Block Diagram

A variety of power management ICs, including protectors, LDOs, and buck converters, is needed in robotic systems.

Introduction to the MAXM17633 MAXM17634 MAXM17635 4.5V to 36V, 2A Himalaya uSLIC Step-Down Power Modules

This video provides an introduction to Maxim’s 4.5V to 36V, 1A High Efficiency, Synchronous DC-DC Step-Down uSLIC Power modules – the MAXM17633/4/5.

True-wireless earbud charging diagram

Diagram of MAX20340 DC powerline communication management IC and the MAX20343 buck-boost converter with dynamic voltage scaling enable small, power efficient true-wireless earbuds.

Creating Assistive Devices with Maxim Biosensors

 

"You have a solution (Health Sensor Platform 2.0) that is really quite excellent. I was able to leverage everything. All the sensors are Maxim sensors."
 -Marty Stone, Founder and President, Atec Inc.


Featured products: MAX30001, Health Sensor Platform 2.0, MAX86141, MAX30205, MAX32630, MAX20303, MAX32664

Read Their Story ›

Advancing Digital TV Technologies

 

"Our DVB-C modulators based on the MAX5862 and MAX5868 integrate 32 channels on a single board and up to 96 channels in a single chassis."
 -Mr. Gang Ma, General Manager, R&D, Gospell Digital Technology


Featured products: MAX5862, MAX5868

Read Their Story ›

Mouth-Based Biometrics Monitoring

 

"The Maxim chips performed beautifully when we used them. It really has become a standard with many companies."
 -Mike Saigh, CEO, Equine SmartBits


Featured products: MAX30102, MAX32664, MAX30205, MAX8808X, MAX40200, MAX8902, MAX6775

Read Their Story ›

Simplifying Creation of IoT and Robotic Devices

 

"In the case of the MAX3051, low data error rate and a competitive price were factors in our choice."
 -Hanjun Kim, Hardware Technical Lead, LUXROBO


Featured products: MAX3051, MAX38902C, MAX8969, MAX40200

Read Their Story ›

Creating High-End ATE Products

 

NCATEST was able to reduce its design cycle while creating an ATE solution that is smaller, lower power, and better performing than its predecessor.

Featured products: MAX6350, MAX6325, MAX811, MAX3232, MAX541, MAX4820, MAX11160, MAX14783, MAX6696

Read Their Story ›

Introduction to the DS28C50 DeepCover® Secure SHA-3 Authenticator with ChipDNATM PUF Protection

This video provides an introduction to Maxim's DeepCover® Secure SHA-3 Authenticator with ChipDNA™ PUF Protection - the DS28C50.

Introduction to the MAX17670 MAX17671 MAX17672 Integrated 4V-60V, 150mA, High-Efficiency, Synchronous Step-Down DC-DC Converter with 50mA Linear Regulator

This video provides an introduction to the MAX17670/71/72, a dual-output regulator integrating a 4V to 60V, 150mA high-voltage, high-efficiency synchronous step-down converter with internal MOSFETs and a high-PSRR, low-noise, 2.35V to 5V, 50mA linear regulator.

Power management architecture for car camera system

A car camera power protector IC can be part of a fusion ECU for the camera system.

Introduction to the MAXM17536 MAXM17537 4.5V to 60V, 4A Himalaya Step-Down Power Modules

This video provides an introduction to Maxim’s 4.5V to 60V, 4A High Efficiency, DC-DC Step-Down Power Module with Integrated Inductor – the MAXM17536/7

electronica 2018 – 360 View

See the full view of Maxim solutions at electronica 2018.

Learn more ›

Introduction to the MAX86171 Best-in-Class Optical Pulse Oximeter and Heart-Rate Sensor AFE for Wearable Health

This video provides an introduction to Maxim's Best-in-Class Optical Pulse Oximeter and Heart-Rate Sensor AFE for Wearable Health - the MAX86171

Xilinx VCU108 FPGA Power Solution

 

Complete Power Solution for the Virtex Ultrascale VCU108 Reference Design

Learn more ›

Xilinx KCU105 FPGA Power Solution

 

Complete Power Solution for the Kintex Ultrascale KCU105 Reference Design

Learn more ›

Xilinx VCU110 FPGA Power Solution

 

Complete Power Solution for the Virtex Ultrascale VCU110 Reference Design

Learn more ›

Bluetooth Low Energy: The Physical Layer—Part 1 of 7

In the first video of this series on Bluetooth® Low Energy, we investigate the radio (or physical) layer, including operating frequency, modulation, and channel management techniques. In Part 2, “Bluetooth Low Energy: How to Define a BLE Application,” we’ll explore using a sample BLE application.

Learn more: MAX32666 ›

Bluetooth Low Energy: How to Define a BLE Application—Part 2 of 7

In the second video in this series, we explore a typical Bluetooth® Low Energy application - a heart rate monitor - to examine how BLE devices use profiles to organize and share information. In Part 3, “Bluetooth Low Energy: Understanding GAP Roles,” learn how to use Generic Access Profiles in BLE applications.

Learn more: MAX32666 ›

Bluetooth Low Energy: Understanding GAP Roles—Part 3 of 7

The third video in this series describes how the Generic Access Profile assigns a set of roles used by Bluetooth® Low Energy (BLE) devices to form a Piconet. We define those roles, explain how peripherals and centrals establish a connection, and introduce the concept of the host and controller pieces of the Bluetooth stack. In Part 4, “Bluetooth Low Energy: Unpacking the Physical Layer Packets,” learn how packets are used for data communication.

Learn more: MAX32666 ›

Bluetooth Low Energy: Unpacking the Physical Layer Packets—Part 4 of 7

In Part 4 of this series, we show how Bluetooth® Low Energy (BLE) uses packets for data communication. We describe the BLE packet structure, before examining an advertising packet in more detail. In Part 5, “Bluetooth Low Energy: Dissecting the Controller Layer,” we’ll examine the host and controller layers.

Learn more: MAX32666 ›

Bluetooth Low Energy: Dissecting the Controller Layer—Part 5 of 7

The Bluetooth® Low Energy stack consists of two parts: the host, which is home to the higher layer protocols and profiles, and the controller, where the radio and associated PDU control logic is located. In the fifth part of this series, we dissect the controller into its constituent components and show how the individual blocks work together to ensure a reliable transfer of information. In Part 6, “Bluetooth Low Energy: All About BLE Security,” we’ll learn how BLE keeps information private.

Learn more: MAX32666 ›

Bluetooth Low Energy: All About BLE Security—Part 6 of 7

Bluetooth® Low Energy (BLE) is often used to transport sensitive information, such as health-related data. The sixth video in this series shows how BLE keeps this information private by using security protocols to protect the data transport link. In Part 7, “Bluetooth Low Energy: Developing an Application,” we’ll explain the concept of an API.

Learn more: MAX32666 ›

Introduction to the MAX22520 One-Time Programmable (OTP) Industrial Sensor Output Driver

This video provides an introduction to Maxim's One-Time Programmable (OTP) Industrial Sensor Output Driver - the MAX22520.

Introduction to the MAX2223 Ultra-Wideband, Direct-Conversion, L-Band Satellite Tuner

This video provides an introduction to Maxim’s Ultra-Wideband, Direct-Conversion, L-Band Satellite Tuner – the MAX2223.

Introduction to the MAX16141 MAX16141A 3.5V to 36V Ideal Diode Controller with Voltage and Current Circuit Breaker

This video provides an introduction to Maxim's 3.5V to 36V Ideal Diode Controller with Voltage and Current Circuit Breaker - the MAX16141 MAX16141A.

698MHz to 3800MHz RF Power Amplifier Linearizer

SC1905

True RFin/RFout solution supports 100MHz BW for modular power amp designs, including 3G, 4G, and 5G cellular infrastructure.

Learn More ›

300MHz–960MHz (G)FSK Transmitter with I2C Interface

MAX41464

Includes Bits-to-RF single-wire MCU for low-cost implementation, up to +16dBm output power to increase short-range transmissions.

Learn More ›

Low-Power DOCSIS 3.1 Programmable-Gain Amplifier

MAX3523

Passes stringent DOCSIS 3.1 specifications. Low 3.5W power dissipation surpasses cable modem/gateway requirements.

Learn More ›

Frequency Synthesizer Shield

MAXREFDES161

Frequency synthesizer generates 23.5MHz to 6GHz microwave radio signals. Level translators connect to +3.3V and +5V microcontrollers.

Learn more ›

Evaluation Kit for Multiband Universal GNSS Receivers

MAX2771EVKIT

Provides multi-constellation/multi-band support with superior RF performance for the highest position accuracy.

Learn More ›

Evaluation Kit for Universal GNSS Receivers

MAX2769CEVKIT

Fully programmable, supports GPS, GLONASS, and Galileo systems in a single chip.

Learn More ›

Frequency Synthesizer Shield

MAXREFDES161

Frequency synthesizer generates 23.5MHz to 6GHz microwave radio signals. Level translators connect to +3.3V and +5V microcontrollers.

Learn more ›

Evaluation Kit for Multiband Universal GNSS Receivers

MAX2771EVKIT

Provides multi-constellation/multi-band support with superior RF performance for the highest position accuracy.

Learn More ›

Evaluation Kit for Universal GNSS Receivers

MAX2769CEVKIT

Fully programmable, supports GPS, GLONASS, and Galileo systems in a single chip.

Learn More ›

LiDAR system

Diagram of LiDAR system with the TIA and COMP optical receiver system.

MAX40660 and MAX40661 transimpedance amplifiers block diagram

Diagram of MAX40660/MAX40661 transimpedance amplifiers (TIA1 and TIA2) for automotive LiDAR.

MAX40025 and MAX40026 high-speed comparators

MAX40025 and MAX40026 stabilize the TIA optical signal in LiDAR applications.

Ultra-High CMTI Isolated Gate Driver

MAX22701E

Features single-ended input with Miller clamp output.

Learn more ›

How to Design a Negative Voltage Reference Using MAX828

Katie explains the purpose of a stable voltage reference and describes three common methods used to create one. Next, she shows how the MAX828 can be used to quickly and easily create a small, efficient negative voltage reference for applications which use a bipolar supply.

Learn more: MAX828 ›

Bluetooth Low Energy: Developing an Application—Part 7 of 7

Nobody writes programs for Bluetooth® Low Energy (BLE) from scratch. In the final video of this series, a sample fitness tracking application is used to explain the concept of an API (Applications Programming Interface).

Learn more: MAX32666EVKIT ›

Fan motor efficiency and power factor for 38–50W shaded-pole motor and PMSM motors

Fan motor efficiency and power factor for 38–50W shaded-pole motor and PMSM motors. Image courtesy of Oak Ridge National Laboratory.

Fan motor efficiency and power factor for 38–50W ECM and PMSM motors

Fan motor efficiency and power factor for 38–50W ECM and PMSM motors.

11.5A, 900V silicon carbide power MOSFET from Wolfspeed

An 11.5A, 900V silicon carbide power MOSFET from Wolfspeed. Image courtesy of Wolfspeed, a Cree company.

A standard AC induction motor

Compact Development Board for Secure IoT Applications

MAX32520-KIT

Cortex®-M4 secure microcontroller provides secure boot and protection against physical tampering for IoT applications.

Learn more ›

Introduction to the MAXM17712 MAXM17720 and MAXM17724 Integrated 4V-60V, 150mA, Himalaya uSLIC Step-Down Power Module with 50mA Linear Regulator

This video provides an introduction to Maxim's Integrated 4V-60V, 150mA, Himalaya uSLIC Step-Down Power Module with 50mA Linear Regulator - the MAXM17712 MAXM17720 and MAXM17724

EE-Sim DC-DC Tool Overview

See a demonstration of the most commonly used functionality in EE-Sim. Includes opening a new DC-DC design, changing design requirements, creating a schematic, running simulations, comparing designs, and generating a report.

Learn more: EE-Sim Design and Simulation Tool ›

EE-Sim Design Requirements

How to set the Design Requirement specifications and create a schematic.

Learn more: EE-Sim Design and Simulation Tool ›

EE-Sim Working with Components

Review the manufacturer, part number, and key properties for each recommended component in your schematic. Select a different component, or define your own component. How ceramic capacitor performance is derated, and why that is important.

Learn more: EE-Sim Design and Simulation Tool ›

EE-Sim Simulation

Use the Simulation Setup Window to run up to six simulation types. If desired, customize a variety of simulation settings. Places to access the resulting waveforms.

Learn more: EE-Sim Design and Simulation Tool ›

EE-Sim Design Tradeoffs

Prioritize the design size, efficiency, or BOM cost based on your design needs. Learn how this selection is implemented in your schematic.

Learn more: EE-Sim Design and Simulation Tool ›

NFC/RFID Tags and Readers

Fundamentals of NFC/RFID Communications

What’s the difference between NFC and RFID? Learn about the technology behind near field communication (NFC) and radio frequency identification (RFID) and the unique application characteristics of each. See how NFC and RFID ICs use modulation and demodulation processes, and through electromagnetic waves, move from the transmitter or tag to the receiver or reader.

Learn more › NFC/RFID Tags and Readers

Enabling High-Performance Automotive Infotainment

 

"MAX9286 is highly integrated and can support up to four camera links. This compact integration takes up less space on the mainboard and also reduces the bill of materials cost for customers.”
-JC Hsu, Corporate Vice President, MediaTek


Featured products: MAX9286, MAX96705, MAX15007C, MAX8902B

Read Their Story ›

Introduction to the MAX14828 Low-Power, Ultra-Small IO-Link Device Transceiver

This video provides an introduction to the MAX14828, a Single 250mA IO-Link Transceiver + DI.

Redefining Motion Capture

 

"Maxim ICs are making our products work in a more stable and reliable manner.”
-Dr. Tristan RuoLi Dai, CTO, Noitom


Featured products: MAX17224, MAX14841E, MAX809S, MAX14527, MAX8887, DS3231M, MAX8881

Read Their Story ›

Making Clothes Smarter

 

“Maxim support enabled us to use these parts effectively, and we created a design that is more or less without compromise.”
 -Dylan Jackson, Lead Embedded Engineer, Spire


Featured products: MAX30110 and MAX17223

Read Their Story ›

Dual-Channel, Synchronous Buck High-Brightness LED Controller with SPI Interface

MAX20096

Ultra-fast transient response with near-fixed frequency minimizes EMI for matrix lighting, wide dimming ratio allows high contrast.

Learn more ›

2A Synchronous Buck LED Driver with Integrated MOSFETs

MAX20050

High-performance, compact, and efficient buck LED driver simplifies automotive and general lighting designs.

Learn more ›

Automotive High-Voltage, High-Brightness LED Controller

MAX20090

Single-channel HB LED driver for front-light applications such as high-beam, low-beam, and daytime running lights.

Learn more ›

12-Switch Matrix Manager for Automotive Lighting

MAX20092

Single/dual/quad-string configurations, programmable 12-bit PWM dimming, enables matrix/pixel lighting up to 1.5A

Learn more ›

Synchronous Buck, High-Brightness LED Controller

MAX20078

Industry's First Automotive Buck Controller with Ultra-Fast Response and Pseudo Fixed-Frequency Regulation

Learn more ›

60V, 1A, Automotive Synchronous Step-Down DC-DC Converter

MAX20058

60V Synchronous Buck Converter with Internal FETs Enables High Efficiency and Low Temperature Rise

Learn more ›

36V, 2.5MHz Automotive Boost/SEPIC Controllers

MAX16990

2.5MHz Automotive PWM Controller Enables Space-Efficient Preboost Supplies for Cold/Warm Crank Applications

Learn more ›

High-Voltage, 3-Channel Linear High-Brightness LED Driver with Open LED Detection

MAX16823

Highly Integrated, High-Voltage LED Driver Ideal for Automotive Applications

Learn more ›

Introduction to the MAX17662 3.5V to 36V, 2A, High-Efficiency, Synchronous Step-Down DC-DC Converter

This video provides an introduction to Maxim's 3.5V to 36V, 2A, High-Efficiency, Synchronous Step-Down DC-DC Converter - the MAX17662.

Understanding Power Losses in Buck Converters

Anthony examines the large power losses associated with the rectification diode of a traditional buck converter. He then shows how a synchronous buck converter, like the MAX17506 or MAX17503, can significantly improve efficiency, thermal performance, and reliability by replacing the diode with an integrated MOSFET.

Learn More > Himalaya Buck Converters

Transimpedance Amplifier with 100mA Input Current Clamp for Automotive LiDAR

MAX40660

Small 3x3 TDFN with wide 490MHz bandwidth captures road condition detail and low 2.1pA/√Hz noise density reduces signal distortion and misinterpretation.

Learn more ›

How to Use DC-Biasing Configurations to Extend the Operating Voltage Range of a Flyback Converter

Teja considers the advantages and disadvantages of three commonly used DC biasing configurations that allow a flyback converter to operate above its absolute maximum voltage rating. He explains why transformer auxiliary winding is the best option, before using the MAXREFDES1193 to calculate the efficiency of this configuration.

Learn more: MAXREFDES1193 ›

Simplify System Power Designs and Achieve Bigger, Sharper Automotive Displays

Maxim's automotive-grade power ICs enable a wide range of display capabilities, helping you implement solutions to support higher luminance, higher current, and increased channel, making it easier to design bigger, sharper automotive displays. Our automotive display ICs also meet ASIL-B and high power requirements for greater reliability.

Learn more: Automotive Display Power ›

Michael Kratsios, U.S. Chief Technology Officer

U.S. Chief Technology Officer Michael Kratsios discusses AI leadership at CES

Elaine Chao, U.S. Secretary of Transportation

Elaine Chao announced AV 4.0, the U.S. initiative on autonomous vehicles, at CES 2020.

5G Technology

5G technology promises to bring the IoT to more people.

Driverless Taxi

Hyundai and Uber are teaming up to bring a driverless taxi to the market.

How to Fix a Corrupted EEPROM on an SC1905EVKIT or SC1894EVKIT

Samantha shows how to identify if your SC1905EVKIT or SC1894EVKIT has a corrupted EEPROM by measuring the supply current or by running the GUI. She then shows some simple fixes to restore your EV kit if this is the case.

Learn more: SC1905 ›

Beacon Current Profile

Typical Beacon Block Diagram

Bluetooth Beacons in the Smart Factory

Tutorial: All About Frequency Synthesis

Learn how variable frequency synthesis is achieved with the phase-locked loop (PLL). This video covers PLL theory and design including the phase detector, loop filter, voltage-controlled oscillator (VCO), integer dividers/multipliers, and the benefits of fractional division. Resources for finding integrated frequency synthesizer ICs are provided.

Learn More › PLLS and VCOs

USB to 1-Wire adapter

DS9481R-3C7

With the OneWireViewer PC utility, easily exercise and evaluate 1-Wire devices.

Learn more ›

Evaluation kit for the DS9090EVKIT

DS9090EVKIT

With the OneWireViewer PC utility, exercise and evaluate a broad range of 1-Wire devices.

Learn more ›

MAX17301/11 functional diagram

Pack-side fuel-gauge implementation

Host-side fuel-gauge implementation

1-Wire Technology Overview - Part 2

In “1-Wire Technology Overview - Part 1," you learned about the 1-Wire® protocol. In part 2, learn how the 1-Wire communication protocol can be used in authentication, memory, and temperature sensing applications.

Learn more: 1-Wire ›

1-Wire Technology Overview - Part 1

Learn how the 1-Wire® communication protocol works, its advantages over other types of serial communication, common implementation configurations, and popular 1-Wire applications. In the next video, “1-Wire Technology Overview - Part 2,” you’ll learn how the 1-Wire protocol is used in applications.

Learn more: 1-Wire ›

Introduction to the MAX77504 14Vin 3A High Efficiency Buck Converter

This video provides an introduction to Maxim's 14Vin 3A High-Efficiency Buck Converter - the MAX77504.

Introduction to the MAX77501 110VPK-PK High Efficiency Piezo Haptic Actuator Boost Driver

This video provides an introduction to Maxim’s first high voltage high efficiency piezo haptic driver – the MAX77501.

Introduction to the MAX20412 Automotive Low-Voltage 2-Channel Step-Down Controller

This video provides an introduction to the MAX20412, a dual-output, high-efficiency synchronous step-down controller IC that operates with a 3.0V to 5.5V input voltage range and provides a 0.25V to 1.275V output voltage range.

Introduction to the MAX14813 Ultra-Compact Octal 3L/Quad 5L Pulser with T/R Switches and Beamforming Capability

This video provides an introduction to Maxim's Ultra-Compact Octal 3L/Quad 5L Pulser with T/R Switches and Beamforming Capability - the MAX14813.

Evaluation Platform for Wrist-Based Heart-Rate and SpO2 Monitoring

MAXREFDES103#: Health Sensor Band

Demonstrates the high sensitivity and algorithm processing functions of health-sensing applications.

Learn more ›

3.5V to 36V Ideal Diode Controllers with Voltage and Current Circuit Breaker

MAX16141/MAX16141A

Mitigates high-voltage transient spikes, fast (0.3µs typ) shutdown response prevents reverse currents, and 5μA (typ) shutdown current reduces battery drain.

Learn more ›

280ps High-Speed Comparator, Ultra-Low Dispersion with LVDS Outputs

MAX40026

10ps overdrive delay at 20mV to 100mV output drive (dispersion) for 0.018cm time-of-flight measurement error in 2mm x 2mm TDFN.

Learn more ›

Introduction to the MAX25249 MAX25249B Quad Output Mini PMIC for Automotive Camera Applications

This video provides an introduction to Maxim’s Flexible Mini Dual 2.2MHz, 500mA Buck Converter with LDOs for Automotive Camera Supplies – the MAX25249 and MAX25249B

Introduction to the MAX98360A MAX98360B MAX98360C MAX98360D Tiny, Cost-Effective, Plug and Play Digital Class-D Amplifier

This video provides an introduction to Maxim's Tiny, Cost-Effective, Plug and Play Digital Class-D Amplifier - the MAX98360A MAX98360B MAX98360C MAX98360D

Meeting Food Quality Criteria

 

"For our purpose, the iButton is the perfect choice because it’s so small, robust, and can be reused many times.”
 -Dr. Thijs Defraeye, Laboratory for Biomimetic Membranes and Textiles, Empa


Featured product: DS1922L

Read Their Story ›

Introduction to the MAX20340 Bidirectional DC Powerline Communication Management IC

This video provides an introduction to Maxim's Bidirectional DC Powerline Communication Management IC - the MAX20340.

How to Measure Current with the MAX4173 Current-Sense Amplifier and a Microcontroller

In this video, Sean uses the MAX4173 Evaluation Kit together with an Arduino® Uno to measure current. He also discusses the principle behind measuring current and why a current-sense amplifier is a very useful addition to this technique.

Learn more › MAX4173

Ultra-Low Power Octal, Digital Input Translator/Serializer

MAX31910

Translates, conditions, and serializes digital output of industrial sensors and switches.

Learn more ›

Octal, High-Speed, Industrial, High-Side Switch

MAX14900E

Fast 24V driver, low propagation delay, and 100kHz load-switching speed for high-speed PLCs.

Learn more ›

Introduction to the MAX20057 MAX20457 MAX20458 36V Boost Controller with Two Synchronous Buck Converters (3.5A/2A) for Automotive Applications

This video provides an introduction to Maxim's Synchronous Buck Converters for Automotive Applications.

Introduction to the MAX40056F/T/U Bidirectional Current Sense Amplifier with PWM-Rejection

This video provides an introduction to the MAX40056, a bi-directional current-sense amplifier with an input common-mode range that extends from -0.1Vto +65V together with protection against negative inductive kickback voltages to -5V.

How to Set Up a SerDes Reverse Control Channel When PCLK is Not Available - Using the MAX96705/MAX96706 GMSL SerDes

Learn how to establish the I2C reverse control channel when PCLK is not available using the MAX96705 Gigabit Multimedia Serial Link (GMSL) serializer and MAX96706 GMSL deserializer.

Also see: How do I program the remote side of a SerDes link when PCLK is not present?

Learn more: MAX96705 16-Bit GMSL Serializer ›

Learn more: MAX96706 14-Bit GMSL Deserializer ›

Automotive displays

Bigger, sharper automotive displays benefit from highly integrated power management ICs.

MAXREFDES103#

The MAXREFDES103# is a full wrist-worn wearable reference design for heart-rate, heart-rate variability, and SpO2 measurements.

Introduction to the MAX17634A, MAX17634B and MAX17634C 4.5V to 36V, 4.25A, High-Efficiency, Synchronous Step-Down DC-DC Converter

This video provides an introduction to Maxim's 4.5V to 36V, 4.25A, High-Efficiency, Synchronous Step-Down DC-DC Converter - the MAX17634A, MAX17634B and MAX17634C.

Kingston A2000 SSD

The Kingston A2000 SSD delivers fast, reliable performance for laptops.

LynQ people compass

The LynQ device creates a private network to help users find one another.

Sublue WhiteShark Mix underwater scooter

Sublue’s WhiteShark Mix underwater scooter propels users underwater, in pools or in the ocean.

Sublue WhiteShark Mix underwater scooter

Explore the ocean with Sublue’s WhiteShark Mix underwater scooter.

Ricoh Imaging Theta SC2 360° camera

The Theta SC2 360° camera creates still or video images that you can rotate around.

Miracle-Gro Twelve

The Miracle-Gro Twelve Indoor Growing System is a smart hydroponic garden for growing herbs and vegetables inside.

Blood-Pressure Monitoring Smartwatch

Smartwatches and other wearables deliver accurate, continuous monitoring of blood pressure for better preventive health measures and disease management.

Introduction to the MAX17576 4.5V to 60V, 4A, High-Efficiency, Synchronous Step-Down DC-DC Converter with Internal Compensation

This video provides an introduction to Maxim's 4.5V to 60V, 4A, High-Efficiency, Synchronous Step-Down DC-DC Converter with Internal Compensation - the MAX17576.